Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe & Sound @ E14-CLEWE @#10_430hsite
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
  • Author Author: jkutzsch
  • Date Created: 7 Jul 2017 5:41 PM Date Created
  • Views 1691 views
  • Likes 3 likes
  • Comments 12 comments
Related
Recommended

Safe & Sound @ E14-CLEWE @#10_430hsite

jkutzsch
jkutzsch
7 Jul 2017

Posted by jkutzsch in Safe and Sound on Jul 5, 2017 11:44:00 PM

 


E14-C.L.E.W.E. INDEX:

#1_”The word.”

#6_Energia!

#2_”The Science.”

#7_Blog7

#3_"GPS decisions."

#8_GPS_Issues

#4_"GPS arrives!"

#9_GPS_Stalled

#5_"The box, the box!"

#10_43ohSite

                                                                             image

 

Okay as discussed in the last post I am still project blocked by a failure on my part to get the TI talking with the GPS.  Undoubtedly something simple but as of yet unknown.

 

I had found mention of someone else having similar issues and getting answers on the forum 43oh site.  It appears that basic browsing and searching without a user account will yield no information so here I will connect to that site.

 

image

 

Here we have the basic view once you have connected and NOT logged in with a user account.  Looks promising!

 

(Well Technically I would think the view would be the same even if you are logged in.)

 

 

image

 

Here we have the result of trying to go deeper into any of those interesting forums and not having an account.

 

If somewhere it states you need to have an account to view those threads I missed that in my excitement to discover a solution to my problem.  :-)

 

So lets follow the tested advice from rachaelp on registering and then the site opening up for access!

 

 

image

 

Ah the basics, time to sign up and get some more emails!

 

 

image

 

Oddly enough it didn't show it in the cut and paste but you do get a popup saying to check your email and confirm.  So off to my email and clickity click.

 

 

 

 

image

 

Tada.  I am now a registered user and and able to jump into the Energia subforum!  Woohoo!

 

image

 

Let's try doing a search on gps to see if that pulls up what I have been looking for and anyone else experimenting with it.

 

Nope 0 results found.  Hmm...

 

image

 

GSM?  Nope.

 

image

 

By the way, don't be too quick in your search efforts or else you get this!

 

So no go with searching.  Or at least with my new experience to their search options.  I did try using the author option and apply the gentleman's name that was talking about the problem on the other site but couldn't find that either.

 

image

 

So let's start browsing through the forum manually.  Only 1,524 topics available.  :-)

 

 

image

 

Wait what?  Why is this back?  I went to double check something while writing the blog...

 

Ah it seems that it has a super fast auto-logoff.  Sigh...

 

image

 

Not sure if they kick you at an hour or what.  You can see I am the newest member of an hour ago.

 

Okay.  End of the blog for now.  I will need time to browse those 1.5k topics.  :-)

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 9 years ago +2
    It's worth checking the comments that people posted on your 7th blog. There are ways to verify if serial communication is working. Look at Jon's and mcb's posts in particular. You can use a loopback to…
  • jkutzsch
    jkutzsch over 9 years ago in reply to Jan Cumps +2
    Ah, I think you mean blog 8. I will have to try and figure out the best loopback option. I was actually using the offered com port code by Energia to test with, which kind of made me confused on why I…
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to jkutzsch +2
    I'll do a check of the program you posted. I've got a bus pirate (useful when you want to do a quick test of a protocol) I've removed the TX and RX jumpers from the LaunchPad so that there's no contention…
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to jkutzsch

    I'll do a check of the program you posted.

     

    I've got a bus pirate (useful when you want to do a quick test of a protocol)

    image

     

    I've removed the TX and RX jumpers from the LaunchPad so that there's no contention between USB and UART.

    (also have to download energia - it's been a while since I used it - a laptop ago image )

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 9 years ago in reply to Jan Cumps

    Even just receiving the NMEA strings from the GPS would be great!  :-)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to jkutzsch

    Thanks. I'll try to see if that communication receives correctly from a 9600 baud UART.

    This seems to be an input only program, it doesn't send data to the GPS ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 9 years ago in reply to Jan Cumps

    Here is the example Energia code that the provide:  Energia Reference - Tutorials

     

    /*

      Serial Event example

     

      When new serial data arrives, this sketch adds it to a String.

      When a newline is received, the loop prints the string and

      clears it.

     

      A good test for this is to try it with a GPS receiver

      that sends out NMEA 0183 sentences.

     

      Created 9 May 2011

      by Tom Igoe

      Modified 24 April 2013

      by Sean Alvarado

     

      This example code is in the public domain.

     

    */

     

    String inputString = ""; // a string to hold incoming data

    boolean stringComplete = false; // whether the string is complete

     

    void setup() {

      // initialize serial:

      Serial.begin(9600);

      // reserve 200 bytes for the inputString:

      inputString.reserve(200);

    }

     

    void loop() {

      // print the string when a newline arrives:

      if (stringComplete) {

      Serial.println(inputString);

      // clear the string:

      inputString = "";

      stringComplete = false;

      }

    }

     

    /*

      SerialEvent occurs whenever a new data comes in the

      hardware serial RX. This routine is run between each

      time loop() runs, so using delay inside loop can delay

      response. Multiple bytes of data may be available.

    */

    void serialEvent() {

      while (Serial.available()) {

      // get the new byte:

      char inChar = (char)Serial.read();

      // add it to the inputString:

      inputString += inChar;

      // if the incoming character is a newline, set a flag

      // so the main loop can do something about it:

      if (inChar == '\n') {

      stringComplete = true;

      }

      }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to jkutzsch

    Good luck. If you want me to test out your code (I don't have the GPS module but have a 432 and can snoop serial coms), just ask what you want to have checked.

    Your project is worth having live. Let's try to make it happen.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>