Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe & Sound @ E14-CLEWE @#9_GPS Stalled
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
  • Author Author: jkutzsch
  • Date Created: 6 Jul 2017 4:44 AM Date Created
  • Views 1645 views
  • Likes 3 likes
  • Comments 12 comments
Related
Recommended

Safe & Sound @ E14-CLEWE @#9_GPS Stalled

jkutzsch
jkutzsch
6 Jul 2017


E14-C.L.E.W.E. INDEX:

#1_”The word.”

#6_Energia!

#2_”The Science.”

#7_Blog7

#3_"GPS decisions."

#8_GPS_Issues

#4_"GPS arrives!"

#9_GPS_Stalled

#5_"The box, the box!"

                                                                             image

 

I have to apologize that this project has came to such a sad state of stalling.

 

I have continued to research and see if there are other ways that I can get this working but so far no luck.

 

I have completely ripped the project back down, retested the gps with arduino Uno and then re-assembled and retried code provided as good to go for serial/gps testing.

Code is same as in Blog 8.

 

I did find some hints that others have had the same issue:  https://e2e.ti.com/support/microcontrollers/msp430/f/166/p/586961/2165670

 

"Please help somehow the serial monitor is not displaying any readings when I connect the GPS to P3.2 and P3.3 ..."

 

and

 

"Well I have been working in arduino for sometime now and the first part was implemented correctly..No problem at all...But when I am going to implement the same in msp432  nothing is happening..."

 

This sounds mighty similar to what I am running into.

 

Later he references success from information he found at 43oh.com but never details what was done.  :-(

 

"Thanks at least I can now get the location in my serial monitor...Forum 43oh was of great help"

 

and

 

"Thanks for all your help...I was finally able to successfully complete the whole project"

 

No links, so I have been checking the forum myself but keep getting:

 

image

 

Sigh...

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 9 years ago +4
    Hey John, have you logged a post on 43Oh, ti e2e or here to get help for your problems? I usually get help there - also when there's an existing ticket with the same simptoms. people will tell you that…
  • rachaelp
    rachaelp over 9 years ago in reply to Jan Cumps +3
    Hi John, I second Jan's suggestion, it's probably worth posting up on all these forums to try and get help if you haven't already, as somebody will likely be able to point you in the right direction. It…
  • jkutzsch
    jkutzsch over 9 years ago in reply to jkutzsch +3
    One of the items I referred to quite a bit when planning this was dougw awesome table of pins from his blog 5 when he was explaining his pcb. Safe and Sound - Hazardous Gasses PCB - blog 5 I really found…
  • rachaelp
    rachaelp over 9 years ago in reply to Jan Cumps

    Hi John,

     

    I second Jan's suggestion, it's probably worth posting up on all these forums to try and get help if you haven't already, as somebody will likely be able to point you in the right direction.

     

    It looks like there is a forum issue on 43Oh which they may or may not be aware of as that particular section you reference gives an error but you can still run a search and get to posts in that section from the results so you might find something that way.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago

    Hey John, have you logged a post on 43Oh, ti e2e or here to get help for your problems?

    I usually get help there -  also when there's an existing ticket with the same simptoms.

     

    people will tell you that there's an exisiting ticket, but will help you when you explain that it didn't help you.

     

    there's still time....

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
<