Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog UpCycle It - R2I - #1 - Introduction
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
  • Author Author: jkutzsch
  • Date Created: 24 Mar 2017 2:24 AM Date Created
  • Views 2992 views
  • Likes 6 likes
  • Comments 16 comments
  • incubator
  • upcycle it design challenge
  • upcycle_it_r2i
Related
Recommended

UpCycle It - R2I - #1 - Introduction

jkutzsch
jkutzsch
24 Mar 2017

UpCycle IT – R2I INDEX:

 

Blog #1_”Introduction”

Blog #2_”Designing”

Blog #3 "The Kit"

Blog #4_"Mother Natures Version"
Blog #5_"Research"
Blog #6_"Competition01"

Blog #7_"Edison Setup"

Blog #8_"Edison 2 Ardunio"
Blog #9_"Grove-ON"
Blog #10_"Hot2Not"

UpCycle It - R2I –Refrigerator 2 Incubator

Refrigerators, everyone loves them, they keep your food cold, extend the life span of meats and dairy and when they stop working, take up a LOT of space.

Here in the U.S. you have to pay a lot of extra charges to have refrigerators properly disposed of.  Undoubtedly one of the reasons you will see them laying in vacant lots and piled outside of buildings in low income areas.  No one wants to deal with them after they can no longer keep items cold.

 

image

I found an online news article that discussed how second hand refrigerators being imported into Ghana from the European Union reached such a critical mass point that on January 1st 2013 they banned the import of all used refrigerators, freezers and air conditioners.

While newer model systems avoid the old issues of chlorofluorocarbons (cfc) which can damage the ozone layer they can still provide quite an impact on land fills and similar disposal options due to their size and quantity.

As such I am taking an old mini-fridge and using it as the main part of my Upcycle project!  Something that later can be expanded to full sized items easily by anyone desiring to do so.  (In fact I also have another plan to take a full size standing freezer with glass door and Upcycle that in the future but I was unable to find a donor freezer and so that will wait for a future blog posting to Element 14.)

 

image

 

Here is the basis of my project getting a much needed cleaning prior to tear down.

 

image

Here is the door removed, inside compartments of door removed and beginning of inside tear down.  The fridge is actually upside down here since I was cleaning up parts to get ready for a professional to remove the compressor and cooling systems.

image

The Fridge ready to start having items added and tested for the R2I project!

image

The rear showing the compressor and various parts removed and a nice open space in the back.

image

Here is Blue Dude showing us the next piece of the project, eggs!

My idea is to take the Challenger Kit comprising of the IntelRegistered Edison Kit for Arduino, IntelRegistered Edison Breakout Board, Arduino Protoshield R3, the Grove Starter Kit for Arduino, an AC/DC power supply and a USB cable.  Add my stripped and cleaned up mini-fridge, a heating element (looking at heating tape), a custom designed egg turning assembly and of course a dozen or more fertilized chicken eggs to have an Incubator.

 

I want to use as many of the Grove Starter Kit pieces as possible in the incubator (such as the mini-servo, led lights, relays, temperature sensor) but believe I will need to add a high quality humidity sensor as well since I am not seeing such an item reflected in the literature on the kit.

image

Here is a general idea with the Heat tape along the back.  The custom egg holder/rotator going from side to side and there being a divider across the center of the fridge to allow heat to be kept at the top side with a possible use of the bottom for holding the kit.

In addition I will cut a viewing window in the door and replace with plexi-glass to allow us to monitor everything without having to open the device and upset the temperature/humidity.

The Intel Edison Kit looks to be a great option for implementing all of my desired features and I look forward to taking this to the next step and blogging as we create this Upcycle Project.  Ultimately to take it through the incubation of chicken eggs to show success!  I see great video opportunities!

  • Sign in to reply

Top Comments

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +2
    A tip would be to ensure the plastic of the fridge interior will take the heat from the tape If you are planning on using Mains powered heaters this become more critical as a failure could lead to injury…
  • mcb1
    mcb1 over 9 years ago in reply to jkutzsch +2
    The 3 options seemed to be: Light bulb. Ceramic heater that goes into a light bulb socket. Heat tape . There are two others I can think of 1. was another heat pad that I saw for keeping welding electodes…
  • shabaz
    shabaz over 9 years ago +2
    It's a shame the Edison is power-efficient, otherwise you could have put a few of them inside, and designed it so they perform useful computation until the inside is at the right temperature, and then…
Parents
  • DAB
    DAB over 9 years ago

    Nice update.

     

    I like the idea of using the sensors to monitor the environment within the refrigerator.

    We take for granted that it is stable and good for the food inside.

    It would be very interesting to see what really happens.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 9 years ago

    Nice update.

     

    I like the idea of using the sensors to monitor the environment within the refrigerator.

    We take for granted that it is stable and good for the food inside.

    It would be very interesting to see what really happens.

     

    DAB