Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog [Upcycle It] Interactive Race Car Driver - Car modification
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
  • Author Author: Workshopshed
  • Date Created: 15 Apr 2017 1:16 PM Date Created
  • Views 839 views
  • Likes 5 likes
  • Comments 4 comments
  • interactiveracecardriver
  • upcycle_it
  • upcycled_interactiveracecardriver
Related
Recommended

[Upcycle It] Interactive Race Car Driver - Car modification

Workshopshed
Workshopshed
15 Apr 2017

My main concerns about the car were the high driving position and general space for the electronics. There were some handy screws on the front and back so I though those would make good points to attach my own platform. There is also a bit of flex in the chassis now so my additions will need to include re-enforcement.

 

{gallery} Car Modifications

image

Before: The car base

image

Step 1: After removing the battery box the platform was still quite high

image

Stripped: So I stripped it down even further

image

Driver: New lower driving position

image

Edison: There should be space in the engine compartment for the Edison

 

Disaster and repair

Although I'd previously thought that the gearboxes were fine, I noticed that one of the wheels was freewheeling whereas the other side turned as a pair. I opened up the gearbox again and spotted that one of the pinions was rotating freely on it's axle. When I removed it, it split into two.

image

I looked through my collection of gears and found a replacement, except it was connected to another gear. I sawed it off with a junior hacksaw and it fitted onto the spindle. It was a little loose so I added some cyanoacrylate adhesive (superglue).

 

imageimageimage

Now my vehicle is back on the road and ready for some new electronics.

 

Previous Posts

[Upcycle It] Interactive Race Car Driver - Plan of action

[Upcycle It] Interactive Race Car Driver - Software

[Upcycle It] Interactive Race Car Driver - Lights

[Upcycle It] Interactive Race Car Driver - Detailed Plan

[Upcycle It] Interactive Race Car Driver - Edison

[Upcycle It] Interactive Race Car Driver - Drive Motor Testing

  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago +1
    Great fix in the true engineering spirit. DAB
  • jasonwier92
    jasonwier92 over 9 years ago +1
    I like the Frankenstein it is becoming. Using the servo to "lean" into a corner would be cool.
Parents
  • jasonwier92
    jasonwier92 over 9 years ago

    I like the Frankenstein it is becoming.  Using the servo to "lean" into a corner would be cool.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jasonwier92
    jasonwier92 over 9 years ago

    I like the Frankenstein it is becoming.  Using the servo to "lean" into a corner would be cool.