Merry Boxes & LEDs
  • Challenges & Projects
  • Project14
  • Merry Boxes & LEDs
  • More
  • Cancel
Merry Boxes & LEDs
Blog Merry Boxes - A Project Within a Project
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Merry Boxes & LEDs to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 11 Jan 2019 5:04 AM Date Created
  • Views 1522 views
  • Likes 8 likes
  • Comments 3 comments
  • wifi
  • merryboxesledsch
  • box
  • paper
  • holidayspecial19ch
  • xmas
  • enclosure
  • arduino
  • wemos
  • sensor
Related
Recommended

Merry Boxes - A Project Within a Project

ntewinkel
ntewinkel
11 Jan 2019
image

Merry Boxes & LEDs

Enter Your Project for a chance to win a Maker Tool Kit, an Oscilloscope Grand Prize for the project that brings the Most Joy to the Heart, and Gift to Gives!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

I was having trouble finding suitable enclosures for the electronic bits of my Connected Xmas Trees project.

I have lots of Altoids tins, but being metal they would not be ideal, likely blocking the WiFi signal of the Wemos controllers.

 

Then while I was putting away the Christmas decorations on the weekend I noticed a little box a friend had given us some years ago - made out of a Christmas card!

So I thought I'd try that to make the little boxes to hide the electronics for the trees, and have it be somewhat festive at the same time.

 

Tools and Materials:

* 1 Christmas card to make 1 box

* Clear tape or glue

* Scissors

* Ruler

* Pencil

 

Step 1: Cut the card in half. We'll use the pretty front of the card for the box lid, and the back for the bottom box.

image

 

Step 2: Size the bottom box on the back side of the card. I used an Altoids tin, as that size looks about right for my project.

image

 

Step 3: Draw the outlines. The inside lines are the size of the box, so I simply drew around the tin.

I then drew a box, 3/4" bigger on each side, around the outside to make the sides, which will be 3/4" tall.

image

 

Step 4: Cut away everything outside of that 3/4" outline

Step 5: Snip the bottom corners on one of the lines of each corner only (see the next pictures for more clarity)

image

 

Step 6: Pre-fold on all the lines

image

 

Step 7: Fold the sides up and together

image

 

Step 8: Tape the corners

image

 

Step 9: Make the lid slightly bigger so it's easy to put on and take off. I used the bottom box and marked slightly bigger around it.

image

 

Step 10: Repeat steps 3 through 8 to finish the lid. (or is that 6 steps?)

 

Step 11: Admire the finished Merry Boxes!

image

 

The Altoids tin fits!

(You know, in case you want to pretty up an Altoids tin project)

image

 

The electronics of my Connected Xmas Trees project will need a little bit of careful placement, but it should work.

image

 

The resulting boxes aren't Altoids-tin strong, but should be enough to hold the tree securely.

If you need super strong boxes, start with higher quality cards image

 

Cheers,

-Nico

 

ps, did anyone notice I didn't use the card from the first picture? I only needed 2 boxes. Maybe I'll still assemble it.

pps, do I get bonus points for the *ahem* clever naming of the boxes being made? image

ppps, it's actually a pretty quick project - taking pictures and writing this blog entry took most of the time!

 

Previous posts:

Connected Christmas Trees

Assembling the Trees

Finally! Two Trees Assembled

Two Trees by a Tree

Connecting the Tree to the Internet

Motion Sensor on Wemos

Trees! one with motion sickness...

Motion Sensor Issues, continued

The Connected Trees are Working!

 

Next post:

Connected Christmas Trees - Finished!

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 7 years ago +3
    Hardly a CNC made box but just as suitable. We do see the odd micro board coming through in very robust boxes. I must remember that I could use them in future projects. Mark
  • Problemchild
    Problemchild over 7 years ago in reply to mcb1 +1
    I should at some point try and get some thin plywood not unlike a balsa then laser cur it would be fun to see how good a case you can get. Any one have experience of sub 3mm Ply any good for anything or…
Parents
  • mcb1
    mcb1 over 7 years ago

    Hardly a CNC made box image  but just as suitable.

     

    We do see the odd micro board coming through in very robust boxes.

    I must remember that I could use them in future projects.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 7 years ago

    Hardly a CNC made box image  but just as suitable.

     

    We do see the odd micro board coming through in very robust boxes.

    I must remember that I could use them in future projects.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Problemchild
    Problemchild over 7 years ago in reply to mcb1

    I should at some point try and get some thin plywood not unlike a balsa then laser cur it would be fun to see how good a case you can get.

    Any one have experience of sub 3mm Ply any good for anything or as weak as snot ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 7 years ago in reply to mcb1

    mcb1  wrote:

     

    Hardly a CNC made box image  but just as suitable.

    Hehe yep I really need to start making some sawdust with that CNC machine already, just to get the hang of it.

     

    >We do see the odd micro board coming through in very robust boxes.

    Do you mean you can buy them with the enclosures? Or are these specific micro boards?

     

    -Nico