Merry Boxes & LEDs
  • Challenges & Projects
  • Project14
  • Merry Boxes & LEDs
  • More
  • Cancel
Merry Boxes & LEDs
Blog Motion Sensor Issues, continued
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Merry Boxes & LEDs to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 5 Jan 2019 11:39 PM Date Created
  • Views 4218 views
  • Likes 8 likes
  • Comments 18 comments
  • wifi
  • merryboxesledsch
  • xmas
  • motion
  • arduino
  • wemos
  • sensor
Related
Recommended

Motion Sensor Issues, continued

ntewinkel
ntewinkel
5 Jan 2019
image

Merry Boxes & LEDs

Enter Your Project for a chance to win a Maker Tool Kit, an Oscilloscope Grand Prize for the project that brings the Most Joy to the Heart, and Gift to Gives!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

I spent a fair bit of time today trying to figure out what was going on with the motion sensor on Tree 1.

 

I tried a few things, starting with switching the Wemos itself, and it turns out that when I use the Wemos from the working tree, Tree 1 does work properly.

So it's not the tree itself or the wiring around it, or the PIR sensor. That's a good thing.

 

Here is a video of me testing the PIR sensor directly, powered by the breadboard power supply. It works nicely.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Then I thought maybe I had shorted something out and broken the Wemos board, but further testing showed that switching input pins made no difference, and I could set the inputs directly to GND or to 3.3 volts, and it would read correctly.

 

The motion sensor does require 5v input power, with minimum of 4.5v, so I thought I'd compare the two Wemos boards. They have pretty much identical voltage showing at the 5v pin. Actually a little low - 4.69v, when powered from my Mac. Yet one works, and the other doesn't!

So I decided to directly power the board with a USB charger instead, but alas, it still did not work.

 

A video showing my pain:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The sketch running on the Wemos is just one that does serial coms for debug, and checks for PIR input. However, if you look carefully the PIR sensor wire is only going to the multimeter, and thus the GPIO input is always just 10k to gnd. In short - the Wemos is only used to power the PIR sensor at this point.

 

As you can hear me say in the video, I was thinking of just giving up on the motion sensors altogether and just using a pushbutton instead. That might actually make more sense in real life use anyway.

 

The other thought I had is that PIR sensors can be sensitive to interference (so they say on the internets, it may or may not be true) - maybe this difficult Wemos board was causing more interference than the other?

 

Then I had a thought... The official Raspberry Pi power supply provides a slightly higher 5.1v, maybe that gives the PIR sensor that little extra edge to work?

And lo and behold! it works! Kinda surprised me at this point, actually.

 

So it appears that, annoyingly enough, the PIR sensor should probably not be powered by the Wemos 5v pin. I thought it was a direct connection to the USB input, but I wonder if there's something else in the way.

In general, the whole setup should probably provide power to the tree and the sensor separately from the power supplied to the Wemos. But that's beyond the scope of this project.

 

So I will reassemble Tree 1, upload the Connected Trees sketch back on it, add some nail polish to the connections, and then make it all look pretty... and I'll make sure to use the RPi power adapter for the difficult Wemos.

 

I'm not entirely happy with the finicky results, but for now this will have to do. If we do end up using this "in real life" next Christmas, I'll probably just switch it to use pushbuttons instead.

 

Here's a picture of the solder joints with dollar-store nail polish protecting the joins. I ended up buying a pack just for the red and green in it, and it turns out the rainbow of colours works well here!

 

image

 

Edit:

Here is a quick sketch of the schematic that I used to keep things straight in my mind while soldering. The input pins have since changed a little (pls see the source code for the updated numbers).

image

Note that in this sketch "Tree 1" and "Tree 2" refers to the two wires going to the trees, not to separate trees. I probably should have written it more clearly, like "Main Tree" and "Tree top LED". The transistors are basic NPN 2N2222a.

 

Cheers,

-Nico

 

 

Previous posts:

Connected Christmas Trees

Assembling the Trees

Finally! Two Trees Assembled

Two Trees by a Tree

Connecting the Tree to the Internet

Motion Sensor on Wemos

Trees! one with motion sickness...

 

Next posts:

The Connected Trees are Working!

Merry Boxes - A Project Within a Project

Connected Christmas Trees - Finished!

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 7 years ago +5
    Good work sorting out the issues. On the link you sent for the PIR, it appears there is a diode in series with the +ve input, which then goes to what looks like a regulator. I found this here https://www…
  • mcb1
    mcb1 over 7 years ago in reply to mcb1 +4
    There is an interesting note here about the 'boot' time. https://forum.arduino.cc/index.php?topic=538734.0 He has also managed to reduce the 10sec delay. Mark
  • mcb1
    mcb1 over 7 years ago in reply to ntewinkel +4
    Not sure if I want to keep using the PIR sensors for these trees though Perhaps those microwave sensors that fmilburn suggested here LS Cubed: Little Sister Security System Mark
Parents
  • Gough Lui
    Gough Lui over 7 years ago

    It may well be 5V from the USB on the Wemos is actually the RAW input. But the problem might be resistance from your USB lead - perhaps try a shorter lead or one with thicker gauge wire - there's a lot of cheap chargers with bad leads. The peak Wi-Fi transmission current could cause the input voltage to dip enough to cause strange behaviour too.

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Gough Lui
    Gough Lui over 7 years ago

    It may well be 5V from the USB on the Wemos is actually the RAW input. But the problem might be resistance from your USB lead - perhaps try a shorter lead or one with thicker gauge wire - there's a lot of cheap chargers with bad leads. The peak Wi-Fi transmission current could cause the input voltage to dip enough to cause strange behaviour too.

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ntewinkel
    ntewinkel over 7 years ago in reply to Gough Lui

    You make a really good point! This reminds me of power issues with the Raspberry Pi.

    I never thought it would be an issue here, being a relatively simple setup. But like you say, the Wi-Fi transmission could be a heavy current draw that I wasn't thinking of.

     

    I'll use some better cords and adapters for the final setup.

     

    Thanks,

    -Nico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 7 years ago in reply to Gough Lui

    But the problem might be resistance from your USB lead

    That is relevant for the Pi with the peak currents it draws, but these ESP devices are drawing much less.

     

     

    Unless they are using a LDO (Low droput regulator) they need 2v above the output voltage to function correctly.

    Even some LDO are  1.0 to 1.2v (depending on current) ... so 3.3 + 1.2 = 4.5v and the diode can add another 0.5v so you're looking for 4.8 to 5.0.

     

    No wonder it was struggling.

     

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago in reply to mcb1

    Well, the OP was measuring slightly low on the 5V (USB supply pin) of the WeMos, hence my suggestion. I think he was powering the PIR from there as it was a 5V unit. That's why the LDO itself can't affect the voltage to the PIR (which appeared to be the source of the trouble).

     

    Of course, if you start dipping on the input of the regulator, the ESP8266 may undervolt .In my experience, peak current is about 170mA for the chip itself. Despite being rated for 3.3V, I have had no issues operating down to 2.0-2.1V unregulated from a pair of AA cells, so I doubt that should be a major source of issues. Most ESP prototype units do use an AMS1117 LDO if I recall correctly, makin tthis even less likely to be an issue.

     

    Instead, you can never underestimate the crass low quality USB leads available - some are just barely good enough for a USB charged Bluetooth headset and its 350mA draw. Other times, it can be mechanical - due to poor connector tolerances causing high resistance.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 7 years ago in reply to Gough Lui

    Sorry Gough but Nico was having issues with the PIR playing up.

    Yes the power was coming via the 5v pin on the Wemos which it was obtained via a USB lead and slightly low supply.

     

     

    My calculations were for the 3v3 on the PIR.

    If the input voltage is below the dropout, then the chip (not sure which one it is for this particular PIR) doing all the work could well be struggling.

    All the versions I've seen state 4.5v to 20v input, which seems to be the voltage range of the regulator.

     

    I do like the idea of feeding the PIR with 3v3 directly from the ESP device.

    It also means there are less chances of incorrect voltage on an input.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago in reply to mcb1

    Ah, okay, I see where you're coming from.

     

    Sure, if there's a 3V3 already available, might as well use it if it's an LDO that has enough capacity already rather than trying to make a non-LDO linear regulator happy.

     

    - Gough