Open Arduino
  • Challenges & Projects
  • Project14
  • Open Arduino
  • More
  • Cancel
Open Arduino
Blog Arduino in Test Instrumentation - Part 1: SCPI Lib
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 6 Apr 2018 1:00 PM Date Created
  • Views 8976 views
  • Likes 12 likes
  • Comments 16 comments
  • diytestequipch
  • openarduinoch
  • scpi
  • arduino_test_instrumentation
Related
Recommended

Arduino in Test Instrumentation - Part 1: SCPI Lib

Jan Cumps
Jan Cumps
6 Apr 2018
image

Open Arduino

Enter Your Project for a chance to win a grand prize for the most innovative use of Arduino or a $200 shopping cart! The Birthday Special: Arduino Projects for Arduino Day!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Arduino in Test Instrumentation

 

To celebrate Project 14's birthday, I'm going to make a programmable switch with an Arduino UNO.

In this post I try out the SCPI library.

image

 

SCPI Library Installation

 

I'm using a SCPI lib that's written for Arduino: Open Instrument Control.

You can download the GIT archive as a zip.

To install it in the Arduino environment, first check in the Arduino gui where your sketchbook folder is (Via File -> Preferences).

Extract the GIT archive in a temporary location. Copy the src/ArduinoSCPIParser folder to the sketchbook/libraries subfolder

On my PC: D:\users\jancu\Documents\Arduino\libraries\ArduinoSCPIParser.

 

You'll have to comment out one line in the scpiparser.cpp source, or you get compilation errors:

 

// #include <WProgram.h>

 

This is because the SCPI library we're using isn't adapted to the recent Arduino software versions.

 

Test the SCPI Library

 

There are two examples in the SCPI lib. We're using Meter.ino.

Open the example in the Arduino GUI (File -> Open, then navigate to the place where you extracted the GIT archive and open src/Examples/Meter/Meter.ino).

Connect your UNO, select Tools -> Board -> Arduino/Genuino UNO.

Select Tools -> Port -> <the COM port of your Arduino>.

Select Sketch -> Upload.

 

Your Arduino is now programmed with the Meter example and the SCPI lib.

To test the basic setup, open the serial monitor:

Tools -> Serial Monitor

Enter the SCPI command *IDN? and press Send.

The monitor should log the result: OIC,Embedded SCPI Example,1,10.

 

image

 

 

Related Blog
Arduino in Test Instrumentation - Intro: SCPI Programmable Switch
Arduino in Test Instrumentation - Part 1: SCPI Lib
Arduino in Test Instrumentation - Part 2: Firmware
Arduino in Test Instrumentation - Part 3a: LabVIEW Driver Intitialisation Block
Arduino in Test Instrumentation - Part 3b: LabVIEW Driver Switch Control Block
Arduino in Test Instrumentation - Part 3c: LabVIEW Driver Read Status Block
Arduino in Test Instrumentation - Outro: LabVIEW Example
  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +4
    Jan, Nice update on your project. I look forward to following your progress on this project. Maybe this will convince me to look further into Arduino as a potential for future projects. Good luck on your…
  • mcb1
    mcb1 over 8 years ago in reply to Jan Cumps +2
    I tend to have my Arduino in C:\Development\Arduino\ *whatever version* I have multiple versions of the IDE which worked out useful when there was a bug ... it worked on a earlier version so it wasn't…
  • jomoenginer
    jomoenginer over 8 years ago in reply to mcb1 +2
    If the library will not be used in other applications, you could just add a 'src' folder where the .ino file is located and add your code there. You would then need to reference the files with the 'src…
Parents
  • Andrew J
    Andrew J over 5 years ago

    Hi Jan,

    are you still using this library or have you skipped over to Jan Breuer's?  I've used this one - despite it's memory leak! - but with a shift to an Arduino Mega I'm thinking that Jan's might be more suitable as it seems to be maintained.  Do you have a better documented (i.e. commented) example of Jan's library with your Hercules controller?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago in reply to Andrew J

    Have you looked at the one that comes up in the Arduino library manager? It seems to be by someone who simply calls themselves 'Vrekrer'. Just wondered what it was like to use. There's not much documentation, but there are a couple of examples.

     

    I realised a while back that the D-type connector on the back of my Fluke bench meter is an RS232 port and the meter uses SCPI over it, so I thought I might try some simple automation via a UNO, or something like that. I was expecting to use the one that Jan originally introduced us to; I didn't realise that there were now several alternatives.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to jc2048

    I only used the library of this blog post to turn an Arduino into a SCPI device.

     

    Jon, to talk to your SCPI capable meter you don't need a library.  On the "programming" side these libs don't play a role.

    You would need a RS232 physical layer driver or breakout kit on the Arduino side. Then use the Serial lib.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to jc2048

    I only used the library of this blog post to turn an Arduino into a SCPI device.

     

    Jon, to talk to your SCPI capable meter you don't need a library.  On the "programming" side these libs don't play a role.

    You would need a RS232 physical layer driver or breakout kit on the Arduino side. Then use the Serial lib.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jc2048
    jc2048 over 5 years ago in reply to Jan Cumps

    I should have explained better. I'm thinking of a box with some reed relays to switch the meter inputs, ie a hardware multiplexer on the meter input (obviously just for voltage measurements). It could also be used for other things too, as it would just be 4mm connectors in and out. To do that I had thought to intercept the SCPI from the PC, extract any commands for controlling the relays, and pass everything else on to the meter.

     

    I could achieve the same thing with a completely separate relay box, but since I need to do the USB-to-RS232 stuff and generate real RS232 voltage levels for the meter, it seemed like a reasonable combination of things to throw it all together in one small box.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 5 years ago in reply to jc2048

    You will want something to do that in that case Jon.  The library Jan and I have used here works, but it does have a memory leak in the error handling code (easily fixed) and I found it necessary to write a fair bit of processing code with it.  It’s not maintained but I don’t think that’s an issue as it’s pretty simple and quick to get going.  The library you point out didn’t convince me that much so I haven’t tried it.  The Jan Breuer library scpi-parser looks very complete but may be too big for an Arduino depending upon the rest of the sketch.  The examples are enough to get you going but, not being a C/C++ programmer of any experience, I’ve had to trawl through the code to work out what I need to do as it isn’t well commented and the documentation, although much better than most libraries out there, is still a bit lightweight and possibly not up to date.

     

    For something simple, I’d go with the one discussed originally by Jan.  I may well swap back to it.  I also could provide a more comprehensive working example for you as well if you need it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to jc2048

    You could use the error handler for that purpose, maybe: If the parser detects an error, throw it over the wall to the meter?

    And whatever the meter sends back, relay to the host?

     

    In general, it would work.

    You'd have to refine the error querying. Because you will have to be able to report error status on any of the two instruments when SYST:ERR queries are fired.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago in reply to Andrew J

    I'm getting a little bit confused with all this [there are too many Jans in the world, aren't there!].

     

    I need it to be lightweight to run on an UNO, so you're saying that rules out the Breuer one [which, from my cursory glance at the git page, does look like it's done reasonably well].

     

    I was curious about the Vrecker one, mainly because it appears in the Library Manager so it's very easy to use in an Arduino project.

     

    It sounds like I should stick with the original one. How did you find the memory leak? Did you do that with the Arduino IDE somehow, or were you using a different processor and other tools?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago in reply to Jan Cumps

    That's an interesting idea. I'll have a look at that.

     

    I hadn't considered the error status return at all, but I'm sure it can be wangled somehow.