Recycle & Retrofit
  • Challenges & Projects
  • Project14
  • Recycle & Retrofit
  • More
  • Cancel
Recycle & Retrofit
Blog Mr. Machine gets an upgrade - Mostly working, but still needs a little some help.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Recycle & Retrofit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: genebren
  • Date Created: 22 Dec 2020 4:09 AM Date Created
  • Views 5108 views
  • Likes 14 likes
  • Comments 17 comments
  • recycleretroiftch
Related
Recommended

Mr. Machine gets an upgrade - Mostly working, but still needs a little some help.

genebren
genebren
22 Dec 2020

In my prior blogs (Mr. Machine gets an upgrade - working on the pieces. , Mr. Machine gets an upgrade - new internals, motors installed and new PCBs , Mr. Machine gets an upgrade - time is running down  and Mr. Machine gets an upgrade - New boards, but not enough time ) I walked through Mr. Machine's history and some of my updates.  This time (for the second time, thanks to a extended due date, thanks Tariq) I will wrap up what I can as the project14 deadline closes.

 

For the most part I have written enough code to exercise the basic functions of the three boards that make up Mr. Machines electronics.  There was a fair amount of hacking involved to get some of the functions to work and the once pristine PCBs look like that have survived a war.  The most glaring of errors occurred in the LED dimmer circuit.  I have used the dimmer chip (TLC59731) before in another product, but it was a single LED channel.  In copying the circuit (which I designed a few years ago), I failed to remember that I single MOSFET in the serial path was both a switch (to suppress other serial traffic) and an inverter.  The inverter is used to invert the uart output to match the requirements of the dimmer chips requirements, so without it, I was unable to program the LEDs.  Also, due to the use of multiple LEd dimmers I needed to work out a method of injecting a fixed width low signal between programming bursts.  This one took a bit of head scratching, but I ended up using a time interrupt to signal when the serial stream should resume.  Here is an image of the PCBs prior to putting them all back into Mr. Machine:

imageimage

Here are the PCBs getting attached to Mr. Machine's internal frame:

imageimage

From here the internal frame (with attached electronics) was fitted into Mr. Machine's plastic skin.  It was during the assembly process that I ran into a problem.  Mr. Machine's old winding key was supposed to be repurposed into an on/off switch.  But once everything was in place (and because of the rework on the backside of the Power Pack, I noticed that the micro switch was push away from the cam assemble that should have pressed and released the switch.  I tried to shim and reposition things. but I was unable to come up with a clean solution.  With the deadline rapidly approaching, I decided to leave the key assemble out and I would use a pencil through the key hole to press and release the switch.  One mission objective scratched.

 

Speaking of scratched mission objectives, here are a few other features that fell off the table as I struggled to get some of the most basic features working.  Here are a few of the missing and/or limited features:

  1. Motor control - I had initially written a complex motor control function that included ramp up/down stepper controls and a multiple state state machine, but the debugging process was not going well, so I stripped the functions out and quickly wrote some simple code to read the R/C receiver outputs (direction/speed and turning) and convert them into appropriate stepper motor pulse patterns.
  2. Front and Rear IR sensors - I ran out of time to code the fail safe stops and inhibits associated with the sensors, so they were left off.
  3. LED light during movements - I had previously scratched the idea of getting LED lighting cues from the Midi player, but again with time running out, I left off any LED sequencing when Mr. Machine was moving.  I did a short LED sequence on power up for each board (shown below), the more impressive light show will have to wait for later.
  4. Winding key on/off switch - The final fit of all the pieces killed this feature.  I need to use a pencil to reach into Mr. Machine to reach the tiny micro switch to turn him on and off.

 

With everything installed inside Mr. Machine, it was time for a couple of quick (uneditted and very raw) videos of Mr. Machine in action.  First up is a video of Mr. Machine motors running on my desk top/workbench.  This video shows the speed and direction control of the two stepper motors.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Next up is a power up sequence, followed by the Midi file player playing "This Old Man" (a very fitting song given the creator of this project).  (Note: the audio is a bit distorted, but the case also seem to cause some resonance issues)

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Finally, the proof video of Mr. Machine in motion.  I really struggled to speak in this video as I was rushing about trying to get things running and my brains were a bit scrambled.  I did experience some issues with the motors during this video.  I believe that these motors (even with their gear reductions) were a bit over loaded (not enough torque), but I does demonstrate forward/reverse and turning.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Once again, I would like to thank Tariq and the rest of the staff at element14 for givings us all a great place to gather and the opportunity to exercise our creative juices.  I had so much fun working on this project and I look forward to tuning this all up and working out the remain bugs and completing the features that did not make it in yet.

 

Note: attached are all of the source files for the various processors and PCBs.

 

Thanks and enjoy!

Attachments:
Mr. Machine.zip
  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 5 years ago +4
    Gene, Seems pretty good to me. I have always suffered from problems when it comes to stuffing the electronics into the selected shell. I can manage the electronics (mostly) but I always get wildly optimistic…
  • 14rhb
    14rhb over 5 years ago in reply to dubbie +4
    Agree, there's always so much more to a great project than just getting the technical side working. On home projects I too struggle to box projects up and documenting/source configuration is often completely…
  • fmilburn
    fmilburn over 5 years ago +3
    Well done Gene! A really fun project and it gave me an appreciation for the complications that can occur undertaking something like this. I really like the retro style. Frank
Parents
  • jw0752
    jw0752 over 5 years ago

    Hi Gene,

     

    An amazing and well done upgrade to Mr. Machine. One of a kind! Thanks for sharing the trials and tribulations that you encountered.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 5 years ago

    Hi Gene,

     

    An amazing and well done upgrade to Mr. Machine. One of a kind! Thanks for sharing the trials and tribulations that you encountered.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • genebren
    genebren over 5 years ago in reply to jw0752

    Thanks John!  I had a lot of fun and a little stress working on this project.  The grandkids enjoyed seeing the new and improved Mr. Machine this afternoon, which makes it all worth while.