Recycle & Retrofit
  • Challenges & Projects
  • Project14
  • Recycle & Retrofit
  • More
  • Cancel
Recycle & Retrofit
Blog Mr. Machine gets an upgrade - Mostly working, but still needs a little some help.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Recycle & Retrofit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: genebren
  • Date Created: 22 Dec 2020 4:09 AM Date Created
  • Views 5198 views
  • Likes 14 likes
  • Comments 17 comments
  • recycleretroiftch
Related
Recommended

Mr. Machine gets an upgrade - Mostly working, but still needs a little some help.

genebren
genebren
22 Dec 2020

In my prior blogs (Mr. Machine gets an upgrade - working on the pieces. , Mr. Machine gets an upgrade - new internals, motors installed and new PCBs , Mr. Machine gets an upgrade - time is running down  and Mr. Machine gets an upgrade - New boards, but not enough time ) I walked through Mr. Machine's history and some of my updates.  This time (for the second time, thanks to a extended due date, thanks Tariq) I will wrap up what I can as the project14 deadline closes.

 

For the most part I have written enough code to exercise the basic functions of the three boards that make up Mr. Machines electronics.  There was a fair amount of hacking involved to get some of the functions to work and the once pristine PCBs look like that have survived a war.  The most glaring of errors occurred in the LED dimmer circuit.  I have used the dimmer chip (TLC59731) before in another product, but it was a single LED channel.  In copying the circuit (which I designed a few years ago), I failed to remember that I single MOSFET in the serial path was both a switch (to suppress other serial traffic) and an inverter.  The inverter is used to invert the uart output to match the requirements of the dimmer chips requirements, so without it, I was unable to program the LEDs.  Also, due to the use of multiple LEd dimmers I needed to work out a method of injecting a fixed width low signal between programming bursts.  This one took a bit of head scratching, but I ended up using a time interrupt to signal when the serial stream should resume.  Here is an image of the PCBs prior to putting them all back into Mr. Machine:

imageimage

Here are the PCBs getting attached to Mr. Machine's internal frame:

imageimage

From here the internal frame (with attached electronics) was fitted into Mr. Machine's plastic skin.  It was during the assembly process that I ran into a problem.  Mr. Machine's old winding key was supposed to be repurposed into an on/off switch.  But once everything was in place (and because of the rework on the backside of the Power Pack, I noticed that the micro switch was push away from the cam assemble that should have pressed and released the switch.  I tried to shim and reposition things. but I was unable to come up with a clean solution.  With the deadline rapidly approaching, I decided to leave the key assemble out and I would use a pencil through the key hole to press and release the switch.  One mission objective scratched.

 

Speaking of scratched mission objectives, here are a few other features that fell off the table as I struggled to get some of the most basic features working.  Here are a few of the missing and/or limited features:

  1. Motor control - I had initially written a complex motor control function that included ramp up/down stepper controls and a multiple state state machine, but the debugging process was not going well, so I stripped the functions out and quickly wrote some simple code to read the R/C receiver outputs (direction/speed and turning) and convert them into appropriate stepper motor pulse patterns.
  2. Front and Rear IR sensors - I ran out of time to code the fail safe stops and inhibits associated with the sensors, so they were left off.
  3. LED light during movements - I had previously scratched the idea of getting LED lighting cues from the Midi player, but again with time running out, I left off any LED sequencing when Mr. Machine was moving.  I did a short LED sequence on power up for each board (shown below), the more impressive light show will have to wait for later.
  4. Winding key on/off switch - The final fit of all the pieces killed this feature.  I need to use a pencil to reach into Mr. Machine to reach the tiny micro switch to turn him on and off.

 

With everything installed inside Mr. Machine, it was time for a couple of quick (uneditted and very raw) videos of Mr. Machine in action.  First up is a video of Mr. Machine motors running on my desk top/workbench.  This video shows the speed and direction control of the two stepper motors.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Next up is a power up sequence, followed by the Midi file player playing "This Old Man" (a very fitting song given the creator of this project).  (Note: the audio is a bit distorted, but the case also seem to cause some resonance issues)

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Finally, the proof video of Mr. Machine in motion.  I really struggled to speak in this video as I was rushing about trying to get things running and my brains were a bit scrambled.  I did experience some issues with the motors during this video.  I believe that these motors (even with their gear reductions) were a bit over loaded (not enough torque), but I does demonstrate forward/reverse and turning.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Once again, I would like to thank Tariq and the rest of the staff at element14 for givings us all a great place to gather and the opportunity to exercise our creative juices.  I had so much fun working on this project and I look forward to tuning this all up and working out the remain bugs and completing the features that did not make it in yet.

 

Note: attached are all of the source files for the various processors and PCBs.

 

Thanks and enjoy!

Attachments:
Mr. Machine.zip
  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 5 years ago +4
    Gene, Seems pretty good to me. I have always suffered from problems when it comes to stuffing the electronics into the selected shell. I can manage the electronics (mostly) but I always get wildly optimistic…
  • 14rhb
    14rhb over 5 years ago in reply to dubbie +4
    Agree, there's always so much more to a great project than just getting the technical side working. On home projects I too struggle to box projects up and documenting/source configuration is often completely…
  • fmilburn
    fmilburn over 5 years ago +3
    Well done Gene! A really fun project and it gave me an appreciation for the complications that can occur undertaking something like this. I really like the retro style. Frank
  • jw0752
    jw0752 over 5 years ago

    Hi Gene,

     

    An amazing and well done upgrade to Mr. Machine. One of a kind! Thanks for sharing the trials and tribulations that you encountered.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 5 years ago in reply to ralphjy

    Thanks Ralph!  I really enjoyed the process, which at times was quite challenging.  I really do hope to keep up some momentum on this project, but like you say, it can be difficult to stay motivated with so many other projects to do (both electronics and also home projects, i.e. landscaping, cabinets/workbenches for the shop).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 5 years ago

    Not quite the result that you wanted, but I think you did well with a complex project.  I'm sure with an iteration you could get it perfect, but if you're like me it's hard to get motivated with so many other projects to do image.

     

    Great project!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 5 years ago in reply to dubbie

    Thanks Dubbie!  Fitting everything together was really tough.  I roughly measured the distances between PCBs prior to making the wiring harnesses, but I kept getting the boards turned around or the harness swapped (end to end), making very difficult to get everything into place.  This was all made worse when the winding key (on/off) did not work out well, as the power pack and radio mounting were all apart of the assembly.

     

    I look forward to revisiting the whole wiring and mounting as I continue forward.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 5 years ago in reply to 14rhb

    Thank you.  It was a little scary running with out the edge/object sensors attached, but on the plus side Mr. Machine was not running at full speed.  So far, the main issue with binding on one side seems related to an alignment issue with the main drive gears on the axle.  I hope to come up with an adjustable motor mount that I can better 'dial' in to get a better alignment.  Until then, slow and somewhat steady will be the best approach to driving Mr. Machine around,

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>