• Products and Partners
    Products and Partners
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
Member's Forum What part am I looking for?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Answers 11 answers
  • Subscribers 631 subscribers
  • Views 2524 views
  • Users 0 members are here
Related

What part am I looking for?

justphred
justphred over 6 years ago

Hey all, I recently decided to dive headlong into the micro controller world, with a project I am working on. I'm in way over my head and Amy trying to find a place to get some assistance.

 

I am in the planning phase so far and am trying to figure out what part I need for a specific section of my project.

 

Essentially, I am trying to create a software power button. So I don't have to have a Switch and a button. this project is fairly small and I am trying to save as much space as I can. I have mapped out how I THINK it should work, and have attached a quick diagram. Here is a run down of how I think it will work...

 

  • Power comes in to the Mystery Part from a battery (a 3.7v 420mAH lipo) and is sent to a momentary switch.
  • When the momentary switch is pressed the path of the battery power flips from going to the switch to going to the micro controller. There by powering on the system. (flipping the Mystery Part from RED position to GREEN)
  • The Momentary switch is now being seen by the micro controller. Which will be programed to send a signal to the Mystery Part when the Switch is held down for 5+ seconds.
  • The Signal coming in from the micro controller switches the battery power back to the momentary switch, thus cutting power to the system and powering it off (flipping the  Mystery Part from GREEN position back to RED)

 

 

The Grey box on the diagram is the mystery part. Any help in figuring out what I need to make this happen would be appreciated.

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • genebren
    0 genebren over 6 years ago

    Michael,

     

    There are a few things that you might new to think about, before you can make use of your Mystery part.  You are planning on using a Lipo battery which has a typical voltage of 3.7 volts.  In reality this battery will supply between 4.2V and 2.5V.  This will have some influence over which microprocessor you will use.  What I typically do for battery driven circuits is to use a voltage regulator to provide a fixed voltage to the microprocessor (which will be less than the battery voltage), so with a single Lipo battery, I will use a 2.5V regulator.   Here is a circuit that I have used in several designs:

     

    image

     

    When the switch is press with the circuit off, the battery voltage is used to enable the regulator (AP2127-2.5 or a MIC5504-2.5), allowing it to generate V+ (in this case 2.5V).  The Microprocessor is started and it needs to then drive PS_EN high, thus holding the regulator on.  To turn the circuit off, the voltage at SWITCH_SENSE is monitored by the microprocessor and when the voltage is held high for an extended time (like 5 sec in your example) the microprocessor drives PS_EN low.  When the switch is released, the circuit then shuts down.

     

    This might seem like a lot to do, in order to switch power on and off, but this circuit gives you a lot of flexibility in it's functionality.  You can also add a circuit (a voltage divider like R1/R2) at the battery terminal, and measure the divider to generate a under voltage shutdown (i.e if the battery voltage drops below 2.7V).  Or you could use the microprocessor to turn the circuit off if the circuit is determined to be idle (saving battery life).

     

    Like anything in electronics, there are many ways to do the same thing.  You need to compare the pluses and minuses of each approach based on your needs.

     

    Good luck!

    Gene

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • justphred
    0 justphred over 6 years ago in reply to genebren

    Ok Gene, this is sounds exactly like how I want it to work, and yes it is a very complicated way to do a simple thing but you are correct that it provides a lot of possibilities. the auto off to save power was something that I had as a stretch goal that I figured I could make work if I got this working. I will look up those Regulators.

     

    I looked into it and the trace off of that battery board will be anywhere from 3.7v-4.2v, would the regulator you suggested still work or would I need one for a higher voltage?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • genebren
    0 genebren over 6 years ago in reply to justphred

    The MIC5504-2.5 accepts input voltages in the range 2.5 to 5.5V, so yes, this should be fine. The ItsyBitsy is listed as 3.3V, but it might actually work at lower voltages.  If not, you could use a boost regulator to allow a wider voltage range (4.2V to 2.5V) to generate 3.3V (a little more complicated, but much more versatile).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • justphred
    0 justphred over 6 years ago in reply to genebren

    Gene, you are my hero, and I greatly appreciate you breaking it down like this!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • justphred
    0 justphred over 6 years ago in reply to dougw

    Doug, I think its just my lack of understanding an experience with a FET.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 6 years ago in reply to justphred

    The FET circuit I posted above handles all your requirements as I perceive them. If there is a feature missing, please explain.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • genebren
    0 genebren over 6 years ago in reply to justphred

    Michael,

     

    In each of the examples that I shared with you, I solve the problem with the switch release removing power, by having the microprocessor hold the circuit on (i.e. keeping the regulator, or boost enabled).  This removes the need for timing circuits to keep the transistor and/or MOSFET turned on.

     

    OK, let's break this down just a bit.  In the first image, the switch is pressed and current flows (lower RED path) through the switch to the 'ENABLE' on the boost board (or regulator).  This applies power to the ItsyBitsy. (also showing current path to the boost in RED)

    image

    Now, upon wakeup the ItsyBitys Turns D11 High to provide another current path (ORANGE) to the 'ENABLE' on the boost board (or regulator).  This acts as a 'keep power on' signal.

    image

    Now, when the switch is released and current quits flowing through the lower RED path, the ORANGE path holds the  power on.

    image

    Now it is possible to use the switch as a user interface function, by monitoring the voltage between the two 100K resistors on 'A0' pin of the ItsyBitsy.  When the 'ItsyBitsy' decides that the current should shut down, the ItsyBitsy it turns D11 Low to to the disable on the boost board (or regulator) and shut the circuit down.

     

    I have used this logic on a number of battery powered projects and I find it to work quite well.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • justphred
    0 justphred over 6 years ago in reply to dougw

    What about the timing of it all, using a MOSFET would still give me the same issue wouldn't it? when I let up on the switch the board will lose power, and thus not keep the MOSFET circuit closed. Or am I not understanding how a MOSFET works correctly?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 6 years ago in reply to justphred

    If you use a P-channel mosfet instead of a bipolar transistor, the voltage drop can be negligible and the capacitor will hold it on for a long time.

    However the drive logic would be reversed (low gate voltage turns it on).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • justphred
    0 justphred over 6 years ago in reply to genebren

    Hey Gene,

     

    I had taken the last few weeks to put some distance between me and the project and, also was trying to do some test on my own.

     

    Where I ended up with my own testing was using an NPN Transistor with the switch going to the base. So that when I pressed the switch V would flow to the board.

    This worked, however, I was not able to get the board to keep the transistor open. Mainly due to the timing of it all. When I let up on the switch the power to the board was gone, thus the transistor would close. So I tried to add a capacitor in line with the switch so that when I would let up, there would be some time before the board fully lost power. yet the falloff is still too quick and the board dies almost instantaneously.

     

    What I need fo this to work is a capacitor capable of delivering 5mA for ±500mS after I let up of the switch. I tried putting a resistor in series with the capacitor so that its decay would take longer. But that either made the capacitor never reach the desired voltage. or didn't slow the decay enough. also the larges cap I had on hand was a 1000uF 25v.

     

    The other thing that I noticed this way is that I am now under-volting the board by going through the transistor. I went ahead and picked up two different boost converters. A 5v @ 1A (https://www.adafruit.com/product/4654 ) and a 5v @ 100mA ( https://www.adafruit.com/product/3661  ) both have the enable pin that I believe you are referring too.

     

    I toyed with using the enable pin on the itsybitsy, but that doesn't cut power to the vHi pin which I am using elsewhere in the circuit, which would leave stuff on.

     

    here is the schematic of where I have gotten too. I am gonna take a look at what you drew up. again I took some time from this to try and get a fresh take on it.

     

     

    image

     

    Also, THANK YOU to all. this has been the most helpful forum post I have ever been a part of!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • genebren
    0 genebren over 6 years ago in reply to justphred

    Michael,

     

    Here is a crude attempt at a drawing of a circuit that might work for you.  I found another Adafruit part (#1903) that might help you.  This should allow to prototype your project and see how it works.

    image

    I could see that you were struggling a bit trying to understand how the pieces connected, so hopefully this will clear things up.  There are three Adafruit modules and here is how they connect:

     

    1. Adafruit 2124 - Charger -  5 volts connect to the module at 5V and GND and are used to charge the Li-Ion battery.  The battery voltage (BAT) connects to the switch and to the VBAT terminal of the Boost module (1903).
    2. Adafruit 1903 - Boost - The Enable pin (EN) is driven high by the momentary switch (from VBAT) or from the Adafruit 3800 (ItsyBitsy) to turn on the Boost Circuit.  The output 5.0V provides power to ItsyBitsy.
    3. Adafruit 3800 - ItsyBitsy - Power from the Boost is applied to the VBAT pin (power input). D11 (or any other Dx pin) is used to hold the boost on (high), or to shut it off (low).  A1 is used to sample the switch output to see if it is pressed or not (for user interface functions or to turn off the unit).
    4. Misc parts.  - Diode - this is used to prevent voltage applied by the ItsyBitsy (holding power on) from attempting to charge the battery.  The two 100K resistors are scaling the voltage at the switch output (from 4.2 - 2.5V down to 2.1 to 1.25V so that they will be in the proper ranges of the ItsyBitsy ADC input (< 3.3V).

     

    Hopefully this will be a little clearer of a picture in how things could be interconnected.  Please keep in mind that I have not used any of these modules, and only quickly reviewed the documentation, so some of this may require a bit of tweaking to get it all correct.

     

    Good luck and have fun!

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • genebren
    0 genebren over 6 years ago in reply to justphred

    Michael,

     

    In the most general sense, a regulator is used to reduce one voltage (input) into a lower voltage (output).  In the case of the original schematic fragment that I supplied, we are using a special feature, present on these regulators, but necessarily all regulators, which is an enable input.  The enable signal, can turn the regulator into a switch, along with its voltage control function.

    image

     

    In the schematic, there are to paths to turn on the regulator.  The first path (through R3), passes a voltage from the battery to the enable pin of the regulator to turn it on when the switch is pressed.  Keep in mind that the regulator is powered by the battery, through the connection at pin 1 of the regulator (through the VBAT symbol).  Once the regulator is turned on, the microprocessor must use the second path (set high), through the diode (signal PS_EN) to hold the regulator on.  Then when the switch is released, this second path will hold the regulator on, until the microprocessor decides to turn it off.

     

    The voltage requirements of your ItsyBitsy board might require that you move away from a simple regulator, as the voltage requirement is 5.0 to 3.3 volts is hard to achieve with a regulator, in that the output voltage of the regulator will be less than the input voltage.  With an input voltage (i.e. the battery) of 4.2 to 2.5, a simple regulator will not be able to maintain the minimum voltage of 3.3 over the full charge cycle of the battery.  You could do two things:

    1. Use a 3.3 volt regulator and shut down when the output of the regulator drops below 3.3V (i.e. the battery voltage drops too low).
    2. Use a 5.0V boost regulator that can take any safe voltage from the battery and convert it to 5.0V, which the ItsyBitsy can accept and convert to 3.0V onboard.  The microprocessor could be setup to shut off the boost regulator once the battery voltage gets too low (2.5 to 2.7Volts).  The trick here is to keep the boost circuits output voltage (5.0) greater than the battery voltage (2.5 - 4.2V).
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • justphred
    0 justphred over 6 years ago in reply to genebren

    Gene, I'm not so sure I understand why a Regulator is the wright part. as I look at the diagram I am failing to understand how it does the original specification of switching the battery voltage between two pins.

     

    In your first schematic you have the momentary switch before the regulator. but in my drawing I have it after.

     

    I guess I'm trying to understand how a regulator works. cause I have been looking into it and to my understanding it doesn't switch anything, just keeps it at a set value.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • justphred
    0 justphred over 6 years ago in reply to genebren

    Gene, I'm not so sure I understand why a Regulator is the wright part. as I look at the diagram I am failing to understand how it does the original specification of switching the battery voltage between two pins.

     

    In your first schematic you have the momentary switch before the regulator. but in my drawing I have it after.

     

    I guess I'm trying to understand how a regulator works. cause I have been looking into it and to my understanding it doesn't switch anything, just keeps it at a set value.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • genebren
    0 genebren over 6 years ago in reply to justphred

    Michael,

     

    It appears as if there is a pull-up resistor on the enable input.  You could add a 10K resistor to ground to pull the pin low when it is not being driven high.  (Note: in a quick read of the chip and board datasheets, I see no mention of a pull up on the enable.  I should check this again with glasses on in the morning).

     

    If you have a 10K resistor to try as a pull down.  It will interesting to see what happens.

     

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • justphred
    0 justphred over 6 years ago in reply to genebren

    Ok I have some circuits out in front of me and I'm seeing a problem.

     

    I have one of those voltage boosts wired up. With nothing going to the Enable pin, and as it sits it is sending current to the board. If I jumper enable to ground the circuit shuts off and stops sending power to the board.

     

    Is this Enable working differently than expected?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • justphred
    0 justphred over 6 years ago in reply to genebren

    Gene, you are my hero, and I greatly appreciate you breaking it down like this!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • justphred
    0 justphred over 6 years ago in reply to dougw

    Doug, I think its just my lack of understanding an experience with a FET.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 6 years ago in reply to justphred

    The FET circuit I posted above handles all your requirements as I perceive them. If there is a feature missing, please explain.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • genebren
    0 genebren over 6 years ago in reply to justphred

    Michael,

     

    In each of the examples that I shared with you, I solve the problem with the switch release removing power, by having the microprocessor hold the circuit on (i.e. keeping the regulator, or boost enabled).  This removes the need for timing circuits to keep the transistor and/or MOSFET turned on.

     

    OK, let's break this down just a bit.  In the first image, the switch is pressed and current flows (lower RED path) through the switch to the 'ENABLE' on the boost board (or regulator).  This applies power to the ItsyBitsy. (also showing current path to the boost in RED)

    image

    Now, upon wakeup the ItsyBitys Turns D11 High to provide another current path (ORANGE) to the 'ENABLE' on the boost board (or regulator).  This acts as a 'keep power on' signal.

    image

    Now, when the switch is released and current quits flowing through the lower RED path, the ORANGE path holds the  power on.

    image

    Now it is possible to use the switch as a user interface function, by monitoring the voltage between the two 100K resistors on 'A0' pin of the ItsyBitsy.  When the 'ItsyBitsy' decides that the current should shut down, the ItsyBitsy it turns D11 Low to to the disable on the boost board (or regulator) and shut the circuit down.

     

    I have used this logic on a number of battery powered projects and I find it to work quite well.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • justphred
    0 justphred over 6 years ago in reply to dougw

    What about the timing of it all, using a MOSFET would still give me the same issue wouldn't it? when I let up on the switch the board will lose power, and thus not keep the MOSFET circuit closed. Or am I not understanding how a MOSFET works correctly?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 6 years ago in reply to justphred

    If you use a P-channel mosfet instead of a bipolar transistor, the voltage drop can be negligible and the capacitor will hold it on for a long time.

    However the drive logic would be reversed (low gate voltage turns it on).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • justphred
    0 justphred over 6 years ago in reply to genebren

    Hey Gene,

     

    I had taken the last few weeks to put some distance between me and the project and, also was trying to do some test on my own.

     

    Where I ended up with my own testing was using an NPN Transistor with the switch going to the base. So that when I pressed the switch V would flow to the board.

    This worked, however, I was not able to get the board to keep the transistor open. Mainly due to the timing of it all. When I let up on the switch the power to the board was gone, thus the transistor would close. So I tried to add a capacitor in line with the switch so that when I would let up, there would be some time before the board fully lost power. yet the falloff is still too quick and the board dies almost instantaneously.

     

    What I need fo this to work is a capacitor capable of delivering 5mA for ±500mS after I let up of the switch. I tried putting a resistor in series with the capacitor so that its decay would take longer. But that either made the capacitor never reach the desired voltage. or didn't slow the decay enough. also the larges cap I had on hand was a 1000uF 25v.

     

    The other thing that I noticed this way is that I am now under-volting the board by going through the transistor. I went ahead and picked up two different boost converters. A 5v @ 1A (https://www.adafruit.com/product/4654 ) and a 5v @ 100mA ( https://www.adafruit.com/product/3661  ) both have the enable pin that I believe you are referring too.

     

    I toyed with using the enable pin on the itsybitsy, but that doesn't cut power to the vHi pin which I am using elsewhere in the circuit, which would leave stuff on.

     

    here is the schematic of where I have gotten too. I am gonna take a look at what you drew up. again I took some time from this to try and get a fresh take on it.

     

     

    image

     

    Also, THANK YOU to all. this has been the most helpful forum post I have ever been a part of!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • genebren
    0 genebren over 6 years ago in reply to justphred

    Michael,

     

    Here is a crude attempt at a drawing of a circuit that might work for you.  I found another Adafruit part (#1903) that might help you.  This should allow to prototype your project and see how it works.

    image

    I could see that you were struggling a bit trying to understand how the pieces connected, so hopefully this will clear things up.  There are three Adafruit modules and here is how they connect:

     

    1. Adafruit 2124 - Charger -  5 volts connect to the module at 5V and GND and are used to charge the Li-Ion battery.  The battery voltage (BAT) connects to the switch and to the VBAT terminal of the Boost module (1903).
    2. Adafruit 1903 - Boost - The Enable pin (EN) is driven high by the momentary switch (from VBAT) or from the Adafruit 3800 (ItsyBitsy) to turn on the Boost Circuit.  The output 5.0V provides power to ItsyBitsy.
    3. Adafruit 3800 - ItsyBitsy - Power from the Boost is applied to the VBAT pin (power input). D11 (or any other Dx pin) is used to hold the boost on (high), or to shut it off (low).  A1 is used to sample the switch output to see if it is pressed or not (for user interface functions or to turn off the unit).
    4. Misc parts.  - Diode - this is used to prevent voltage applied by the ItsyBitsy (holding power on) from attempting to charge the battery.  The two 100K resistors are scaling the voltage at the switch output (from 4.2 - 2.5V down to 2.1 to 1.25V so that they will be in the proper ranges of the ItsyBitsy ADC input (< 3.3V).

     

    Hopefully this will be a little clearer of a picture in how things could be interconnected.  Please keep in mind that I have not used any of these modules, and only quickly reviewed the documentation, so some of this may require a bit of tweaking to get it all correct.

     

    Good luck and have fun!

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer