Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Legacy Personal Blogs

Please Note:

This blog contains the legacy personal blog posts of our members, other than our Top Members whose content has been migrated into individual blogs in this area. Our new platform does not have personal blogs so this is how we have preserved the personal blog posts of our members from the Jive platform. No new posts will be permitted in this blog. Instead, if you wish to create blog content, please post it in the blog in the most appropriate topic area.

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Transistors: Output Characteristic Curves

    jc2048
    jc2048
    This one is similar to what I did with the gain, except that this time I kept the base current constant and measured the collector current in relation to the collector-emitter voltage. I reworked the original test circuit, which is how this blog foll...
    • 27 Mar 2017
  • How one electrical passive element can cause issue

    kk99
    kk99
    Few days ago I got TV with following issue: there is no way to power on TV (only standby LED is on). I have checked that all voltages on IP board (power supply and inverter) were correct. Next I have checked key elements on main board. After analyze ...
    • 26 Mar 2017
  • Transistors: Current Gain (Beta or hFE)

    jc2048
    jc2048
    Another 'Transistors' blog. I thought this one would be easy, but it turned out to be quite challenging and, in some ways, a bit of a failure. The current gain of a bipolar junction transistor (when the emitter is the common terminal bet...
    • 24 Mar 2017
  • Getting Started with PADI IOT Stamp module from Pine64 | AT Commands

    oksbwn
    oksbwn
    www.youtube.com/watch  The IoT Stamp module is powered by Realtek RTL8710AF ARM Cortex M3 WiFi SoC running at 83 MHz. This module features same form factor and GPIO layout as of ESP8266 but lacks ADC input.But it featuresUp to 1x SPI @ 41.5...
    • 23 Mar 2017
  • Archery timer prototype

    WarrenW
    WarrenW
     This is the remote end. Still need to connect the radio links and test them, I have been concentrating on the code for the rest of the timer first.Simple 1602 dual line 16 character display, using a ptotboard shield for easy soldering, 4 x 4 ma...
    • 22 Mar 2017
  • Progress on archery timer

    WarrenW
    WarrenW
    Hi All,Looks like I am making progress on my archery timer.I have flags se for the traffic light indicators and a pre-timer countdown prior to the start of the shoot. Then the main timer kicks in and changes the traffic lights and sounds buzzers etc....
    • 21 Mar 2017
  • Innovative Light-Responsive LEDs

    rohm_eu
    rohm_eu
    This dual-functioning nanorod LEDs can simultaneously emit and detect light. Therefore they could bring us one step closer to the next-generation of smart device displays.  Cell phones and other devices with light-responsive LED displays will so...
    • 21 Mar 2017
  • Microchip and 50 click board in 50 days

    koudelad
    koudelad
    Hello,I noticed there is a new event combining Microchip's  PICs and click boards from MikroElektronika.https://www.mikroe.com/50-in-50-with-microchip-everything-you-need-is-just-a-click-away/?utm_source=homepage&utm_campaig… 50 project in 5...
    • 20 Mar 2017
  • Simple Automatic Threshold Generation for Embedded Systems

    satyavrat
    satyavrat
         Very often it so happens in sensing-actuation based projects that an embedded system must take a certain action when the value of a sensed parameter is above a certain threshold. The most basic method of handling such a contr...
    • 20 Mar 2017
  • Arduino basics 101: how to use analog pins

    charlie_marks
    charlie_marks
    Hello people of the interweb! In this post i shall be explaining what analog pins are and how to us them. To start things of what is an analog pin? An analog pin can be used to read analog data such as a potentiometer, however  they can also be ...
    • 19 Mar 2017
  • casus telefon

    e14 Contributor
    e14 Contributor
    E-CASUS.COM iphone ANDROID  casus telefon dinleme SOSYAL MEDYA ve WHATSAPP telefon takip programlari ile casus yazilim, dinleme cihazlari CASUS TELEFON DINLEME VE TELEFON TAKIP PROGRAMI ILE CASUS YAZILIMLARI  Yazılım, Whatsapp Wiretap, İzle...
    • 18 Mar 2017
  • History of Galveston, Texas

    chelsiebelinco
    chelsiebelinco
     The History of Galveston, Texas, begins with the archaeological record of Native Americans who used the island. The first European settlements on the island were constructed around 1816. The Port of Galveston was established in 1825 by the Cong...
    • 17 Mar 2017
  • DIY Soldering Station Part 3

    adsicks
    adsicks
    I made the clamp to hold my extra pair of hands in place yesterday. It took about an hour.  I started out measuring the base of my hands and making a 3D model in OpenScad. To start my cuts I set my blade to take out approximately half of th...
    • 16 Mar 2017
  • TI SimpleLink MCU Platform is released

    jomoenginer
    jomoenginer
    TI has updated their SimpleLink offerings to bring the SimpleLink MCU Platform where the SimpleLink devices will be converged under a single platform and share the same tools across each device in the platform. SimpleLink MCU Platform This ...
    • 16 Mar 2017
  • DIY Soldering Station Part 2

    adsicks
    adsicks
    I got the lip glued onto my base. The most important thing to remember when clamping and gluing lap joints is to clamp them on all three axes. I started by sanding The side pieces I cut. I just used 80 grit sandpaper and a hand sander. The idea ...
    • 15 Mar 2017
  • Optimization for ARM Processors

    msimon
    msimon
    Embedded systems have various types of the processors which range from 8-bit family to 64-bit family, from 32 bytes to a few gigabytes of RAM and, from kilohertz clock source to a few gigahertz clock source. When the resources of the processor are in...
    • 14 Mar 2017
  • DIY Soldering Station Part 1

    adsicks
    adsicks
    Having an organized work area is a must when working with electronics. Having an extra pair of hands and plenty of light is also essential. This is why after looking at DIY workstations built by many other electronics enthusiasts I decided to build m...
    • 14 Mar 2017
  • Oulu 3D Sensor Game Jam 2017

    rohm_eu
    rohm_eu
    The Oulu 3D Sensor Game Jam 2017 is a global game jam event taking place in the City of Oulu, Finland. This event is a hackathon focused on making a working game prototype using 3D sensors such as accelerometer, gyroscope, magnetometer, pressure sens...
    • 13 Mar 2017
  • tempus fugit

    beacon_dave
    beacon_dave
    tempus fugit - time flies Joined the Element14 community one year ago today...
    • 13 Mar 2017
  • PID on a EK-TMC4C123GXL Evaluation Board. Part 2: The Hardware.

    jc2048
    jc2048
    Part 1 can be found here: PID on a EK-TMC4C123GXL Evaluation Board. Part 1: Getting started.  At this point I had to decide what to try and control. I wanted something that would be slow enough that the processor could keep up, but fast eno...
    • 11 Mar 2017
  • Breadboard BoosterPack Sidekick for TI LaunchPad

    jomoenginer
    jomoenginer
    This looks like a nifty tool to have when working with TI LaunchPads.  The Breadboard BoosterPack is a break-out board that plus on to the LaunchPad from either the top or the bottom of the board providing access to the LaunchPad pins even when ...
    • 11 Mar 2017
  • PID on a EK-TMC4C123GXL Evaluation Board. Part 1: Getting started.

    jc2048
    jc2048
    When jancumps introduced us to the PID library (link below) I said I'd have a go with it, since I had a TI evaluation board (an EK-TMC4C123GXLwith a Tiva TM4C123G on it), wanted to learn a bit about ARM coding, and thought that running a control ...
    • 11 Mar 2017
  • I received the radio links

    WarrenW
    WarrenW
    Well the archery timer has taken on a new phase with more hardware arriving.2 Nordic NRF24L modules to play with. These have the power amp and stub antenna.I might need to boost the power supply stability a bit with a dc - dc converter as I don't thi...
    • 10 Mar 2017
  • Meccano 2.0 with 2.0 many serv.0s

    kayoteq
    kayoteq
    Hello, figured you need a good overview of my sense of metering reality. AKA "My first humanoid form factor robot" the plastic pal who's fun to be with.www.youtube.com/watch
    • 9 Mar 2017
  • Seven segment and arduino

    idanre1
    idanre1
    I have bought a 4 digit seven segment module on banggood.1 Pcs 0.561 Pcs 7-Segment 4 Digit Super Red LED Display Common Anode Time - US$1.79these things cost about 2$ and i wanted to test if they worth anything. I have decided to connect them to...
    • 7 Mar 2017
<>