Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) APPCRASH EAGLE 6.4 on WIN 7 64
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 195 subscribers
  • Views 5061 views
  • Users 0 members are here
  • eagle
Related

APPCRASH EAGLE 6.4 on WIN 7 64

terje
terje over 13 years ago

Dear the support team at Cadsoft!

I have just purchased and installed Eagle pro shematic and layout package on to my brand new win 7 64 computer.

 

I'm now trying to design some new components with the library editor but every 3 to 10 minutes the application crashes and the work is lost.

To me it appears that the crash happens randomly. It can happen when I'm resizing the window, moving a element, copy a element, changing the grid. pushing the undo button  etc. etc.

For now the Eagle is useless as this happens too frequently.

 

The eagle program is installed under C:\eagle

The version is 6.4.0.

 

What did I do wrong?

 

Is this a known issue?

 

 

 

Windows crash report:

 

Problem event name: APPCRASH

Programname: eagle.exe

Programversion: 0.0.0.0

Timestamp for program: 50eaf0df

Error module name: ntdll.dll

Error module version: 6.1.7601.17725

Timestamp on error module: 4ec49b8f

Exeption code: c0000005

Exeption scew: 0002e3be

OS-versjon: 6.1.7601.2.1.0.256.48

ID for national setting: 1044

Additional information 1: 0a9e

Additional information2: 0a9e372d3b4ad19135b953a78882e789

Additional information3: 0a9e

Additional information4: 0a9e372d3b4ad19135b953a78882e789

 

 

 

Best Regards

Terje

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to auspoundy

    On 2/26/2013 10:18 PM, Brett Pound wrote:

    This is NOT an x64 vs x86 64-bit/32-bit issue. The app has worked reliably in 6.3.0 on x64 so I strongly feel it's something that has changed in 6.4.0 that is causing the instability.

     

    I too have moved my projects and libraries to a different location. It is on a different logical partition on the same physical hard drive - it's a laptop so it's not network connected.

     

    One of the real issues here that Cadsoft should be taking into account here is that the "user data" store should not default to be inside the program files directory. That's the reason people change these locations - and that's why they should make that a part of the design.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/70845#70845/l/re-appcrash-eagle-64-on-win-7-64

     

     

    Hi Brett and others,

     

    Let's try to troubleshoot this. Reply with a detailed and exact

    description of what you do to create the crash. We have a Windows 7

    laptop here in the office with EAGLE installed on which I could try to

    recreate the issue. If I can recreate it, then I will pass it on to our

    developers and this will be fixed for the next update.

     

    Be as detailed and specific as you can mention any relative conditions

    in a step by step manner.

     

    Thanks everyone and we'll get this solved soon.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • auspoundy
    auspoundy over 13 years ago in reply to e14 Contributor

    This is NOT an x64 vs x86 64-bit/32-bit issue. The app has worked reliably in 6.3.0 on x64 so I strongly feel it's something that has changed in 6.4.0 that is causing the instability.

     

    I too have moved my projects and libraries to a different location. It is on a different logical partition on the same physical hard drive - it's a laptop so it's not network connected.

     

    One of the real issues here that Cadsoft should be taking into account here is that the "user data" store should not default to be inside the program files directory. That's the reason people change these locations - and that's why they should make that a part of the design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Considering the number of applications out there (Photoshop, Sony Vegas Pro

    etc.) that are going to 64 bit only, having to switch back to 32 bit is

    hardly a "handy" solution these days (although I do dual boot into XP Pro

    32 if I want).  My wife won't let me have a separate computer for each

    application though ...

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    I hope your problem really does go away in the Win64 if you run in 32-bit mode, but I would be very careful and not count on it.  My computer is a 32-bit machine and it is having crashing issues with version 6.4 too.  Version 6.3 is still working fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to Krycek

    TO ALL:

         The problem is with all 32bit programs running within the 64bit Windows. Change from 64 to 32 and probelm solved. From the day Windows XP was avalilable in 32bit and 64bit mode, it has been a problem. And it has not been solved.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Krycek
    Krycek over 13 years ago

    I am having the same problems using 6.4.0 under Windows 7 64 bit.

     

    First I could get the app to crash while editing text properties in the schematic editor but now I have just lost a lot of work in the library editor when editing the properties of a plated through hole drill size when modifying an existing part.

     

    When I booted Eagle 6.4.0 back up it had lost the working directory I use as well as where my libraries are stored and reverted back to defaults.

     

    My projects and library files are saved on a network drive and have been since I first started using Eagle at version 6.0 so its not that - I have reverted back to 6.3 so I can continue working on an urgent project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • auspoundy
    auspoundy over 13 years ago in reply to auspoundy

    As an aside, I uninstalled 6.4.0 and then reinstalled it,no change in status - open an existing board or a new board, change layer on a text object, bam.

    I then uninstalled 6.4.0 and installed 6.3.0 and the same action now works, so I'm leaving it this way.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • auspoundy
    auspoundy over 13 years ago in reply to auspoundy

    Hi anyone from the CadSoft team.... is this the right way to register this as an issue?  Any other suggestions on how to get working? Uninstall/reinstall of 6.4.0 didn't help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • auspoundy
    auspoundy over 13 years ago

    I have crashing in 6.4.0 as well.

     

    I am not running on Windows 7, but am on Windows 8 (x64).

     

    I can repro the crash relatively easily.

     

    Open a new schematic. Drop a couple of parts on the schematic. Doesn't seem to matter what, really.

     

    Go to board view.

     

    Add text. Type something. Drop it on the board twice.  Escape, escape to get out of text mode.

     

    Get info of one of the text objects. Change it from whatever layer it was on to tPlace (or any other layer really - in fact you don't need to change anything in this dialog.  Click OK.

     

    App crashes.

     

     

    Faulting application name: eagle.exe, version: 0.0.0.0, time stamp: 0x50eaf0df

    Faulting module name: eagle.exe, version: 0.0.0.0, time stamp: 0x50eaf0df

    Exception code: 0xc0000005

    Fault offset: 0x0025bc77

    Faulting process id: 0x25e8

    Faulting application start time: 0x01ce114d2e13ba7d

    Faulting application path: C:\Program Files (x86)\EAGLE-6\bin\eagle.exe

    Faulting module path: C:\Program Files (x86)\EAGLE-6\bin\eagle.exe

    Report Id: 4d071fc6-7d42-11e2-be8d-f0def1a60605

    Faulting package full name:

    Faulting package-relative application ID:

     

    I can probably capture more info if the team can tell me what you want. 

     

    As you can guess, this is a pain to work around.  Having to place the item in question on the right layer from the outset is a drama, particularly when you want to copy an existing item to the other side of the board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to terje

    Hi, I also just encountered this problem with version 6.4.0  I emailed tech support and Jorge Garcia responded and mentioned moving my user libraries and projects like he did for you.  I tried this and it did not help.  I'm using Windows 7 Pro 32-bit.  My computer at home is the main problem.  I can crash the program on it easily.  I have re-installed the program and still have the same problem.  I even uninstalled all older versions to make sure nothing was interfering.  My problem seems to be related to the buffer that the program uses to store copied items to.  For example, when you want to move several items, you but a box around them to select them and then can copy and paste.  If you forget to choose items and then click on Paste, it usually pops up a little window telling you that the buffer is empty and you can clear that and try again.  This program is not doing that on my machine.  If I try and copy anything or just click paste, either way, the program just shuts down without any notice. 

     

    Right now, I've got version 6.30 installed and it is working fine on both computers with all libraries and projects in subfolders under the Eagle directories that are created by the installation program.  I can't seem to get version 6.40 to work.  It is working at my office, but I'm scared of it.  It crashed on me once there too the other day and I wondered why because I had never had this program do this.  Now after my experience at my home computer, I've decided to use version 6.3 until I can get someone to help figure out what is going on.

     

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>