Rohde & Schwarz
  • Products & Partners
  • Manufacturers
  • Rohde & Schwarz
  • More
  • Cancel
Rohde & Schwarz

Blog

  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Rohde & Schwarz to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Power supply control loop response measurements with a R&S oscilloscope

    rohde&schwarz
    rohde&schwarz
    A well compensating voltage controller enables stable output voltages and reduces the influence of load changes and supply voltage variations.  Why are control loop response measurements important?The quality of a control circuit determines the ...
    • 30 Sep 2020
  • Power Consumption Analysis

    rohde&schwarz
    rohde&schwarz
    The world is getting more and more connected. Myriads of sensors and IoT applications factories and households, enabling optimal industrial operation and contributing to improvement of the social welfare.  Maximizing battery lifetimeMany of thes...
    • 22 Sep 2020
  • 5 techniques for fast, accurate power integrity measurements

    rohde&schwarz
    rohde&schwarz
    What is power integrity?Power integrity is the assurance that power applied to a circuit or device is appropriate for the desired performance of the circuit or device.Such sensitive electronic designs require modern test solutions. When measuring pow...
    • 8 Sep 2020
  • Power Integrity Testing

    rohde&schwarz
    rohde&schwarz
    The power delivery network distributes and delivers the DC power to all active components on the board. Disturbances on power rails can cause serious impairments in the performance of the used ICs and the overall system, so power integrity is a param...
    • 24 Aug 2020
  • Electronic design: efficient analysis of power and signal integrity

    rohde&schwarz
    rohde&schwarz
    Modern electronic designs increasingly integrate more functionality into less space. At the same time, processor speeds, clock and data rates are rising while signal levels are decreasing. All these developments result in a growing need for testing a...
    • 18 Aug 2020
  • Deep memory: history and segmented memory option

    rohde&schwarz
    rohde&schwarz
    What is your challenge?Embedded designs are an integral part of today’s electronic systems comprising analog signals as well as signals from serial and parallel buses. When debugging such designs, a common challenge is to simultaneously capture enoug...
    • 27 Jul 2020
  • The importance of deep memory in oscilloscopes

    rohde&schwarz
    rohde&schwarz
    Why does deep memory in an oscilloscope matter? In brief, deep memory ensures that long waveforms are captured in high resolution with all needed signal details thanks to a high sustained sample rate.Acquisition memory depth, equals the number of sam...
    • 20 Jul 2020
  • Emulate real-world scenarios with R&S power supplies

    rohde&schwarz
    rohde&schwarz
    Modern circuitries require different voltage and/or current levels in different operating states. For example, when simulating a startup sequence of an embedded system specialized voltage and current profiles synchronized across several channels are ...
    • 7 Jul 2020
  • Logging & charting tool for R&S power supplies

    rohde&schwarz
    rohde&schwarz
    Let’s learn more about the logging and fast logging functionality of R&S®︎NGM and R&S®︎NGL. The associated application program provides charting functionality for logged voltage, current and power values. Standard loggingStandard logging r...
    • 3 Jul 2020
  • Testing battery management systems (BMS) with R&S power supplies

    rohde&schwarz
    rohde&schwarz
    The importance of battery lifetimeRechargeable batteries used in battery-powered devices and vehicles need to be stimulated, measured and tested. Overcharging and deep discharging reduce the lifetime of rechargeable batteries. Defects could lead to o...
    • 23 Jun 2020
  • Power Converter Efficiency: Measuring Efficiency with highest Accuracy

    rohde&schwarz
    rohde&schwarz
    Efficiency is often the key factor in power converters, where efficiencies above 90% are required. This is true for battery operated IoT devices to get the most out of the battery, and it is also true for small DCDC converters supplied by a DC rail. ...
    • 9 Jun 2020
  • Simplify railway field maintenance with R&S®︎Scope Rider RTH user apps

    rohde&schwarz
    rohde&schwarz
    Oscilloscopes are everyday instruments for engineers and electricians. Maintenance tasks, however, sometimes require very specific measurements that are not available as standard functionality or are difficult to set up manually. For instance, the R&...
    • 25 May 2020
  • Different trigger types for faster debugging

    rohde&schwarz
    rohde&schwarz
    The correction of a bad circuit can be difficult with conventional edge triggers because the error state cannot be selected precisely. That is the reason why modern oscilloscopes offer various digital triggers that are specialized to address specific...
    • 18 May 2020
  • How to make basic voltage vs. time measurements using an oscilloscope?

    rohde&schwarz
    rohde&schwarz
    Oscilloscopes are widely used for electrical designing as well as for testing and debugging almost anything that runs electricity. They are primarily used to measure and display voltage versus time for periodic or repeating waveforms. Modern oscillos...
    • 18 May 2020
  • Boost your efficiency with quadcore power!

    rohde&schwarz
    rohde&schwarz
    The new era of performance power supplies from Rohde & Schwarz has now begun with the launch of the R&S®︎NGP800 series. These power supplies are designed for versatile applications. They are ideal when speed and advanced programming features a...
    • 18 May 2020
  • EMI Debugging with Spectrum Analyzers

    rohde&schwarz
    rohde&schwarz
    Precompliance, as well as debugging tests, are most commonly done with the help of a spectrum analyzer or an oscilloscope. The approach and diagnostic techniques of oscilloscopes were discussed in the last blog post. Testing Setup This arti...
    • 13 May 2020
  • EMI Debugging with an Oscilloscope

    rohde&schwarz
    rohde&schwarz
    Benefits of using an oscilloscope Oscilloscopes are the workhorses for power electronics engineers. With powerful and easy-to-use FFT analysis capabilities, their application fields extend to EMI debugging – and that saves a lot of time and mone...
    • 13 May 2020
  • EMI Debugging & Pre-compliance Tests: Oscilloscope or Spectrum Analyzer?

    rohde&schwarz
    rohde&schwarz
    Different test equipment for EMI testsEMI debugging revolves around a simple idea – to have a convenient and affordable setup that can be used during product design for verification and early detection of potential problems. Each step of the product ...
    • 13 May 2020
  • EMC & EMI Pre-compliance Testing

    rohde&schwarz
    rohde&schwarz
    What is EMC and why is it important?Electromagnetic compatibility (EMC) testing is a critical part of any product development journey. EMC is strictly regulated by development and production standards to ensure products’ safe operation next to other ...
    • 13 May 2020