PCB Design, Prototyping and Production
  • Products
  • More
PCB Design, Prototyping and Production
PCB Blogs Create a custom footprint in KiCad 7 - 2b: create the footprint for an SMA coax connector with the editor - copper pour, solder mask clearance, holes, pads
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 21 Jan 2023 7:10 PM Date Created
  • Views 4704 views
  • Likes 12 likes
  • Comments 8 comments
  • kicad
  • footprint
  • pcb
  • amphenol
  • SF2921-61506
  • SF2921-61506-1S
Related
Recommended

Create a custom footprint in KiCad 7 - 2b: create the footprint for an SMA coax connector with the editor - copper pour, solder mask clearance, holes, pads

Jan Cumps
Jan Cumps
21 Jan 2023
Create a custom footprint in KiCad 7 - 2b: create the footprint for an SMA coax connector with the editor - copper pour, solder mask clearance, holes, pads

Part 2b of the exercise to create a custom footprint for the Amphenol /  SV Microwave SF2921-61506-1S   SMA coaxial connector. In the previous post created the initial footprint boundaries. Now: the rest.

image

Copper pour and the pads

I first drew a theoretical - good enough - outline on the silkscreen.

image

It will have to go later, because the whole area will become exposed copper plane. But for now, it's a good guideline for the other activities:

  • copper plane and solder mask clearance should at least cover this area
  • it shows the centre of poth drill holes, and for the centre pin

I then drew the 2 pours with a polygon:

image 

and SMD pads:

image

When you right - click a pad, select Edit as Graphical Shapes, then click again and end that mode, all copper that touches the pad becomes "pad". So I end with two copper polygons that have PAD number 1 and 2. I also put 2 keepout areas on the copper  layer:

image

On the front courtyard layer, I drew the real estate that should be respected (purple rectangle in the first image)

Mask clearance

I then put a filled polygon on the front mask, similar to the main copper pour outline. This allows the connector base to sit flush on the plane.

image

I added a little clearance on the side where the microstrip exits the connector. This as a hint for the PCB designer that the whole microstrip area should be maskless.

Drill holes

Easy. Because I had the centers on silkscreen , I just had to put pads on those locations. I removed their number, made the copper size 0 and the drill size the correct one for a 0-80 UNF-2B bolt: 

image

3/64, according to the internet, is a 0.05 inch hole.

image

That's it. The result is this:

On a PCB :

image

In 3D view (using the image I downloaded in the very first post):

image

image

Blog Index

  • Overview: Amphenol / SV Microwave SF2921-61506-1S SMA coaxial connector series
  • Amphenol / SV Microwave SF2921-61506-1S SMA coaxial connector: behavior under vibration
  • Create a custom footprint in KiCad 7 - 1: collect info and component details
  • Create a custom footprint in KiCad 7 - 2a: create the footprint for an SMA coax connector with the editor - initial outline
  • Create a custom footprint in KiCad 7 - 2b: create the footprint for an SMA coax connector with the editor - copper pour, solder mask clearance, holes, pads
  • Use a LibraryLoader Footprint in KiCad 7
  • Sign in to reply
  • Jan Cumps
    Jan Cumps over 3 years ago

    Snippet from the video on the Farnell product page:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to Jan Cumps

    Such is life, currency is quite valuable!

     image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to scottiebabe

    Soon enough your going to have your RF wizards hat!

    I should team up with my brother. He's a civil engineer with specialisation in high frequency and antennas.
    Just like me he sold his soul and is doing corporate software management :).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago

    photo of the actual base:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to shabaz

    I gave it a little :) - 1,52. Bigger than the hole in the 3d model.

    This is the view of my footprint top, and yours bottom, seen from the bottom layer. You can see the holes of the connector through the holes.

    image

    In my initial design, they were exact the same. If wrong, I'll have to take out the drill :).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>