Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi PoE (Power Over Ethernet) Hat
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 13 Mar 2018 1:45 PM Date Created
  • Last Updated Last Updated: 19 Jun 2020 12:12 PM
  • Views 12793 views
  • Likes 13 likes
  • Comments 41 comments
Related
Recommended

Raspberry Pi PoE (Power Over Ethernet) Hat

image
NEW! Raspberry Pi 3 Model B+

Technical Specifications | Compliance Documentation | GPIO Pin Out | Unboxing Video | Benchmark Tests | Frequently Asked Questions | Comparison Chart | Pi PoE Hat | Pi Accessories | Pi Projects

 

Boot and power your Raspberry Pi 3 B+ or 4 over Ethernet.

 

imageimage

Buy NowBuy NowBuy Now

 

The official Power over Ethernet (PoE) add-on board for the Raspberry Pi 3 Model B+ or Raspberry Pi 4! Use this HAT to power a Raspberry Pi via an Ethernet cable, removing the need for a separate power supply, an ideal solution for embedded and IoT projects. For Raspberry Pi 3 Model B+ and onwards, an 802.3af compliant POE injector, switch, or router device is required (not included).

 

  • Power over Ethernet 802.3af compliant
  • Power over Ethernet Boot (PXE Boot)
  • Class 2 device
  • Fully isolate Switched-Mode Power Supply (SMPS)
  • 36-56V Input Voltage
  • 5V Output Voltage
  • Supplies up to 2.5A
  • Fan Control
  • Plug-and-play compatibility with Raspberry Pi 3 Model B+ or Raspberry Pi 4

 

Best of all, it fits within the official Raspberry Pi Case!

An Alternative Product: Buy NowBuy Now

  • power over ethernet
  • rpi4
  • 3b+
  • raspberry pi 4
  • poe
  • raspberry pi 3 model b plus (b+)
  • power_over_ethernet
  • rpi3b+
  • 4
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 8 years ago +6
    It does seem that this has been designed for the single purpose of powering the RPi over Ethernet. They have provided access to the camera and display connectors, which is nice. HOWEVER the GPIO has been…
  • e14phil
    e14phil over 8 years ago in reply to balearicdynamics +5
    Hey Enrico, This will provide the Pi with its 5V 2.5A needed as if it were plugged into the official power supply. More info about upcoming roadtests and more information on the PoE board will be released…
  • dhussenet
    dhussenet over 8 years ago +4
    Hi Everybody. I'm sorry but it will not use the 40pin GPIO connector. Power is taken directly on the RJ45 connector, and on the Pi3 B+, there's a new 4pin connector (close to the USB connectors) called…
  • hansamann
    hansamann over 8 years ago

    So I plan to use the PEO hat for a hobby project but I need to connect a pi camera (should be no issue) and I need to have access to the

    GPIO pins. What is the recommended solution to get that done? Will the 40 pin stackable header work painlessly (e.g. not make the pin plastic bottom stand out too high and make connection to the PEO header painful)?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • troyfontaine
    troyfontaine over 8 years ago in reply to richardhh

    I spoke with someone at Newark Canada about a month ago-they wouldn't even estimate on the wait time....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • richardhh
    richardhh over 8 years ago

    So... ETA?

     

    Somewhere, I'd seen that it was targeted to start shipping from Newark / Farnell about a week ago.  Waiting with baited breath...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • pylonsoft
    pylonsoft over 8 years ago
    This comment was deleted.
    • Cancel
    • More
    • Cancel
  • richard_damon
    richard_damon over 8 years ago in reply to rew

    Power over Ethernet uses the fact that the signals are defined to have transformer isolation one each pair. With POE, the voltage is applied between the center taps of the pairs.

     

    You need the transformer coupling because the devices on the two ends likely have differing ground references, so you need the transformers for isolation anyway. By applying the DC bias to the center taps, POE is largely transparent to the data transmission.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cinderblock
    cinderblock over 8 years ago in reply to dhussenet

    dhussenet  wrote:

     

    Hi Everybody. I'm sorry but it will not use the 40pin GPIO connector.

     

    Power is taken directly on the RJ45 connector, and on the Pi3 B+, there's a new 4pin connector (close to the USB connectors) called PoE. So, 2 pins for the input voltage from the RJ45 connector (35-56V tolerant I think, so conform with 48V of the 802.3af), and 2 pins for the output voltage (5V@2.5A max)

     

    The HAT will be connected to this connector to do the job, leaving the 40pin connector completely free

    As much as I'd like this to be true, this is incorrect. Each of the 4 new pins is connected to one twisted pair of the RJ-45. So you still need to use some of the pins of the 40-pin header or the input USB to provide power to the PI. I've verified this with a multimeter.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • nenner
    nenner over 8 years ago

    woops we did measure again

    the 4 pins connect to regular rj45 input, good tomake our own poe input

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • aspork42
    aspork42 over 8 years ago

    I'm a little sad that this doesn't appear to support Ad-Hoc POE (unless I'm mistaken).

    I use this midspan injector to run stuff at my house.

    image

     

    Unless I'm mistaken - could the 4-pin header be used to just run a regular voltage regulator to step down, say 12VDC to a decent 5VDC back to the board?

     

    The other reason for this is that the Pi has lots of power conditioning on-board and doesn't have any "VIN" pin available on the header. I've done projects where I'd like to bring power in via a Hat or perma-proto board (like in ad-hoc POE) but then I lose out on all the power regulation.

     

    I'll have to do some more research to find out...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • nenner
    nenner over 8 years ago

    i did not do it myself, needs a double check

    shall let you know

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bernhardmayer
    bernhardmayer over 8 years ago in reply to nenner

    Hi Thomas,

    how did you measure?

    I checked with my Raspberry Pi 3B+ and there all 4 pins are connected to the pins of the RJ45 connector.

    Bernhard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>