RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs Analog Discovery 3 - Neat Enclosure
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: dougw
  • Date Created: 31 Dec 2023 9:22 PM Date Created
  • Views 3896 views
  • Likes 15 likes
  • Comments 17 comments
Related
Recommended
  • dougw
  • AD3 enclosure
  • BNC Adapter
  • Digilent Analog Discovery 3

Analog Discovery 3 - Neat Enclosure

dougw
dougw
31 Dec 2023

Intro

I am road testing a Digilent Analog Discovery 3 which included a BNC Adapter accessory module. The adapter connects to the Analog Discovery module via a 30 pin header, but there are no other mechanical fasteners to stabilize the connection. BNC cables are usually stiff enough to create stress on the header connection so I designed a chassis to mount both modules and stabilize the connection.

Enclosure Image

image

Design Features

  1. Shelters exposed PCB and connections from accidental touching and ESD
  2. Provides mechanical stability between the modules
  3. Prevents random metal objects from accidentally shorting pins on the pass-through 30 pin connector
  4. Prevents the pass-through connector pins from getting bumped and bent
  5. Retains visual access to labels on the main module
  6. Holds the 2 modules rigidly in optimal mating positions
  7. Provides clear labels for the BNC connectors
  8. Provides access to the configuration jumpers without any disassembly
  9. Provides easy access to the pass-through logic analyzer pins without any disassembly
  10. Provides non-slip feet that prevent the device from slipping around on the bench
  11. Provides clearance under the BNC connectors to allow adequate finger access to operate BNC connectors
  12. The case is a snug fit and quick to assemble
  13. Matches the black color scheme while still exposing the green side walls
  14. Provides the system with a robust, functional, "finished product" aesthetic

Enclosure Video

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Discussion

I put some significant thought into designing an appropriate enclosure for the AD3 and BNC adapter assembly and it paid off with a very functional system that meets all my design criteria.

I am very pleased with the way it turned out. It definitely makes the AD3 into a more useful instrument.

AD3Case .stl files

DigilentAD3stl.zip

Links:

AD3 Unboxing

 Pretty Cool Raster Text Display on an AD3 

AD3 Enclosure

AD# - Frequency-to-Voltage Converter

AD3 - Capacitance-to-Voltage Converter

My Road Test of the Analog Discovery 3

Digilent Analog Discovery 3 road test page

Digilent AD3 page

  • Sign in to reply
  • dougw
    dougw over 2 years ago in reply to baldengineer

    Sure, I'll post the stl files, but I am making a few touch-ups to the design. I works great as built, but  I had to make a couple of manual trims to get it to fit well. Also I have to find the part number for the rubber feet. And of course I need to get on with the actual road test....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 2 years ago

    So... can I ask the obvious question...

    Are you going to share the files for your awesome enclosure?

    If I had kept the AD3, I would definitely want one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<