Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog MAX32660 Evaluation Kit - part 1: IDE install and Build First Example
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 9 Dec 2018 5:04 PM Date Created
  • Views 6684 views
  • Likes 7 likes
  • Comments 13 comments
  • RoadTest
  • max32660
  • maxim
  • road_test
Related
Recommended

MAX32660 Evaluation Kit - part 1: IDE install and Build First Example

Jan Cumps
Jan Cumps
9 Dec 2018

I'm road testing the  Ultra-Low Power Arm Cortex-M4 Darwin MCU EVM.

In this blog post (I don't have the hardware yet): Trying if I can use Maxim's Eclipse bundle.

image

Maxim hasn't altered Eclipse, but they provide an install that sets up a fully working environment with debugger and examples.

Here's my real-time blog about the first experience.

 

 

Eclipse as IDE

 

The Maxim Webinar: What Can You Do With the World’s Smallest ArmRegistered CortexRegistered M4 with FPU Microcontroller?  discusses mbed (on- and offline), Arduino and Eclipse as the three free environments of choice.

I prefer to have an IDE with fully integrated build and debug functionality (and with version control integration). For me personally, Eclipse is way ahead of the two others on those fronts.

 

image

source: element14 webinar

 

The controller's homepage has a link  to the toolchain installer, for Windows and Linux..

That installs (I tested the Windows version) Eclipse, the GDB OpenOCD debug plug-in (what a great open source development !!),

USB driver, compiler chain (with MiniGW supporting the build).

And it installs firmware libs, example projects and documentations for our microcontroller.

 

Once installed, everything works out of the box - just execute eclipse.bat, not eclipse.exe.

The install is so kind to not put any of the modules in your standard path (thank you Maxim !!) .

The batch file takes care that the environment (e.g. MiniGW) is configured before Eclipse starts.

(it would be good if Maxim documented that in the Eclipse Quick Start guide - it prevents compilation errors).

The overall experience is perfect. Installation works as it should.

After importing the first two examples - one bare metal, one with FreeRTOS - they both compiled without errors and warnings.

I used the instructions for another controller in the family.

 

Examples

 

Maxim has a set of examples for this controller. Most of them show how the peripherals work. Very practical, and I'll review them.

But they should 'just work as per spec'.

 

More interesting are the low power example and the RTOS project.

These two can reveal how the device compares to others out there - in the same low power niche.

I'll also focus on the DMA, Real Time Clock and watchdog examples because they are device specific.

 

Out of curiosity, I'd also like to investigate the 'Instruction Cache' example.

I've seen the option with other controllers.

But I never saw an example that compares execution times on an ARM controller with instruction cached enabled vs disabled.

 

image

 

A little gripe: when you add new source files or folders to the project, you have to edit the Makefile.

This is not Eclipse-like. You are expected to just add sources and source folders and everything works automatically. You can use the exclude option to  not add files to a build.

Other manufacturers that have an Eclipse flavour comply with that natural Eclipse use.

 

image

It's not a big deal but it's a hurdle.

It makes the learning ramp unnecessary steeper if you haven't stumbled on this comment (written for another device, not available from the MAX32660 homepage).

 

edit: one example - Instruction Cache Example - fails to compile, because the icc.h file is missing.

I'll try to find out why ...

 

Summary

 

This first review, checking out the software, is a positive experience.

The "Hello World!" example build finished without errors - a relief for any reviewer. That sets the expectations for the real work...

 

edit: I have now received the device and the first debug session worked perfect too. See the comments below.

 

 

 

Some notes to myself for further activities

first review the low power example in depth, with debugger, and then without debugger and with power measurements

Then make the DSP example that my friend martinvalencia and I ported to other controllers before. The MAX32660 explicitly positions itself as a DSP capable device.

 

 

part 1: IDE install and Build First Example
part 2: Mod the PCB for Power Measurement
part 3: Power Measurement
part 4a: Low Power Sensor design - Barometer Hardware
part 4b: Low Power Sensor design - Barometer i2c and Init
part 4c: Low Power Sensor design - Barometer, Not Yet Power Optimised
MAX32660 Evaluation Kit - part 5: FreeRTOS Example
side note A: C++ Eclipse Project
side note B: Create a Release Configuration
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Jan Cumps +3
    If you follow these instructions , you can add the terminal functionality in the Eclipse installation of Maxim.
  • Jan Cumps
    Jan Cumps over 7 years ago +2
    One of the projects, the Instruction Cache Example, fails to build in the Maxim's toolchain. The header fie icc.h is mising. I found one on github for another controller (part of the mbed-os part of their…
  • DAB
    DAB over 7 years ago +2
    Good start Jan. DAB
  • Jan Cumps
    Jan Cumps over 7 years ago

    Second experience is not that positive. If you download the SDK now - or if you take the update at startup, it removes MAXIM debug support from the OpenOCD debug plugin (the debugger on this evaluation kit).

    Funny enough, it leaves support for competitor's systems in place. Maxim's config files are gone.

    I raised support case CAS-23802-C3X7H7.

     

    It shows that Maxim does not test new releases and auto updates on their own devices. As far as I can see, the whole MAX3xxxx range is impacted.

    They haven't replied to my ticket, but it's an issue confirmed by another user.

     

    That other user, an element14 member, has found a way to spoof data from the installation program and was able to get a previous version of the MAX32660 specific file. He posted it on the roadtest page, in the comments.

    With that file in the right place, it works.

     

    A road test shows real life experience with a device. I will include it in my end report - also my experience with the support ticket.  I believe Maxim is aware that their device is being reviewed, I mentioned it in the ticket.

    I also think it's wise for a company to have someone monitor the proceedings of road tests on element14.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago

    One of the examples doesn't work fully on my board.

    The FreeRTOSDemo works in general.

    It blinks the onboard LED as expected, and listens to commands from a serial terminal.

     

    But once I test the low-power mode (tickless), by executing, from the serial terminal the command tickless 1, the board does not wake up from pressing the on-board button.

    I've opened a support case at maxim:

     

    This test is part of the proposal I submitted when applying:

    I will also check how easy it is to wake up, what the possible wake-up triggers are.
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Jan Cumps

    If you follow these instructions, you can add the terminal functionality in the Eclipse installation of Maxim.

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Jan Cumps

    Jan Cumps  wrote:

     

    ...

     

    What I haven't found out yet - it's the first time that I work with the OpenOCD debugger - is where the printf() output can be seen.

            printf("count = %d\n", count++);

     

     

    I found the solution. The output is redirected to the serial port and can be captured via a serial terminal program:

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago

    The device arrived, and the first debug session worked perfectly.

    When I plugged the debugger into the laptop, the drivers were automatically applied.

    • serial port
    • HID device
    • disk
    • debugger

     

    That's a lot for a single USB port. Windows Explorer automatically opened (like for all mbed enabled devices).

    In Eclipse, I used the debug configuration that was created when I imported the Hello World example.

    image

     

    What I haven't found out yet - it's the first time that I work with the OpenOCD debugger - is where the printf() output can be seen.

            printf("count = %d\n", count++);

     

    If you are an OpenOCD user, tell me the secret image.

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>