Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog PID temperature controller for the EasyL1105 MSPM0 board - Pt. 3: PWM
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 2 Oct 2025 6:27 PM Date Created
  • Views 1565 views
  • Likes 5 likes
  • Comments 25 comments
  • MSPM0L1105
  • MSPM0
  • easyL1105
  • texas instruments
Related
Recommended

PID temperature controller for the EasyL1105 MSPM0 board - Pt. 3: PWM

Jan Cumps
Jan Cumps
2 Oct 2025
PID temperature controller for the EasyL1105 MSPM0 board - Pt. 3: PWM

 shabaz designed a development kit for the recent Texas Instruments MSPM0 microcontroller series. 
This 4 part blog series documents the steps to design a PID temperature controller. Part 3: add PWM to generate a PID controlled output.

image
(post that introduces the kit)

Goal of this 3nd post

  • add PWM generation logic, based on  PWM example for the EasyL1105 MSPM0 board 
  • drive duty cycle from PID's output signal

not a goal of this post: have the PID regulation working 100%.

Set up PWM SysConfig

The code uses timer TIMG1, channel 0, to drive PA26. There's no interrupt involved. The duty cycle gets adjusted in the regulation loop.

At this point, I have set the PWM period count to 65535, in an attempt to have the output range identical (but 32768 offset) to the input. 

image

image

Code

note: this design doesn't regulate perfectly yet. At this point in the blog series, all modules are in place and they are tied to the PID. But finetuning PID parameters, input, output, ADC and PWM settings is for post 4.

void perform_pwm() {
    DL_TimerG_setCaptureCompareValue(PWM_0_INST, i32_Output_PID + 32768,
        DL_TIMER_CC_0_INDEX); // update ccr0 value  
}


int main(void) {
    SYSCFG_DL_init();

    // /* timer 5 interrupt ticks per second */ 
    // /* Enable Timer0 NVIC */
    NVIC_EnableIRQ(TIMER_0_INST_INT_IRQN);

    NVIC_EnableIRQ(ADC12_0_INST_INT_IRQN);
    gCheckADC = false;

	/* Initialize the parameters of PID */
	Initialize_PID_Parameter();

    /* Start PWM */
    DL_TimerG_startCounter(PWM_0_INST);

    /* Start Timer counting */
    DL_TimerG_startCounter(TIMER_0_INST);    

    while (1) {
        if (perform) {
            perform = false;
            DL_GPIO_setPins(GPIO_GRP_LEDS_PORT,
                GPIO_GRP_LEDS_PIN_LED_GREEN_PIN);

            perform_adc();
            
            perform_pid();

            perform_pwm();

            DL_GPIO_clearPins(GPIO_GRP_LEDS_PORT,
                GPIO_GRP_LEDS_PIN_LED_GREEN_PIN);
        }
    }
}

void perform_pid() {
    /* Execute PID control in every TM0 interrupt. */
    i32_Output_PID = PID(&PID_Var, i32_Target_Command, gAdcResult);
}

If you compare the perform_pid() with the one from the previous post, you 'll see that it now uses ADC as feedback, and output to drive the PWM.

Demo circuit

I used the same (random) low pass filter as in  MSP432 and TI-RTOS: PID Library Part 2 - Real World Example , to turn the PWM into a DC signal.

image

The filter sits between PWM out  (P26) and ADC in (PA25).

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

ccs project for EasyL1105: pid_EasyL1105_20251002_02.zip

Related posts

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 1 year ago in reply to colporteur +1
    It's a Control Technique algorithm. A function that will try to regulate a process' output, in relation to a desired setting. First used in 1911. It requires that you give it feedback on the current…
  • colporteur
    colporteur over 1 year ago

    This is the second time I've seen PID referenced and I am confused.

    PID was a Process IDentifier assigned by an operating system. Now it is a Proportional-Integral-Derivative (PID) controller, a type of control system commonly used in automation.

    Can someone explain this new coin of PID?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to shabaz

    Video of the annoying flicker! The display is very bright, and the large temperature digits are readable from at least a couple of metres away, which is really nice, but cosmetically it's ruined by the flicker.

    I know of some methods to significantly reduce this, but all of them will no longer be general-purpose (currently I can place arbitrary text on the display), but if sticking to numbers only, it should be possible to pre-render and store in Flash, and that would fit in the MSPM0. Anyway, that's a mini-project in itself, for now, I'll leave the flicker as-is : (

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to jc2048

    Hi Jon,

    Thanks for the feedback! I'll take some photos later today, to show what the setup looks like, in case that helps to try to model it. (in brief it's a block of aluminium about 25x25x12mm with a 40W heater and thermistor buried inside, with [I think] quite good thermal contact). I was looking at automated techniques, and Matlab supports what they call 'pidtune' that can support not just PID but some variants too, including 2DOF PID but I do not have the toolboxes to try it out (and don't want to purchase, because of their weird licensing, which means I'd need to purchase maintenance on a lot of existing toolboxes I have). 

    Alternatively there's free software that should work with GNU Octave: https://github.com/marcov/pidtune which just seems to need a step response logged, which is easy enough to do hopefully! I'll probably switch to assembling up the hardware for now, but hopefully revisit this, because while the existing setup works OK-ish, I would like to try to try devising a model, or use some sort of tuning method, to achieve better results.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to jc2048

    Shabaz and I both have a different integrator. My PWM to DC setup has that RC filter.

    In Shabaz' design, the PWM isn't filtered, but it switches a MOSFET. And that fet manages a heating element with a big aluminium mass around it. A lot of mass, and a mega-integrator (and radiator Blush).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 1 year ago in reply to shabaz

    This is great stuff. I'm impressed at how productive you both are here (for a part-time personal project). It looks pretty good to me for many purposes.

    I'm no control system expert (I don't have the practical experience to give good advice), but looking from the perspective of circuit feedback, I think the main complication is all the integrators in the loop. The low pass filter on the PWM is an integrator (at cutoff [10Hz, or so] the phase will be 45 degrees and move higher as you go up towards the PWM repetition rate of about 30Hz), any thermal mass on the output is an integrator sitting within the control loop [probably the dominant low pole, forcing the phase to 90 anywhere up near the PWM rate], and you have sampling and processing which will add other delays, so adding any more with the PID controller is going to make for a very fragile situation with, if not actual oscillation, a very poor phase margin. Since the main job of the PID integrator is to deal with the proportional term not being able to drive all the way to the set point [so as to mop up the very last bit of error], the 'hack' the AI has given you is to disable the I in all the other situations where there is enough gain to drive really embarrassing oscillation. It might be possible to tune the PID better - essentially the ID is a form of lag-lead compensation, so if you were to roughly model the load and the filter in electrical terms and draw a Bode plot of the open loop, you could maybe then see what was needed get a decent gain and phase margin - though I'm not sure how the sampled nature of the control and any latency is dealt with, and I'm not convinced a single D term can counter three integrators, can it?

    I don't know if this would work, but an alternative approach might be to turn off the PID I term entirely and dither the low bits of the set-point input (would need good random numbers with no DC offset, obviously), which might be enough to get the thermal mass integrator to the right point. Might be added complication for no real advantage though.

    Of course, if what you've got is good enough, stick with that. But if you want to develop it further, I think you are going to have to roughly model the 'mechanical' part of the loop [the 'plant'] and include it in your considerations.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>