Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog PSoC6: Low Power Management - prepare the board for current measurements
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 19 Feb 2021 4:21 PM Date Created
  • Views 2575 views
  • Likes 8 likes
  • Comments 5 comments
  • low_power
  • psoc6
Related
Recommended

PSoC6: Low Power Management - prepare the board for current measurements

Jan Cumps
Jan Cumps
19 Feb 2021

When you're making a low power design, it's interesting to know the energy use of your gizmo.

I'm working on PSoC6 projects, and I'm going to calculate its energy profile.

I'll need to measure the current used by the SoC, and that requires a mod of the proto kit.

image

 

The PSoC6 has several sleep modes. Depending on the one that's active, parts of the controller are switched off:

  • Normal state
  • Low Power mode
  • Low Power state
  • Ultra Low Power mode
  • MCU Active
  • CPU Active
  • MCU Sleep
  • CPU Sleep

 

Keeping the power low is tricky. It's hard to assess how much time the device spends in different modes by looking at the code.

And you can't use a debugger to check it. Most power modes are not available when in debug mode.

 

A solution is to measure the SoC's current consumption. The voltage is known and constant. If you log the current use over time, you know the energy profile.

Cypress provides a solution for current measurement on the PSoC6 prototyping kit.

image

If you remove R65, a 0 Ohm resistor, you can put a DC current meter  in its place.

You can then log the measurements and analyse them.

 

R65 is easy to remove. There are no sensitive components near it. I used a hot air pencil.

In case you want to put it back later, tape it for safekeeping in the inside of the kit's box.

image

Here is the result after wicking remaining solder from the pads.

image

 

I want to have a replacement that makes it easy to put a meter in the circuit. Also to make it easy to bypass if I'm not measuring.

I'm using a male pcb header for that. When not measuring, I can put a jumper on it. When measuring, I can make a little cable with female pcb headers.

image

I used a tiny drop of hot glue to fix the header on the pcb. I glued it without the jumper in place to avoid that it gets stuck there.

Then I soldered two thin wires from header pins to the pads of R65. A little crimp sleeve isolates the 2 pins.

image

That's it. The board is now ready for energy profiling.

 

PSoC 6 series
Create a Project with its own Board- and Module configurations
Low Power Management - prepare the board for current measurements
Power consumption without WiFi or Bluetooth
Create a FreeRTOS 10.3 Project
UART receiver with FreeRTOS
FreeRTOS message queue
UART receiver with FreeRTOS - Deep Sleep support
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 5 years ago in reply to Jan Cumps +4
    Here is the result of running the power modes example. Ignore the red overflows. They are pull resistor current during button clicks. You see 10 green lines. They translate to these 10 steps: After programming…
  • Jan Cumps
    Jan Cumps over 5 years ago +3
    Preview of current measurements: The peaks in the measurements are button presses. I measure between 12 mA with the controller full on, and 20 µA in deep sleep. I haven't turned WiFi or BT on.
  • DAB
    DAB over 5 years ago +2
    Good start Jan. DAB
Parents
  • DAB
    DAB over 5 years ago

    Good start Jan.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 5 years ago

    Good start Jan.

     

    DAB