FPGA
  • Technologies
  • More
FPGA
Blog 7 Segment Interfacing - Digilent Cmode S6 FPGA Board
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mahmood.hassan
  • Date Created: 25 Sep 2019 6:39 PM Date Created
  • Views 2263 views
  • Likes 3 likes
  • Comments 2 comments
  • spartan- 6
  • blink led
  • digilent adept
  • digilent
  • cmod s6
  • hello world
Related
Recommended

7 Segment Interfacing - Digilent Cmode S6 FPGA Board

mahmood.hassan
mahmood.hassan
25 Sep 2019

FPGA is fun and easy to learn. Interfacing of Digilent Cmod S6 FPGA development board with 7 segment display. In this code 7 segment display is directly connected to FPGA but it can also be connected through BCD to 7 segment decoder to minimize the number of IO pins.

 

Demo:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Important Links:

Cmod S6 Schematics: cmods6_sch.pdf

Master UCF file: cmod_s6_master_ucf.zip

Factory Loaded Example: cmods6_demo.zip

Reference Manual for Factory Loaded Demo: reference-manual

VHDL Syntax for Port, Mode, and Type Signal Concurrency : lecture.html

How to create MCS file using Xilinx ISE: Tutorial.pdf

VHDL reference: VHDL ref

Attachments:
blink_led.zip
  • Sign in to reply

Top Comments

  • clem57
    clem57 over 7 years ago +1
    Very cool. How much fabric (LUT's, CLB, SRAM, etc did this use?) Thanks mahmood.hassan
  • mahmood.hassan
    mahmood.hassan over 7 years ago in reply to clem57 +1
    Its a fairly simple design and I am working with FPGA after so many years and feeling happy that it didn't took more than few minutes to write this code. Design Summary Number of errors: 0 Number of warnings…
  • mahmood.hassan
    mahmood.hassan over 7 years ago in reply to clem57

    Its a fairly simple design and I am working with FPGA after so many years and feeling happy that it didn't took more than few minutes to write this code.

     

    Design Summary

    Number of errors:      0

    Number of warnings:    0

    Slice Logic Utilization:

         Number of Slice Registers:                  12 out of   4,800    1%

         Number of Slice LUTs:                         12 out of   2,400    1%

         Number used as Memory:                    0 out of   1,200    0%

     

    Slice Logic Distribution:

         Number of occupied Slices                   8 out of     600    1%

         Number of fully used LUT-FF pairs:      12 out of      12  100%

         Number of unique control sets:             1

         Number of slice register sites lost

              to control set restrictions:               4 out of   4,800    1%

     

    Specific Feature Utilization:

         Number of RAMB16BWERs:                0 out of      12    0%

         Number of RAMB8BWERs:                  0 out of      24    0%

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 7 years ago

    Very cool. How much fabric (LUT's, CLB, SRAM, etc did this use?)

    Thanks mahmood.hassan