FPGA
  • Technologies
  • More
FPGA
Blog Building (and testing) the Cheap and Tiny FPGA board.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: michaelkellett
  • Date Created: 31 Dec 2018 3:56 PM Date Created
  • Views 3252 views
  • Likes 12 likes
  • Comments 8 comments
  • fpga
Related
Recommended

Building (and testing) the Cheap and Tiny FPGA board.

michaelkellett
michaelkellett
31 Dec 2018

Those of you with long memories will remember the first blog about this board:

Ultra cheap and Tiny FPGA Board

 

I've built up a couple of boards and got them running some very simple start up software and VHDL.

The good news is that there are only two small bugs on the board, neither is too grim to fix.

 

Other E14 members (notably Jan Cumps ) have been Roadtesting the MAX32660 which provides one half of the good stuff on this board.

My approach to coding the processor is very different so I've hit a different stream of snags and I'll talk a little about one of them and it solution.

 

But first the building !

 

The MAX32660 variant I used comes in a 0.4mm pitch QFN package which is too tricky for pure hand soldering. I used a bought in metal stencil for solder paste printing, hand placed the parts using microscope and tweezers and re-flowed in a CIF drawer type re-flow oven.

The results were quite good, no shorts on either the 0.4mm pitch or 0.5mm pitch QFNs. It's not quite a home process, the screen printer and the oven are a bit pricey for unpaid work - cheaper Chinese alternatives exist.

 

PCB with solder paste

image

 

 

PCB with components before re-flow

image

 

PCB after re-flow and hand soldered parts fitted

image

 

Debugging on Veroboard breakout board with ARM Ulink and logic analyser attached

image

 

PCB Bugs - C10 fouls J2 and wire link on U3

image

 

Test Code

 

The test code on the FPGA just sets up the PLL to turn the 25MHz clock signal from the oscillator chip into a 50MHz signal output on one pin.

 

The C code on the MAX32660 sets up some IO pins and uses SPI to load the FPGA withe its 100k byte bit pattern. I used bit banged SPI which saves me the trouble of getting the MAX32660 SPI hardware going (I'll do that later.)

But to bit bang you need need to be able to set output pins high and low and you would like to be able to do it reasonably quickly.

 

To test the speed of pin toggling I wrote this into Maxim's GPIO example project:

 

while(1)

     {

     GPIO_OutSet(&gpio_out);          //official Maxim way of setting pin

     GPIO_OutClr(&gpio_out);

     }

 

this is pretty grim in that you need to define gpio_out and set it up like this:

 

gpio_cfg_t gpio_out;

gpio_out.port = GPIO_PORT_OUT;

gpio_out.mask = GPIO_PIN_OUT;

 

It's a bit bonkers because the chip only has ONE port - so it must be set to zero but every pin will need you to set its port to zero. I assume this is an attempt to make the code general across the chip family but it is really ugly.

 

But it gets much, much worse:

 

When we run it the toggle rate is 0.86MHz, on a processor with 96MHz core clock and a 48MHz peripheral clock - ugh !

There's a quick gain by turning the instruction cache on (why provide example code that doesn't do this ?)

 

So add

 

ICC_Enable();

 

at the beginning of your c code and the toggle rate improves to 2.347MHz, which is better but still dreadful.

 

The problem is GPIO_OutSet() which is a full on function call, if we replace the calss to the official functions with

 

gpio->out_set = (1u << 4);

gpio->out_clr = (1u << 4);

 

the toggle rate gets up to a more respectable 7.97Mhz.

 

gpio is the single gpio port and is defined in one of the Maxim header files which is how I know about the out_set and out_clr registers, which are NOT documented in the chip's User Manual.

 

It's not very pretty to do it quite like this so I've defined some macros to make it nicer:

 

first we define our pins like this:

 

#define LED GPIO0,4          // I've kept up with allowing more than one port, although it is a bit daft on this processor

 

then (in a header file where we only have to look at it once) we define the macros:

 

#define GPIO(g, p) GPIO_(g, p)

#define GPIO_(g, p) g

 

#define PIN(g, p) PIN_(g, p)

#define PIN_(g, p) p

 

#define GPIO0    ((mxc_gpio_regs_t*)MXC_BASE_GPIO0)

 

 

#define PIN_SET(p) (GPIO(p)->out_set = 1 << PIN(p))

#define PIN_CLR(p) (GPIO(p)->out_clr = 1 << PIN(p))

 

 

and now we can toggle the pins with:

 

PIN_SET(LED);

PIN_CLR(LED);

 

(In the spirit of full disclosure - I did not write the original version of those macros, that honour belongs to my son, Edward, who did them originally for STM32Fxx IO)

 

The first person who can explain simply why the macros must be  defined in two steps (or suggest an alternative that works) can have a board of their very own !

 

Of course the macros PIN_SET and PIN_CLR go at the same speed as gpio->out_set = (1u << 4);

 

It's 9.25x faster than Maxim's demo code.

 

I'm thinking I'll make a breakout board next - any suggestions as to what to put on it are welcome - I want something simple that you can't easily do without the FPGA.

 

MK

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 7 years ago +5
    Hi Michael, It looks like a fun board : ) I'm not too great on macros, (kind of used to quickly closing any header file, if I cant see it then it doesn't exist : ) so a guess is something to do with needing…
  • Jan Cumps
    Jan Cumps over 7 years ago +4
    I’m trying to break the macro riddle, to see why it is multi step. On paper because I’m away from compilers until Sunday. An idea for a breakout board that’s FPGA-interesting? 2 DACs, so you can build…
  • michaelkellett
    michaelkellett over 7 years ago in reply to jc2048 +4
    It's really not the right FPGA for ethernet, a reasonable MAC would use up half the FPGA, the low speed would make an RMII difficult. The processor could manage but would still need to pump all the Ethernet…
Parents
  • shabaz
    shabaz over 7 years ago

    Hi Michael,

     

    It looks like a fun board : )

    I'm not too great on macros, (kind of used to quickly closing any header file, if I cant see it then it doesn't exist : )

    so a guess is something to do with needing to split the comma during a first pass, but maybe the GPIO0 define is preventing that unless it is done in a second macro?

    I tried this on my PC, since curiosity got the better of me..

     

    #include <stdio.h>
    
    #define LED GPIO0,4
    // comment out the two macros for now
    //#define GPIO(g, p) GPIO_(g, p)
    //#define GPIO_(g, p) g
    
    //#define PIN(g, p) PIN_(g, p)
    //#define PIN_(g, p) p
    
    // try just single macros:
    #define GPIO(g, p) g
    #define PIN(g, p) p
    
    
    #define GPIO0    ((mxc_gpio_regs_t*)MXC_BASE_GPIO0)
    
    
    #define PIN_SET(p) (GPIO(p)->out_set = 1 << PIN(p))
    #define PIN_CLR(p) (GPIO(p)->out_clr = 1 << PIN(p))
    
    typedef struct bob
    {
      char out_set;
      char out_clr;
    } mxc_gpio_regs_t;
    
    
    mxc_gpio_regs_t reg;
    mxc_gpio_regs_t* MXC_BASE_GPIO0;
    
    int
    main(void)
    {
      MXC_BASE_GPIO0=®
      MXC_BASE_GPIO0->out_set=0;  // set to some initial value
      MXC_BASE_GPIO0->out_clr=0;
    
      PIN_SET(LED);  // try it out!
    
      printf("out_set is 0x%x\n",  MXC_BASE_GPIO0->out_set);
    
    
      return(0);
    }

     

    For me, the single macro seems to give the right result, it prints out_set is 0x10) but this is with gcc on x86.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 7 years ago

    Hi Michael,

     

    It looks like a fun board : )

    I'm not too great on macros, (kind of used to quickly closing any header file, if I cant see it then it doesn't exist : )

    so a guess is something to do with needing to split the comma during a first pass, but maybe the GPIO0 define is preventing that unless it is done in a second macro?

    I tried this on my PC, since curiosity got the better of me..

     

    #include <stdio.h>
    
    #define LED GPIO0,4
    // comment out the two macros for now
    //#define GPIO(g, p) GPIO_(g, p)
    //#define GPIO_(g, p) g
    
    //#define PIN(g, p) PIN_(g, p)
    //#define PIN_(g, p) p
    
    // try just single macros:
    #define GPIO(g, p) g
    #define PIN(g, p) p
    
    
    #define GPIO0    ((mxc_gpio_regs_t*)MXC_BASE_GPIO0)
    
    
    #define PIN_SET(p) (GPIO(p)->out_set = 1 << PIN(p))
    #define PIN_CLR(p) (GPIO(p)->out_clr = 1 << PIN(p))
    
    typedef struct bob
    {
      char out_set;
      char out_clr;
    } mxc_gpio_regs_t;
    
    
    mxc_gpio_regs_t reg;
    mxc_gpio_regs_t* MXC_BASE_GPIO0;
    
    int
    main(void)
    {
      MXC_BASE_GPIO0=®
      MXC_BASE_GPIO0->out_set=0;  // set to some initial value
      MXC_BASE_GPIO0->out_clr=0;
    
      PIN_SET(LED);  // try it out!
    
      printf("out_set is 0x%x\n",  MXC_BASE_GPIO0->out_set);
    
    
      return(0);
    }

     

    For me, the single macro seems to give the right result, it prints out_set is 0x10) but this is with gcc on x86.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • michaelkellett
    michaelkellett over 7 years ago in reply to shabaz

    Hmmm, that seems to work fine - I just put it in the MAX32660 code.

     

    I wonder if I missed something when I transferred it from the original target.

     

    Any way - I owe you a board but I'll probably make you wait until I've done the breakout board, which so far will have a cheap stereo codec on it.

    But it's not too late to suggest additional goodies.

     

    Thanks.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down