FPGA
  • Technologies
  • More
FPGA
Blog Cheap Cyclone 10
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: michaelkellett
  • Date Created: 31 Jul 2021 2:28 PM Date Created
  • Views 5925 views
  • Likes 15 likes
  • Comments 24 comments
  • fpga design
  • vhdl
  • altera
Related
Recommended

Cheap Cyclone 10

michaelkellett
michaelkellett
31 Jul 2021

I've been following the discussions about the VIDOR4000 in the FPGA group. There was a giveaway associated with the Webinar but of course there will be sonme disapointed non-winners.

 

If you want to get into playing with FPGAs one of the cheapest routes I've found so far is to buy a simple dev board from Aliexpress. There are lots avaialble but this blog is about the Cyclone 10

board from QMTech.

https://www.aliexpress.com/item/1000006634063.html?gps-id=pcStoreJustForYou&scm=1007.23125.137358.0&scm_id=1007.23125.13…

I paid about £16 for mine. I already have a "ByteBlaster" programmer but if you don't it will cost about another £10.

 

The free version of Altera Quartus will do for development.

 

The Cyclone 10 FPGA on this board is smaller than the one on the Vidor board with only about 6k logic elements - but that's enough for useful work.

 

image

 

The board has a 50MHz clock oscillator, a boot Flash chip and a 32MByte SDRAM and the usual regulators for the supply. It comes with a resaonable set of examples which are

extermely useful in getting it running. I downloaded Version 17.1 of Quartus from Intelto match the version used on the board examples. I've also downloaded the 20.1 version for

my own stuff. Running FPGA designs on different versions of the tools often causes problems - so it's best avoided if you can.

The examples are all in Verilog.

 

There's a good blog from  jc2048   at VIDOR 4000: Servo Interface where we have had some discussions about VHDL coding (style and substance image) and a thing that came up

was the possibility of using standard VHDL to infer Block Rams on the FPGA. (The other way is to explicitly refer to the block ram using special IP blocks specific to the FPGA vendor).

 

Having got the LED flasher Verilog demo translated to VHDL I've added a chunk of RAM to the design. It doesn't have anything to do right now so to stop the tools  optimising it away

I've connected it to pins. (Which takes me to another big virtue of the QMTech board, it has about 100 IO pins available on its headers.)

 

This a block diagram of the project. It's done in Aldec-HDL. It's a complete VHDL/Verilog simulator (and more). The block diagram automatically makes all that boring VHDL or Verilog

that links blocks together. The actual code is inside the blocks. I find it helps a great deal to visualise a complex project and saves a lot of time. It isn't free.

 

image

 

This is the RAM code:

 

library IEEE;
use IEEE.std_logic_1164.all;   
use IEEE.NUMERIC_STD.all;


entity mem_inf_sp_64_12 is
     port(
         we : in STD_LOGIC;
         en : in STD_LOGIC;
         clk : in STD_LOGIC;
         address : in STD_LOGIC_VECTOR(5 downto 0);
         data : in STD_LOGIC_VECTOR(11 downto 0);
         q : out STD_LOGIC_VECTOR(11 downto 0)
         );
end mem_inf_sp_64_12;

--}} End of automatically maintained section

architecture mem_inf_sp_64_12 of mem_inf_sp_64_12 is   

    type ram_type is array (0 to 63) of std_logic_vector(11 downto 0);   -- array must be 0 - n, if declared the other way wit downto to match Xilinx example then Quartus fitter fails
    signal ram : ram_type;

begin

    process(clk)
    begin
        if rising_edge(clk) then
            if en = '1' then
                if we = '1' then
                    ram(to_integer(unsigned((address)))) <= data;
                end if;
                q <= ram(to_integer(unsigned((address))));
            end if;
        end if;
    end process;

end mem_inf_sp_64_12;

 

All pure VHDL but note that comment on line 21 - my Xilinx example codes the array "63 downto 0" - I don't have a Xilinx toolset runing so I can't test if they care, but the Altera tools

only infer the block memory one way round.

(There seem to be some extra brackets in lines 31 and 33  - but they do no harm)

 

image

 

The screenshot shows the loveliness of the Altera toolset and the resources used

 

So there you go -  a really cheap (and by FPGA standards, a quite simple) way into FPGA.

 

QMTech do a very similar board (but about twice the price) with an Artix 35 on it - I'll attempt to repeat this experiment when it turns up.

 

MK

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 5 years ago in reply to 14rhb +5
    Happy to share ! If anyone buys one of these and needs to talk about I'll (almost always) respond on E14. I suppose I should point out that I have no connection with Aliexpress or QMTech. Just trying to…
  • 14rhb
    14rhb over 5 years ago +4
    When trying to learn electronics on a small budget it can be a difficult decision whether to pay out for a reputable dev board or to opt for a low-cost one via the route you have identified. Therefore…
  • dang74
    dang74 over 5 years ago +4
    Thank you Michael, Three years ago I purchased a Cyclone IV board made by QMTECH. It is the same form factor as your board. I don't remember the exact price but it was very inexpensive and I've put it…
  • michaelkellett
    michaelkellett over 5 years ago

    Agree re.version problems. Happy to see you can still get at alot of the free IP.

     

    Altera are better in this respect - much easier to download earlier versions and they don't have the same enthusiasm for changing the names.

     

    My boards (when they come) for Artix have demo code written for Vivado 2018.2 - I may reget going for the current version

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to michaelkellett

    michaelkellett  wrote:

    ...If you look in the Vivado IP thing (IP Generator ?)  you can access IP blocks to use all sorts of stuff, including DSP blocks. I don't have Vivado

    installed on a machine at the moment but I'll sort that.

    ...

    you are correct, the DSP IPs are available, except for one FFT flavour:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to michaelkellett

    version hell: 2021.1 does not work with Zynq

    2020.1 and 2020.2 do, but to be in line with the current Pynq designs, you need 2020.1.

    The toolchain mess is my least favourite part of working with (xilinx) FPGAs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 5 years ago in reply to Jan Cumps

    Well, that one has gone !

     

    I'm installing Vivado 2021.1 Standard Edition which is today's free version.

     

    I tried to limit it to 7 series parts no processors but it's till going to need 22GB download and 40+Gb disk space.

    Only 6 hours to go .....

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to michaelkellett

    I'm running the Vivado suite, version 2020.2. With WebPack license.

    - Vivado (the new ISE)

    - Vitis (eclipse environment, used to compile executables for Microblaze soft cores and other things)

    - Vitis HLS ("FPGA accellerator", turns C algorithms into Verilog or VHDL blocks so that they become executable hardware implementations)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>