FPGA
  • Technologies
  • More
FPGA
Blog Tips for Integrating WiFi on the Ultra96-V2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: narrucmot
  • Date Created: 30 Jan 2020 11:02 PM Date Created
  • Views 3795 views
  • Likes 5 likes
  • Comments 3 comments
  • ultra96-v2
  • wilc3000
  • avnet
  • petalinux
  • github
  • linux modules
  • ultra96
  • designed by avnet
  • zynq mpsoc
  • bsp
  • git
  • wifi driver microchip atwilc3000
  • github_repository
  • linux
Related
Recommended

Tips for Integrating WiFi on the Ultra96-V2

narrucmot
narrucmot
30 Jan 2020

A key feature of Avnet's Ultra96-V2 board is its WiFi and Bluetooth connectivity that is made possible using the on-board ATWILC3000 module from Microchip. This module is IEEE 802.11 b/g/n plus Bluetooth 5 LE and is certified in more than 75 countries globally.  The module provides SDIO (WiFi) and UART (Bluetooth) interfaces for connecting to the host processor and can achieve WiFi throughput of up to 46 Mbps UDP & 28 Mbps TCP/IP.  Though this is a very popular module that is used in countless products, we did have some challenges when integrating it for use in Linux on the Ultra96-V2 board.  A few of the challenges we faced were:

  • Arm v7 vs Arm v8 architecture and Linux kernel v4.9 vs. v4.14
  • Device driver patch
  • Device tree settings
  • Ever-changing application source files
  • Xilinx shell script and configuration file require patches

 

Arm v7 vs Arm v8 architecture and Linux kernel v4.9 vs v4.14

Perhaps the most significant challenge we faced in our development with the ATWILC3000 module was that the device driver was targeted to Arm v7 CPU architecture (e.g. Arm Cortex-A9, etc.), but the Xilinx Zynq UltraScale+ device on the Ultra96-V2 board has an Arm v8 CPU (quad core Cortex-A53).  Though this module was known to work and had been tested with many Microchip Arm MCUs and CPUs, none of them were Arm v8 like the Zynq UltraScale+.  The difference is in how memory gets allocated and shared up and down the driver stack.  This issue was also exacerbated by changes in the Linux kernel.  In Linux kernel v4.9 (PetaLinux 2017.x) the driver worked as expected and we used this kernel for our initial testing of this module with the Ultra96-V2 board.  However, starting with Linux kernel v4.14 (PetaLinux 2018.x) it became clear that the driver was now broken.  The Linux device driver was no longer able to read the chipid from the ATWILC3000 module, and this of course made the driver non-functional.  The v4.9 Linux kernel allowed the driver to use a local stack variable to pass data up the stack and the v4.14 Linux kernel changed this to require that kmalloc be used instead.  Once we changed the driver to use kmalloc we were able fetch the chipid from the WiFi module and the device driver started working again.  This is all likely because the Arm v8 architecture introduced support to control access to shared memories, and this change was implemented in the Linux v4.14 kernel.

 

Device driver patch

In addition to the kmalloc issue with the device driver, we also needed to patch a Linux kernel source to correctly toggle the module's reset pin at boot time.  This is a requirement for the ATWILC3000 module to be initialized in a known-good state.  The device driver originally performed this function, but it did not work correctly so we disabled it in the device driver and instead moved this task to the drivers/mmc/core/pwrseq_simple.c kernel source file.  This patch is supplied as part of a kernel configuration bitbake recipe in the PetaLinux BSP.

 

image

 

Device tree settings

In additional to having a working Linux device driver, it is also critical to make sure the device tree settings are correct. If the device tree description for the WiFi module is incorrect, Linux won't know how to make the connection between the hardware device and the device driver in the system.  For the ATWILC3000 there are two parts to the device tree description - one for the toggling of the module's reset pin and another to describe the SDIO interface and "connect" it to the WiFi module.

Description of connections for toggling the reset pin:

/ {

   sdio_pwrseq: sdio_pwrseq {  /* This needs to be able to manipulate the chip_en and the resetn properly */

      compatible = "mmc-pwrseq-simple";

      reset-gpios = <&gpio 7 1>; // MIO[7] for WILC3000 RESETN, Active low

      chip_en-gpios = <&gpio 8 1>;

   };

};

 

Description of the attachment of the device driver to the SDIO interface:

&sdhci1 {

   bus-width= <0x4>;

   max-frequency = <50000000>;

   /delete-property/cap-power-off-card; // This is not compatible with the WILC3000 and means the WILC will always be powered on

   status = "okay";

   #address-cells = <1>;

   #size-cells = <0>;

   wilc_sdio@1 {

      compatible = "microchip,wilc3000", "microchip,wilc3000";

      reg = <0>;

      bus-width= <0x4>;

      status = "okay";

   };

};

 

Ever-changing application source files

One of the applications that is included in the PetaLinux BSP that we post for users to download is a Python webserver.  This webserver is created and maintained by Xilinx.  In addition to acting as the webserver for the example projects and documentation, etc. stored in the Linux filesystem on the Ultra96-V2 board, this application also takes care configuring the WiFi interface via the on-board access point.  This configuration mechanism has undergone several changes in recent PetaLinux versions.  Packaged along with this webserver are accompanying html pages, etc. for the webpages it serves.  Because these files are different for the Ultra96-V1 vs the Ultra96-V2 board, Avnet maintains a separate "ultra96v2" branch in the git repository for these sources that are specific to the Ultra96-V2 board.  This requires Avnet to keep this branch updated each time Xilinx makes a change to the master branch of Ultra96-V1 files.  Keeping up with the changes that Xilinx makes to this webserver in the "master" branch and incorporating them into the "ultra96v2" branch can be a bit of a challenge and cumbersome process of git commits and pull requests.

 

Xilinx shell script and configuration file require patches

In the "out of box" Linux OS image for the Ultra96 there is a shell script (/usr/share/wpa_ap/ap.sh) that runs at Linux boot time that loads the ATWILC3000 device driver and starts the WiFi access point (AP).  This AP allows any WiFi device to connect to the WiFi AP SSID (ULTRA96-V2_<MAC ID>) and open the webpage (http://192.168.2.1/wifi_setup.html) to configure the board to connect to a WLAN by providing the WLAN SSID and password.  This script is created and maintained by Xilinx and was first used with the Ultra96-V1 board which had a Texas Instruments WiLink8 WiFi & Bluetooth module installed.  The device driver for the WiLink8 provides two interfaces for WiFi connectivity - one for the AP (wlan1) and another for the WLAN connection (wlan0).  This script was written with "wlan0" and "wlan1" hard coded to match the WiLink8 device driver and at that time it was never expected that the WiFi module would change.  However, Avnet needed to spin a rev of the Ultra96 board - now named Ultra96-V2 - to replace an end-of-life DDR4 memory device and to change the WiFi & Bluetooth module to the Microchip ATWILC3000.  The device driver for the ATWILC3000 provides the same two interfaces but they are named "p2p0" (AP) and "wlan0" (WLAN).  This meant that this script had to be updated to match the ATWILC3000 device driver and the best way to do that was via a patch that gets applied via a bitbake recipe at PetaLinux build time.  There is also a configuration file (/usr/share/wpa_ap/udhcpd.conf) that configures a DHCP server that is used by the AP to serve IP addresses to those WiFi devices that connect to the AP's SSID.  Like the AP shell script this was also hard coded with "wlan1" to match the AP interface provided by the WiLink8 device driver.  Avnet also provides a patch and bitbake recipe to change this to "p2p0" at PetaLinux build time. 

 

As ubiquitous as WiFi connectivity has become in our lives - from smart phones and gadgets to cars and appliances - the engineer's task of integrating it into the hardware and software of these devices remains a sometimes arduous and complex task.  For all of the development boards that Avnet has created over the years integrating WiFi and Bluetooth connectivity has always been a challenge - especially for the software.  This blog post highlights some of those challenges and hopefully provides a blueprint to follow for your own development with theUltra96-V2 board.  All of the patches and fixes mentioned here have been integrated into the PetaLinux BSPs that Avnet provides for the Ultra96-V2 board.  It is recommended that any user looking to do any development with this board start with these BSPs.

 

Here are a few more useful links related to the Ultra96-V2 board and the Microchip ATWILC3000 module:

Ultra96 Hardware Design Forum

Microchip ATWILC3000 product page

Avnet's git repo for the modified ATWILC3000 Linux device driver sources

Microchip's official git repo for the ATWILC3000 Linux device driver sources

Xilinx git repo for the Python webserver

 

  • Sign in to reply

Top Comments

  • bhfletcher
    bhfletcher over 4 years ago in reply to kevinkeryk +1
    The passphrase problem that you mention was a bug that has been corrected. Our team has corrected that in the design files on GitHub, and we should have a new SD card image to share shortly. Bryan
Parents
  • kevinkeryk
    kevinkeryk over 5 years ago

    Thanks for all the great tips on how to get the Wi-Fi working on Ultra96-V2 Tom, this is very helpful!

     

    The instructions in the Ultra96-V2 Getting Started Guide are working very well for me:  http://avnet.me/ultra96v2-gsg

     

    I noticed on my Ultra96-V2 that with one of my WPA2 secured networks, it appears in the Open Networks section of the drop down list which then does not allow me to enter the passphrase until I click on the Text Field option.

     

    Seems to connect to my secured AP fine but then I only get an IPv6 address and not an IPv4 address:

     

    image

     

    But after I access the network for a while (like clone my favorite Avnet GitHub repos) then an IPv4 address also shows up:

     

    image

     

    Any idea why that might be happening?

     

    Best Regards,

     

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kevinkeryk
    kevinkeryk over 5 years ago

    Thanks for all the great tips on how to get the Wi-Fi working on Ultra96-V2 Tom, this is very helpful!

     

    The instructions in the Ultra96-V2 Getting Started Guide are working very well for me:  http://avnet.me/ultra96v2-gsg

     

    I noticed on my Ultra96-V2 that with one of my WPA2 secured networks, it appears in the Open Networks section of the drop down list which then does not allow me to enter the passphrase until I click on the Text Field option.

     

    Seems to connect to my secured AP fine but then I only get an IPv6 address and not an IPv4 address:

     

    image

     

    But after I access the network for a while (like clone my favorite Avnet GitHub repos) then an IPv4 address also shows up:

     

    image

     

    Any idea why that might be happening?

     

    Best Regards,

     

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • nhphuong
    nhphuong over 4 years ago in reply to kevinkeryk

    Hi Kevin,

     

    about the problem with entering passphrase, I realize that we have to scroll the wifi list further down and choose the one in the group of secured AP (the one we chose belong to group of open AP).

     

    Regards,

     

    -Phuong

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bhfletcher
    bhfletcher over 4 years ago in reply to kevinkeryk

    The passphrase problem that you mention was a bug that has been corrected. Our team has corrected that in the design files on GitHub, and we should have a new SD card image to share shortly.

    Bryan