FPGA
  • Technologies
  • More
FPGA
Blog Ultra96-V2 Dual Camera Mezzanine Petalinux Build Instructions
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ctammann
  • Date Created: 14 Jan 2021 9:14 PM Date Created
  • Views 6226 views
  • Likes 5 likes
  • Comments 23 comments
  • image sensor
  • avnet
  • mezzanine
  • vision
  • petalinux
  • xilinx
  • ultra96
  • 96boards
  • ai
  • on semiconductor
Related
Recommended

Ultra96-V2 Dual Camera Mezzanine Petalinux Build Instructions

ctammann
ctammann
14 Jan 2021

As a follow up to the blog I posted on building the hardware design for the out of box image for the ON Semiconductor Dual Camera Mezzanine card, here are the instructions to complete the build with the Petalinux project. The original blog can be found here -
Ultra96-V2 ON Semiconductor Dual Camera Mezzanine hardware build instructions

 

The process of porting the full design over to our Github repo has now been completed. Below I've pasted the instructions to build the full design including Petalinux from the repo. The final command will build the hardware design as part of the script and create the full design.

 

#

# Clone the repositories

#

 

$ cd ~

$ mkdir -p git/avnet

$ cd git/avnet/

$ git clone https://github.com/Avnet/bdf.git

$ git clone https://github.com/Avnet/hdl.git

$ git clone https://github.com/Avnet/petalinux.git

$ cd bdf
$ git checkout master

$ cd ../petalinux

$ git checkout 2020.1

$ cd ../hdl

$ git checkout 2020.1

 

#

# Run the Vivado build script for the Ultra96-V2 dualcam design

#

 

$ cd ../petalinux

$ ./scripts/make_ultra96v2_dualcam.sh

 

 

This process will take a long time and will depend on your pc hardware. When complete, you should see something similar to this:

image

 

Your design has now successfully been built (yay!). So now we need to put it on an SDcard to use on your hardware. Pulling from my colleague Tom Curran's excellent instructions, if you haven't already followed the Getting Started Guide you will need to first partition the SD card with - for example - a 1GB FAT32 boot partition and (assuming you are using the provided 16GB Delkin micro SD card) and a 15GB ext4 partition. I've also attached a handy guide on formatting a new SDcard to this blog.

 

If you have successfully configured your SDcard you are ready to copy over the files. Here are the commands to create the SDcard image. First you must navigate to the folder where the files were generated, then you can copy them over to the proper partitions on your SDcard.

 

$ cd ~/git/avnet/petalinux/projects/ultra96v2_dualcam_2020_1

$ cp ./images/linux/BOOT.BIN /media/training/<UUID of FAT32 partition>/.

$ cp ./images/linux/boot.scr /media/training/<UUID of FAT32 partition>/.

$ cp ./images/linux/image.ub /media/training/<UUID of FAT32 partition>/.

$ sudo rm -rf /media/training/<UUID of ext4 partition>/*

$ sudo tar xvf ./images/linux/rootfs.tar.gz -C /media/training/<UUID of ext4 partition>/

$ sync; sync (VERY IMPORTANT to sync the filesystem BEFORE ejecting the SD card!  If you don't the filesystem may be corrupted. This process can take minutes to complete)

 

You should now be able to run the out of box design from your SDcard with the command

 

$ run_1920_1080

 

The out of box image will show 2 live streams from the cameras on a 1080p monitor.

 

Ultra96-V2Ultra96-V2

Attachments:
imageSD Card Formatting an SD Card.docx
  • Sign in to reply

Top Comments

  • albertabeef
    albertabeef over 5 years ago in reply to _david_ +3
    David, We are actively working on this. My colleagues are stabilizing the hardware/software portions generated by the hdl/petalinux repositories. I am working on the Vitis-AI designs generated by the vitis…
  • zedhed
    zedhed over 5 years ago in reply to jomoenginer +1
    Hi jomoenginer , Yes, I agree that seeing the CRC mismatch is unsettling, but I asked our driver developer about this and the explanation that I got is that it is mostly innocuous. The driver will attempt…
  • narrucmot
    narrucmot over 5 years ago in reply to dje666x +1
    Hi David, This script error is a result of the BUILD_FROM_TAG script variable is set to "true" in the scripts/common.sh file: Change this to "false" and re-run the script and it should complete successfully…
Parents
  • dje666x
    dje666x over 5 years ago

    Thanks Tom,

     

    That fix has allowed me to advance to level-2. Now I need to source the v_OSD IP license. Any idea if this is part of a video IP bundle from Xilinx.?

     

    ta,

     

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dje666x
    dje666x over 5 years ago

    Thanks Tom,

     

    That fix has allowed me to advance to level-2. Now I need to source the v_OSD IP license. Any idea if this is part of a video IP bundle from Xilinx.?

     

    ta,

     

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • narrucmot
    narrucmot over 5 years ago in reply to dje666x

    Currently the Ultra96-V2 dualcam design requires the v_osd IP that has been obsoleted by Xilinx and is no longer available starting with the 2020.2 tools.

     

    If your design needs are urgent you can revert to using the 2020.1 PetaLinux and Vivado tools.  For Vivado 2020.1 the v_osd IP cannot be licensed separately, but it is included in the SDSoC license.  More information and instructions can be found in the comments for this blog post.

     

    If you have some flexibility with your time and can wait, we are currently working on an overhauled design for Vivado & PetaLinux 2020.2 to remove the v_osd IP from the Ultra96-V2 dualcam design.  This development is currently in testing now and will be merged into the 2020.2 git branches soon for the Avnet hdl and petalinux github repositories.

     

    --Tom