FPGA
  • Technologies
  • More
FPGA
Forum Spartan 6 Connectivity issue
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 582 subscribers
  • Views 4503 views
  • Users 0 members are here
Related

Spartan 6 Connectivity issue

Krishnajdl10
Krishnajdl10 over 3 years ago

The spartan 6 board is not getting detected in ISE. The connection is via JTAG. The board is getting powered on but it is not getting recognized when boundary scan is carried out in select target device phase. Kindly help in resolving this issue

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Krishnajdl10 +2
    ISE is not compatible with it.
  • flyingbean
    flyingbean over 3 years ago in reply to Krishnajdl10 +2
    I installed Window 7(64-bit) for ISE14.7. Windows 10 does not work with ISE any more. You might try to use Linux/Ubuntu for ISE14.7.
  • flyingbean
    flyingbean over 3 years ago in reply to Krishnajdl10 +1
    I used this Spartan6 EVB a few years ago. I used ISE 14.7 with Xilinx JTAG debugger without any issues.
Parents
  • saadtiwana_int
    0 saadtiwana_int over 3 years ago

    Since the latest ISE version (14.7) uses a Virtual machine, please make sure the relevant USB-JTAG device is attached to the VM in the VM settings. By default all devices connected to the host are not connected to the VM. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • saadtiwana_int
    0 saadtiwana_int over 3 years ago

    Since the latest ISE version (14.7) uses a Virtual machine, please make sure the relevant USB-JTAG device is attached to the VM in the VM settings. By default all devices connected to the host are not connected to the VM. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Krishnajdl10
    0 Krishnajdl10 over 3 years ago in reply to saadtiwana_int

    It has been selected

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to Krishnajdl10

    Hi,

    You could try a different programmer. Either in the VM, or outside it (by transferring your bit file to outside the VM).

    There are lots of different programmers, for example you could even use a Raspberry Pi as a programmer. You'd have to google to find a decent one. It is fairly common, because there were at one time a fair amount of plug-on boards for the Pi or BeagleBone Black that had a Xilinx FPGA for experimentation, and they needed a way to transfer the data. If you google "Raspberry Pi Xilinx Programmer" or similar, you'll come across it.