FPGA
  • Technologies
  • More
FPGA
Forum Nandland Go Board Kickstarter
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 582 subscribers
  • Views 8927 views
  • Users 0 members are here
  • nandland
  • icestorm
  • fpga
  • ice40
Related

Nandland Go Board Kickstarter

johnbeetem
johnbeetem over 10 years ago

I just found out about the Nandland Go Board on KickStarter.  It’s a nice little FPGA board that looks very well suited to learning about FPGAs since it includes the I/O devices you need for basic FPGA projects.

 

The Go Board uses the Lattice iCE40 HX1K FPGA, the same one as the Lattice iCEstick.  While the HX1K is a rather small FPGA, iCE40 is the only available FPGA I know of that supports open-source FPGA design tools, specifically IceStorm and its partner tools arachne-pnr and yosys.  iCE40 is also a very simple architecture, which is nice for people just getting started with FPGAs.  Nandland wants to make it fun to learn about FPGAs and play with them -- iCE40 is a good way to avoid the complexity of more advanced FPGAs like Xilinx Spartan-6.

 

The big strength of the Go Board is its built-in I/O devices:

image

  • Four user-programmable LEDs.
  • Four push-button switches for user input.
  • Dual 7-Segment LED display.
  • VGA connector for video output.
  • Digilent PmodTm connector for external I/O.
  • 25 MHz oscillator.
  • 1 Mb Flash for booting the FPGA.
  • FTDI FT2232H serial USB chip for FPGA programming and UART communication to projects.

 

All you need to program a Go Board from a PC is a Micro USB cable.  The FT2232H is also used on the Lattice iCEstick, Papilio DUO, and other FPGA boards.  It has both GNU/Linux and Windows support, and the IceStorm programming tool knows how to talk to it so IceStorm should be able to work with the Go Board.

 

The Kickstarter video that demonstrates the board is quite impressive, with some nice LED, VGA, and UART communications examples.  It even has a Pong game image  The Nandland web site has some nice-looking tutorials as well, both VHDL and Verilog.

 

[I don’t have any relationship with Nandland, except as a backer.  As with all Kickstarters, there’s some risk.  However, the Go Board prototype works and the PC board isn’t pushing the state of the art.  February 2016 delivery is probably optimistic what with the holidays and all.]

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to johnbeetem +2
    Hi John and Michael, I'm Russell and I created the Nandland.com Go Board. Michael thanks for the complement about the webpage. My main goal is to create a website that teaches everyone how to use FPGAs…
  • shabaz
    shabaz over 10 years ago in reply to johnbeetem +2
    Hi John, I see. That explains it! It looked a bit bare so close up to the FPGA. I'm sure Russell knows what he's doing, I just watched his video. I have seen other kickstarters though where they totally…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to johnbeetem +2
    Happy New Year all, Russell from nandland.com here... A couple things: 1. I have got Pre-Orders set up on www.nandland.com. You can now place an order for the boards. The post-kickstarter price is $55…
Parents
  • johnbeetem
    johnbeetem over 10 years ago

    Just got my Go Board yesterday.  Everything is working so far.  It has a pre-programmed demo so you can see if it's powering up correctly.  I reprogrammed it using IceStorm, which worked fine except that it took a long time to program the SPI flash.  Maybe there's an option or update that only does a partial reprogram.  Also, IceStorm by default assums a TQ144 so I remapped the Go Board's VQ100 pin numbers.  There may be an arachne-pnr option or update that does VQ100.

     

    Great job, Russell! (rman12345)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 10 years ago in reply to johnbeetem

    Hi John,

     

    Do you have a project in mind for the board or are you just checking out its capabilities?

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 10 years ago in reply to DAB

    DAB wrote:

     

    Do you have a project in mind for the board or are you just checking out its capabilities?

    Go Board is going to be one of the targets for XXICC when I have a chance to get back to it.  I ran an experimental version of XXICC for today's Go Board experiments, using GCHD (GalaxC for Hardware Design) as the front end instead of Verilog.  XXICC generates BLIF (Berkeley Logic Interchange Format) which is the input to arachne-pnr for place & route.  IceStorm generates the iCE40 bitstream from arachne-pnr's text output.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 10 years ago in reply to DAB

    DAB wrote:

     

    Do you have a project in mind for the board or are you just checking out its capabilities?

    Go Board is going to be one of the targets for XXICC when I have a chance to get back to it.  I ran an experimental version of XXICC for today's Go Board experiments, using GCHD (GalaxC for Hardware Design) as the front end instead of Verilog.  XXICC generates BLIF (Berkeley Logic Interchange Format) which is the input to arachne-pnr for place & route.  IceStorm generates the iCE40 bitstream from arachne-pnr's text output.