Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Stepper Motor Control with Hercules High-End Timer - Part 7: HET Assembly Language Test
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 10 Jun 2017 3:51 PM Date Created
  • Views 4558 views
  • Likes 5 likes
  • Comments 9 comments
  • stepper_motor
  • boosterpack
  • drv8711
  • texas_instruments
  • hercules
  • launchpad
Related
Recommended

Stepper Motor Control with Hercules High-End Timer - Part 7: HET Assembly Language Test

Jan Cumps
Jan Cumps
10 Jun 2017

I'm trying to control an unknown stepper motor with the high-end timer (NHET) module of a Texas Instruments Hercules microcontroller

image

I got a freebie from TI almost a year ago. An unknown stepper motor, a driver board and a Hercules RM57 LaunchPad. The code to run the motor was expected to arrive too (it was an assignment for an internal) but that never materialised. In this blog series I'm trying to program the NHET module so that it sends the right signals to make the stepper step.

 

In the 7th blog I create an Assembler program for the HET submodule.

 

 

Hercules High-End Timer

Hercules microcontrollers have a particular type of timer on board. It's an autonomous sub-controller.

The difference with your typical timer is that you don't set registers to control it.

You write a program in the HET assembly language.

The asm commands are also different from those of a controller or a processor. Everything is related to timer, angular functions, tight control of timer loop.

Often they can do several things in parallel during a single click of the HET clock.

 

image

 

And the module can interact with the ARM controller(s) on the Hercules - memory access and interrupts.

Expert programmers can achieve amazing things.

It's possible to handle the whole server motor control (ramp up, constant speed and ramp down) in the HET module.

The ARM would just set the number of steps to take and go to deep sleep. I'd like to achieve that in this blog series.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I have another example published by TI where the whole i²c protocol is implemented in the HET assembly language.

 

HET Test Program

Today I just want to see if I can get a HET program assembled and linked into my code, and have a HET pin generate a PWM signal.

image

The program is a little more complex than it can be, because it allows for flexible period - something we can ignore here.

 

; PWM, 1 channel with buffer field to modulate PWM period
L00  CNT      {  reg=A, irq=OFF, max= 3 }
L01  BR        { next= L03, cond_addr=L02, event= ZERO }
L02  MOV64 { remote= L00, cntl_val= 4, data=0, hr_data=0 } ; CPU to write new period value to control field
L03  MCMP   {  en_pin_action= ON, pin= 4, order= REG_GE_DATA, action= PULSELO, reg=A, data=2, hr_data=64}
L04  BR        { next= L00, cond_addr=L00, event= NOCOND }

 

Don't try to understand this unless you want to learn the assembler language. A manual is available from TI's Hercules product page.

The only thing that's interesting for this exercise is knowing that this code will generate a 234 kHz PWM with 50% duty cycle on HET pin 4.

 

image

I've chosen PIN 4 deliberately because that matches the stepper pin of the DRV8711 Stepper Driver BoosterPack.

There's a HET IDE that asists you when writing code (and can integrate with a simulator to pre-test your design on a PC).

You can also assemble the code from the IDE. This will generate a .c and a .h file. They will end up in your project in the next step:

 

Configure Hercules to Run the HET Code

Like the other modules, HET is configured in HALCoGen. First thing to do is enable the driver:

image

 

This will take care that HALCoGen creates the driver code for the timer. Then we set the PINMUX so that NHET1 pin 4 is active.

(not really really needed because it's the default assignment for the pin, but it helps finding conflicts later on)

image

 

On the NHET module itself, you define the frequency, and say that you want to use HET assembly.

(This module can also be configured as a straightforward PWM generator without programming)

image

The .h and .c files that we select here are the ones generated by the HET IDE when you pressed the assembler.

When you press the HALCoGen "Generate Code" button later on, thes files will be copied into your Hercules project code.

As a last step in this blog, I'll show how all of this can be scripted so that both the assembly and copy step are automatically done as part of a CCS build.

 

The last step in the HET configuration pages is to make HET1 pin 4 an output pin:

image

 

CCS Project Settings and Automating the Build

I prefer to minimise the number of manual steps when building a firmware binary. If at all possible, no manual steps, so that a build is repeatable.

In this case it is possible because the HET suite for the Hercules come with a command line assembler.

In CCS, you have the option to add commands before or after a build, so that's a perfect location to put these.

 

image

I have created my HET IDE project in the het subfolder of the CCS project.

For some reason, the build steps are executed from a folder one level in the project (too lazy to find out which one), so we have to prepend all folders with  ..\.

The first line assembles the .het source into  .c and .h files in the het folder:

${HET_COMPILER} -n0 -v2  -hc32 ..\het\het.het

 

The next two lines copy the .h and .c into the HALCoGen project source:

copy /Y  ..\het\het.h ..\HALCoGen\include\het.h
copy /Y  ..\het\het.c ..\HALCoGen\source\het.c

 

That's all. A little bit of scripting automates the whole thing. The results can be found back in the console after build:

**** Build of configuration Debug for project RM57_Stepper ****

"D:\\ti\\ccsv7\\utils\\bin\\gmake" -k -j 8 all -O 
"D:\Program Files (x86)\Texas Instruments\Hercules\HET IDE\03.05.01\bin\hetp.exe" -n0 -v2  -hc32 ..\het\het.het
NHET Assembler    Release 1.7
Texas Instruments Incorporated. 
 PASS 1
 PASS 2

 No Errors, No Warnings
copy /Y  ..\het\het.h ..\HALCoGen\include\het.h
        1 file(s) copied.
copy /Y  ..\het\het.c ..\HALCoGen\source\het.c
        1 file(s) copied.
' '
'Building file: ../HALCoGen/source/HL_gio.c'
'Invoking: ARM Compiler'
...

 

I've registered the HET command line tool in a project parameter, so that the script is PC independent:

image

 

A last point of attention: if the HET project is a subfolder of your CCS project, you'll have to exclude it from compiling. Else you have the het.c file twice in your build and it'll fail.

image

 

 

Running the HET code

The easiest part. It runs immediately when you initialise the HET module.

 

// ...
#include "HL_het.h"
// ...

int main(void)
{
// ...
    hetInit();
// ...

 

The oscilloscope grab at the start of the blog is the actual result of running the code of this blog.

 

In a next blog we'll communicate with the HET sub-controller so that it only generates pulses when we want it, and how we want it.

The end-game is to get a signal like this out of the module, based on a ramp profile that we define.

image

 

Related Blog
Part 1: Hardware Overview
Part 2: Stepper Controller and MSP430 Firmware
Part 3: SPI Commands and Pulse Control
Part 4: Analyse MSP430 PWM Step Signal
Part 5: Hercules RM57 Hardware Provisioning
Part 6: Hercules RM57 SPI
Part 7: HET Assembly Language Test
Part 8: HET Based Pulse Train Output
  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago +1
    Another excellent post Jan. Good detail and screen captures so that the reader can easily follow along. Well done. DAB
  • michaelkellett
    michaelkellett over 9 years ago +1
    Useful blog Jan, I see that the HET has been around since 2010 (at least) and this is the first time I've noticed it !! Motorola (in the days before On and Freescale) offered a complex programmable timer…
  • michaelkellett
    michaelkellett over 9 years ago in reply to Jan Cumps +1
    Is this a business opportunity ( Currently designing/coding an Ethernet UDP RX/TX offload system in VHDL for FPGA - there must be easier ways to make a living !) MK
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Jan Cumps

    Capture with logic analyser:

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Jan Cumps

    Hooray:

     

    image

     

    I was able to reuse the pulse train generator code of a TI application note.

    It's just what I need. I can pre-program a number of steps, ramp up to some stable speed or ramp down to another stable speed.

     

        ptoCmdCreate(&cmdList[0], 1000000, 50, ptoDirFwd, ptoAccLinAcc);
        ptoCmdCreate(&cmdList[1], 105132, 10, ptoDirFwd, ptoAccZero);
        ptoCmdCreate(&cmdList[2], 105132, 50, ptoDirFwd, ptoAccLinDec);

     

    When you call the activation method, the commands are executed, one by one.

     

        ptoStart(pto1);
        for (i = 0; i < NUMCMD; i++) {
            ptoCmdSubmit(pto1, cmdList[i]);
        }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago

    Here's a capture of a TI NHET example with dynamic period.

    I've compiled it from source and it's running on my controller now, an excellent opportunity to start from working code.

     

    The scope shows how the frequency of the signal dynamically and gradually slows down and speeds up.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago

    Another excellent post Jan.

     

    Good detail and screen captures so that the reader can easily follow along.

     

    Well done.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<