Power & Energy
  • Technologies
  • More
Power & Energy
Blog
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Researchers Achieve Superconductivity at Room Temperature using Molecule Compression

    Catwell
    Catwell
    By compressing simple molecule solids with hydrogen, the researchers create a new material that achieves superconductivity at room temperature. (Image credit: University of Rochester)  Researchers from the University of Rochester have created a ...
    • 19 Oct 2020
  • Researchers create new process that converts plastic into hydrogen

    Catwell
    Catwell
    Researchers have developed a new process that converts plastic waste into hydrogen and carbon nanotubes. This could be used worldwide in an effort to reduce plastic pollution on land and in oceans, lakes, and rivers. (Image Credit: Antoine GIRET/Unsp...
    • 16 Oct 2020
  • Researchers develop graphene circuit that generates limitless, clean energy

    Catwell
    Catwell
    This circuit could be used to provide limitless, low-voltage, clean power for small devices or sensors. (Image Credit: University of Arkansas) Physicists at the University of Arkansas have developed a circuit that utilizes graphene to produce un...
    • 13 Oct 2020
  • Are Modular Nuclear Reactors Safer?

    Catwell
    Catwell
    NuScale has received a final safety evaluation report for its small modular reactor. The reactor is capable of shutting itself off automatically in case of an emergency. (Image Credit: NuScale Power) According to a statement, NuScale received a ...
    • 9 Oct 2020
  • NDB’s proof-of-concept self-charging battery can last for up to 28,000 years

    Catwell
    Catwell
    NDB states that its proof-of-concept battery can outlast lithium-ion batteries and won’t need to ever be recharged since it acts like a self-charging generator. It can last anywhere from 10 to 28,000 years. (Image Credit: NDB) Wouldn’t it be ama...
    • 9 Oct 2020
  • Obermeyer Hydro designs new pumped-hydro system

    Catwell
    Catwell
    The new pumped-hydro design leverages water to add more solar and wind power onto the grid. (Image Credit: NREL) In a collaborative effort with the National Renewable Energy Laboratory (NREL) and other firms, Obermeyer Hydro Inc. designed a new ...
    • 8 Oct 2020
  • What is a metal-air battery and how does it help solve thermal runaway?

    Catwell
    Catwell
    This patent can help solve thermal runaway issues in EV batteries. The mitigation solution involves combining a lithium-ion battery with a metal-air one to prevent it from catching fire. (Image Credit: USTPO) Other than increasing energy density...
    • 5 Oct 2020
  • MIT’s lithium-metal battery could change the world

    Catwell
    Catwell
    This liquid metal battery could replace lithium-ion batteries to provide power to hospitals, manufacturing facilities or a subdivision of several hundred homes. (Image Credit: MIT) The problem with intermittency in non-fossil fuel electricity ge...
    • 2 Oct 2020
  • Researchers discover thermoelectricity response can be changed by factors in nanoscale gold wires

    Catwell
    Catwell
    An image taken by a scanning electron microscope reveals a single-crystal gold nanowire on a thermal oxide substrate. (Image Credit: Natelson Research at GroupRice University) Utilizing an advanced optical detection system, researchers at Rice Unive...
    • 1 Oct 2020
  • Measure Unknown Inductor Value with Function Generator and Oscilloscope

    Jan Cumps
    Jan Cumps
    There are affordable switch mode DC converters available.One that you see often is this Benq 12 V to 5V converter.I can find info on all components, except the inductor. And I don't have an inductance meter.There are several other ways to measure ind...
    • 26 Sep 2020
  • Check out a scrap switch mode Transformer

    Jan Cumps
    Jan Cumps
    When I saw Michael's post on a power supply for the Archeology Resistivity Meter that's being designed here in the community, I remembered I have a switch mode transformator in my scrap parts box.It's there since forever. I unsoldered it ...
    • 26 Sep 2020
  • The effect of a BMS when measuring LIBs

    cookmesomekai
    cookmesomekai
    There is a not so surprising trend to replace lead-acid batteries used in all kind of systems or devices with lithium-ion batteries (LIBs). When checking lead-acid batteries in these devices or systems by service technicians then often a battery test...
    • 20 Sep 2020
  • QuantumScape’s new solid-state batteries could be used in EVs by 2025

    Catwell
    Catwell
    QuantumScape says it has developed a new battery technology that could be utilized in EVs by 2025, and it has more advantages over lithium-ion. (Image Credit: QuantumScape) QuantumScape, a 10-year old startup based in California, says it has res...
    • 8 Sep 2020
  • Did I really commit a "capital sin" using those brass tabs?

    cookmesomekai
    cookmesomekai
    The other day I posted something in this group about how temperature affects a battery measurement because I wanted to find out how much that impact actually is. There was great feedback regarding this post in the comments (thank you very much for th...
    • 6 Sep 2020
  • Orange-tinted solar panels can generate electricity while growing vegetables

    Catwell
    Catwell
    The orange-tinted solar panels could be utilized in the future, allowing farmers to generate electricity while producing vegetables. (Image Credit: University of Cambridge)  In the future, farmers could grow their crops indoors underneath tinted...
    • 3 Sep 2020
  • Researchers in Norway paint a wind turbine blade black to reduce bird deaths by up to 70%

    Catwell
    Catwell
    Painting a blade black can dramatically reduce the number of birds killed by wind turbines by up to 70%. (Image Credit: May et al. ./Ecology and Evolution/Wiley Online Library) The number of birds killed by wind turbines per year could be drasti...
    • 1 Sep 2020
  • Battery makers in Europe to make a green recovery

    Catwell
    Catwell
    Northvolt’s factory, which is under construction, is set to be complete next year. The company is aiming to  (Image Credit: Northvolt)  European battery makers are getting ready to take advantage of huge “green” stimulus packages unveiled s...
    • 28 Aug 2020
  • Researchers develop capacitors with amazingly high energy density

    Catwell
    Catwell
    To create the material, the thin film is deposited via a pulsed-laser deposition process in the chamber. The bright plume represents the laser hitting the target and depositing the material. (Image Credit: Lane Martin, Berkeley Lab) Even though ...
    • 27 Aug 2020
  • How temperature affects battery measurements

    cookmesomekai
    cookmesomekai
    A widely used and very popular battery tester in the maintenance sector is HIOKI's handheld BT3554. In less than three seconds it precisely measures the battery resistance at 1000 Hz as well as the battery voltage and it lets you make pass / fail...
    • 26 Aug 2020
  • Researchers turn common bricks into supercapacitors

    Catwell
    Catwell
    A research team has developed a method to turn common red bricks into an energy storage solution. (Image credit: University of Washington) The growth of solar panels and wind turbine energy solutions may be great for renewable energy, but it pos...
    • 26 Aug 2020
  • Researchers develop structural zinc-air battery that could provide 72x more energy for robots

    Catwell
    Catwell
    The researchers successfully demonstrated the new zinc-air battery in the scorpion and worm toy robots. (Image Credit: University of Michigan) Current stand-alone batteries are inefficient, too large, add significant mass to any robot design, an...
    • 24 Aug 2020
  • Epishine LEH Solar Cell Evaluation Kit Review

    dougw
    dougw
    Epishine is about to launch this interesting light energy harvesting (LEH) kit and has provided some early samples for evaluation. UnboxingHere is an unboxing showing what might be expected in the kit:www.youtube.com/watch LEH Kit FeaturesB...
    • 24 Aug 2020
  • Researchers efficiently convert solar energy into hydrogen fuel

    Catwell
    Catwell
    Researchers could make the conversion from solar energy to hydrogen fuel more efficient by using the machinery of photosynthesis. (Image Credit: Clay Banks, Unsplash) Scientists from the Israel Institute of Technology have achieved record effici...
    • 20 Aug 2020
  • STM32H7B3I - TouchGFX Application Framework: A Mock GUI - Show Statuses, Switch Screens

    Jan Cumps
    Jan Cumps
    I'm selected for the STM32H7B3I-DK -  DISCOVERY KIT road test.I'm working on a touch screen GUI for my electronic load.In this post I'm trying a mock interface - see how I can switch between screensThank you fellow roadtester jomoenginer for sen...
    • 19 Aug 2020
  • Solar Energy Harvesting with Epishine Flexible Solar Cell - Pt 4: Battery Backup

    Jan Cumps
    Jan Cumps
    I received a preview of a light harvesting kit from Epishine and element14. Check my intro here.In this post, I'm checking the behaviour when you provide backup coin cell. players.brightcove.net/.../index.html The setup is identical to the ...
    • 16 Aug 2020
<>