Test & Tools
  • Technologies
  • More
Test & Tools
Blog Keithley DMM6500: Trigger from External Trigger Input in LabVIEW
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 26 Jan 2019 5:17 PM Date Created
  • Views 4462 views
  • Likes 5 likes
  • Comments 2 comments
  • RoadTest
  • dmm6500
  • rt
  • keithley
  • labview
  • scpi
Related
Recommended

Keithley DMM6500: Trigger from External Trigger Input in LabVIEW

Jan Cumps
Jan Cumps
26 Jan 2019

I'm road testing the  Keithley Bench Digital Multimeter DMM6500.

In this post, I investigate how to use the external trigger to start a measurement.

image

In this post, everything is configured and executed in LabVIEW. In the previous post I used the front panel.

 

 

Goal: I want to measure the voltage on a microcontroller GPIO pin just after it is set to high.

Check out the last post for the details.

 

Set Up the External Trigger with LabVIEW

 

I'm using the SCPI :TRIGger:LOAD "LogicTrigger" command to set up the trigger model.

That one can be used to configure the external input.

image

 

 

The string I pass to the SCPI call is: 7, 7, 1, 0, "triggerbuff".

image

parameters:

  1. 7: the external trigger in as active digital input
  2. 7: not used. It enables the external trigger out.
  3. 1: make one measurement
  4. 0: no delay after trigger
  5. "triggerbuff": I created a custom buffer to capture the measurement for this exercise. You can also use one of the 2 standard buffers.

 

edit: this approach sets the meter up to trigger on the falling edged of the external trigger in. That's not what I want.

I had to add a block to reconfigure to the rising edge.

Here's the addition. The LabVIEW project attached to this post is updated.

 

image

 

I think I found an error in that Keithley LabVIEW Configure Event Input block.

I logged a topic on the instrument's forum: https://forum.tek.com/viewtopic.php?f=617&t=141442

 

 

Run the LabVIEW Flow

 

In this short video you can see the meter display updating in real time when I execute the Trigger Template block in LabVIEW:

 

image

 

This is the form used to execute the LabVIEW flow:

image

The flow itself - the trigger part of it - is shown at the top of this post.

I adapted the existing Keithley example Keithley DMM6500 DAQ6500 Series Measuring DCV With High Accuracy DCV.

If you want to view the whole flow, I've attached it to this post.

Related Blog
Keithley Bench Digital Multimeter - Review
Software Control Options Pt 1 - TSP Script Builder, LabVIEW, Web Interface
TSP Script Example - Measure Power
How to Create a Bitmap for a Custom App
Verify a µCurrent Manually
Verify a µCurrent in an Automated Setup
Measure Amp-Hours of a microcontroller with a µCurrent
Trigger from External Trigger Input
Trigger from External Trigger Input in LabVIEW
Software Control Options Pt 2 - Test Commands with Communicator
App to Hold Measurements

Store Multiple Measurements Manually

Script Example - Externally Triggered Measurements
Attachments:
example projects.zip
  • Sign in to reply
Parents
  • svasenius
    svasenius over 7 years ago

    Did you find solution for that triggering bug?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to svasenius

    yes. It’s documented in the post I made on the tek forum: https://forum.tek.com/viewtopic.php?f=617&t=141442

    I changed EXT:IN to EXT 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to svasenius

    yes. It’s documented in the post I made on the tek forum: https://forum.tek.com/viewtopic.php?f=617&t=141442

    I changed EXT:IN to EXT