Test & Tools
  • Technologies
  • More
Test & Tools
Forum MULTICOMP PRO MP750065 Function Generator - 1st impressions
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 382 subscribers
  • Views 12616 views
  • Users 0 members are here
  • MP750065
  • arbitrary
Related

MULTICOMP PRO MP750065 Function Generator - 1st impressions

Jan Cumps
Jan Cumps over 4 years ago

Since yesterday, I have a MP750065  function generator and counter.

image

Specs:

  • DC to 5 MHz
  • 1 µHz resolution
  • 5 Vpp in 50Ω (10 Vpp in high impedance)
  • sine, pulse and flank (triangle)
  • variable duty cycle for pulse. For the other two waveforms this function changes the symmetry
  • Sweep linear and Log, start, end and speed are configurable
  • AM and FM modulation, with external input
  • Sync output, can be used to trigger an oscilloscope while sweeping
  • arbitrary waveforms, 20 preloaded. 20 custom waves can be stored
  • power output that can drive 4W, with a 200 kHz upper limit.
  • counter up to 100 MHz
  • USB, remote software

Unexpected specs:

  • it's SCPI programmable. This is not mentioned on the e14 shops, but a great feature
  • the OEM is UNI-T. This device is the twin of the UTG900C-II

First Use 

The basic functionality is easy to use: switching the traditional wave forms, frequency, amplitude. Even duty cycle.
I got started with the instrument in minutes. It shows a default waveform when switching the device and output on. A 1 kHz, 100 mVpp (in 50Ω) sine wave.
Because the popular parameters can be set with function keys, altering that form just works as you'd expect it to.

A few other functions, such as the output impedance switch from high to 50Ω were less intuitive, but I found how to do that without reading the manual too.
Once you go to the more advanced functions, like sweep setup, you'll need the manual the first few times. It's not difficult, but they require that you know the steps.

I haven't used the arbitrary functionality or the counter yet.

Teardown

(I did a more detailed teardown in a later post)

I took a look inside. Mainly two sections: power supply at the back, Instrument and user interface up front. The middle of the box is empty.
To remove front and back, you pull the baby bumpers on both sides. There's a screw under each of them. The connection point of the bumpers is near the end. Releasing and re-fixing them is easy and requires little force.


image

You can then carefully pull both ends of the instrument from the housing. If you disconnect a few cables, you can remove them fully. I haven't done that.

Here are a few photos of the PSU at the back:

image

image

… and some of the instrument side. Spot the ARM and FPGA.

image

image

image

The next one is unsharp. I added it because it gives a good impression of the front panel's backside.

image

Finally, a peek inside the box:

image

One of the things I learned while peeking inside, is that the PCB had a type number mechanism typically used by UNI-T.
Knowing that MULTICOMP PRO uses OEMs, I went to look online to find the matching model. It's the UTG9000C-II.
It has the identical looks, specs and user documentation. But also a programmer's guide that's not available on AVNET's shops.
There I found that this device should be SCPI controllable. I'll test this out with LabVIEW at a later time.

edit after investigation: it is LabVIEW programmable - but not your typical NI-VISA and SCPI approach. It automates well though.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Thank you for reading.

Related blog:

MULTICOMP PRO MP750065 Function Generator - 1st impressions
Programming Pt1: SDK Demo
Programming Pt2: LabVIEW tryout (a)
Programming Pt3: LabVIEW tryout (b)
Programming Pt4: LabVIEW Driver Lib Init block
Programming Pt5: LabVIEW Driver Lib Read, Write and Close blocks
Programming Pt6: LabVIEW Driver Lib: High Level Functional blocks
Repair and teardown
  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 4 years ago in reply to Jan Cumps +3
    I have had similar experiences with the MP750668 which is *very* similar to the UTG1010. None of the included software functioned, but I did manage to talk to the instrument with uni-t SDK demo applic…
  • misaz
    misaz over 4 years ago in reply to Jan Cumps +3
    Owon is official owner of VID 5345 but see the sequences 1234. When you see something like this in USB descriptor, most probably the device is not manufactured by Owon but someone who do not own VID range…
  • michaelkellett
    michaelkellett over 4 years ago +2
    Nice first look Jan. Interesting to see it's a TxDAC AD9764 from Analog, 14 bit 125Ms/s part and the FPGA is a pretty simple ALtera Max10 part. and a fairly light weight ARM M0 with 16kRAM on chip -…
Parents
  • Jan Cumps
    Jan Cumps over 4 years ago

    For those of us fluent in Dutch, an extensive review of Jos Verstraten from The Netherlands: https://verstraten-elektronica.blogspot.com/p/utg9005c-ii-functiegenerator.html

    His view is similar to mine:

    • great instrument: as per specs, decent and good options
    • software partially not working: the main menu and the remote control know the device and work. The arbitrary waveform software says there's no device connected (and thus isn't usable). See image:
      image

    I did the first attempts to use it in LabVIEW. No success yet.
    With the standard driver delivered with the CD, the device is not recognised as a VISA device. That's normal. I believe I may be able to talk to it via #NET calls that way.
    Without installing the driver, the instrument is using the National Instruments VISA driver. I can connect, but once I try to send commands, it doesn't reply - however long I put the timeout. Also the SCPI testbed I have gets no replies back.

    For the LABView afficionados, a view of my progress:

    image

    I (and a testbed I often use) get timeout on the rightmost VISA block, that reads the results of the command I sent before.
    I tried *IDN?  *IDN?; *IDN?;\n and *IDN?\n\r . I restarted the instrument each time to ensure there was nothing left over from my previous attempt.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 4 years ago in reply to Jan Cumps

    I have had similar experiences with the MP750668 which is *very* similar to the UTG1010. None of the included software functioned, but I did manage to talk to the instrument with uni-t SDK demo application

    image

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to scottiebabe

    edited

    I got the software. When I run the button next to the USB checkbox, I get: 

    [Failed to query devices!], Error id = 0xfffffbdc(hex) , -1060(dec);
    ->Not found any devices!;

    I entered the text in the connect string. It wasn't detected with the query tool. I used the same text as you - it matches my device's USB settings 

    It connects:

    image

    It doesn't like the IDN command though ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    ... although, progress:

    image

    return value success, and the instrument set it's channel 1 (single channel device) to 2 kHz.

    So the reason why I'm struggling is because the *IDN? command is not known. It's the first one in the manual though:

    image

    But not to worry. You got me started. Thank you scottiebabe

    correction it understands IDN? , but I have to submit it in a different way, using the button next to the 50.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to scottiebabe

    First LABView baby steps:

    image

    I'm using this example. It uses the driver that comes with the instrument, not the NI-VISA one.
    At this moment, the only thing it does is open the USB device, configure it, then close.
    Next step is to introduce end points for reading and writing.
    I didn't have that info, but scottiebabe's connection string shows the IDs:

    [EI:0x81][EO:0x3]

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    Reading the current frequency:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    Yandex image translation to the rescue:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 4 years ago in reply to Jan Cumps

    Woohoo! This is wonderful to hear! I had similar experiences to you. The arb enumerated as a usb T&M dev, so I was hoping I could just send scpi commands in a VISA connection but that didn't work. The software included on cd didn't ever connect to the device. Eventually I found this SDK and the demo app worked! :) I could read the SERNO, and set the frequency. Happy to hear your able to make a usb connection too! Trying to get the dll working in matlab is still on my todo list Stuck out tongue

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 4 years ago in reply to Jan Cumps

    This is super helpful! Thank-you :) 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to scottiebabe

    What I can't get to work automated is the counter.

    The register in the UTG1000L and UTG9000L do not list the registers for that functionality, or the command to switch to that function.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 4 years ago in reply to Jan Cumps

    Good question. I have yet to try that. I tried the freq command for oscilloscope's but it didn't work Disappointed

    image

    https://instruments.uni-trend.com/static/upload/file/20210904/UTD2000CM%20Programming%20Manual.pdf

    I can take screenshots though Shrug

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • scottiebabe
    scottiebabe over 4 years ago in reply to Jan Cumps

    Good question. I have yet to try that. I tried the freq command for oscilloscope's but it didn't work Disappointed

    image

    https://instruments.uni-trend.com/static/upload/file/20210904/UTD2000CM%20Programming%20Manual.pdf

    I can take screenshots though Shrug