Test & Tools
  • Technologies
  • More
Test & Tools
Documents Programmable Electronic Load - Analyse the Summing Node Zero Point
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 1 Dec 2017 4:08 PM Date Created
  • Last Updated Last Updated: 15 May 2020 3:38 PM
  • Views 12858 views
  • Likes 8 likes
  • Comments 107 comments
Related
Recommended

Programmable Electronic Load - Analyse the Summing Node Zero Point

This blog documents investigates the feedback node of the electronic load that Robert Peter Oakes, jc2048 and Jan Cumps are designing.

It's an important spot in the load's design. It measures the set point and the feedback from the output.

When the output is driven to 0, it should be on a potential as close as possible to 0 V.

On the first prototype it's -0.2 V. Not so much off, but the negative value  influences our ADC measurements.

This document checks how we can get this node to 0 V.

image

 

Because this document is evolving, some comments below may be out of sync with the content. That's because the content is adapted based on the conversation.

The measurements taken here are based on the original design, without R32 in place and U3B + tied to ground.

The current sense side of R7 is connected to ground, and a variable negative voltage from 0 V down is applied to the current sense side of R8 to simulate current being sensed.

 

The circuit isn't complex. The set point is driven by a DAC. It's set to 0 for this test.

The second input to this node is OpAmp 3C. It has both inputs tied to ground so should theoretically have 0 V at the output.

On my board I measure a potential of -0.212V at the left side of R33.

I hope to get this closer to 0 V to ease the ADC a bit - its performance degrades with negative voltage at its inputs.

Like the other blogs for the electronic load, this is a working document that will be updated with findings from anyone who wants to chime in.

 

Behaviour at 0V

 

buzy image

  • metrology
  • differentiator
  • boosterpack
  • opamp
  • msp432
  • launchpad
  • analog
  • laboratory
  • instrument
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 8 years ago in reply to Robert Peter Oakes +4
    As you say, changing the op-amp is one possibility. There are bipolar op-amps with much lower bias currents, but an alternative nowadays is a precision CMOS op-amp (you'd have to check whether other characteristics…
  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago +3
    To hopefully simplify things a little We have this, Upper op amp is simply to provide an inversion of the measured value back tot he ADC, hence the gain of -1 Lower right op amp measures the volts across…
  • jc2048
    jc2048 over 8 years ago in reply to Jan Cumps +3
    Love the advertisement for "John's excellent probes". It's like one those things from the old days of American TV where the presenter would suddenly turn, look very earnestly at the camera, and start reading…
Parents
  • Jan Cumps
    Jan Cumps over 8 years ago

    I'm going to redo this exercise now that the OpAmps are replaced with lower bias ones and I have more precise measurement tools.

    From the blog Programmable Electronic Load - LabVIEW Test Automation: Characterise the Instrument we can see that the behaviour is very linear.

    But we have a non-0 start point. When th DAC is driven to 0, there is an output current flowing of a few mA.

    image

    I assume that it's our control circuit that's doing that, because if I disable the output (pull the gate to ground), the current that flows is neglectable. And it's the same FET that's fully blocking the current flow then.

     

    I've re-stacked the load so that the control board is on top and I have easier access to the measure point.

    I can't use the LCD display in that case. I'll use the SCPI interface to set values.

    image

     

    I'll measure DAC output and the voltages at relevant control circuit points to see what drives the FET to conduct a little.

    I think I'll document the results in new blog post. We can then think on measures to get the lowest current lower than 2 mA.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 8 years ago

    I'm going to redo this exercise now that the OpAmps are replaced with lower bias ones and I have more precise measurement tools.

    From the blog Programmable Electronic Load - LabVIEW Test Automation: Characterise the Instrument we can see that the behaviour is very linear.

    But we have a non-0 start point. When th DAC is driven to 0, there is an output current flowing of a few mA.

    image

    I assume that it's our control circuit that's doing that, because if I disable the output (pull the gate to ground), the current that flows is neglectable. And it's the same FET that's fully blocking the current flow then.

     

    I've re-stacked the load so that the control board is on top and I have easier access to the measure point.

    I can't use the LCD display in that case. I'll use the SCPI interface to set values.

    image

     

    I'll measure DAC output and the voltages at relevant control circuit points to see what drives the FET to conduct a little.

    I think I'll document the results in new blog post. We can then think on measures to get the lowest current lower than 2 mA.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    I've been checking for a while and get 0.6 µA when measuring with a multimeter. I usd a fairly high input voltage of 14 V to compensate for any cable resistance.