Test & Tools
  • Technologies
  • More
Test & Tools
Documents Programmable Electronic Load - Analyse the Summing Node Zero Point
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 1 Dec 2017 4:08 PM Date Created
  • Last Updated Last Updated: 15 May 2020 3:38 PM
  • Views 11542 views
  • Likes 8 likes
  • Comments 107 comments
Related
Recommended

Programmable Electronic Load - Analyse the Summing Node Zero Point

This blog documents investigates the feedback node of the electronic load that Robert Peter Oakes, jc2048 and Jan Cumps are designing.

It's an important spot in the load's design. It measures the set point and the feedback from the output.

When the output is driven to 0, it should be on a potential as close as possible to 0 V.

On the first prototype it's -0.2 V. Not so much off, but the negative value  influences our ADC measurements.

This document checks how we can get this node to 0 V.

image

 

Because this document is evolving, some comments below may be out of sync with the content. That's because the content is adapted based on the conversation.

The measurements taken here are based on the original design, without R32 in place and U3B + tied to ground.

The current sense side of R7 is connected to ground, and a variable negative voltage from 0 V down is applied to the current sense side of R8 to simulate current being sensed.

 

The circuit isn't complex. The set point is driven by a DAC. It's set to 0 for this test.

The second input to this node is OpAmp 3C. It has both inputs tied to ground so should theoretically have 0 V at the output.

On my board I measure a potential of -0.212V at the left side of R33.

I hope to get this closer to 0 V to ease the ADC a bit - its performance degrades with negative voltage at its inputs.

Like the other blogs for the electronic load, this is a working document that will be updated with findings from anyone who wants to chime in.

 

Behaviour at 0V

 

buzy image

  • metrology
  • differentiator
  • boosterpack
  • opamp
  • msp432
  • launchpad
  • analog
  • laboratory
  • instrument
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 8 years ago in reply to Robert Peter Oakes +4
    As you say, changing the op-amp is one possibility. There are bipolar op-amps with much lower bias currents, but an alternative nowadays is a precision CMOS op-amp (you'd have to check whether other characteristics…
  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago +3
    To hopefully simplify things a little We have this, Upper op amp is simply to provide an inversion of the measured value back tot he ADC, hence the gain of -1 Lower right op amp measures the volts across…
  • jc2048
    jc2048 over 8 years ago in reply to Jan Cumps +3
    Love the advertisement for "John's excellent probes". It's like one those things from the old days of American TV where the presenter would suddenly turn, look very earnestly at the camera, and start reading…
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Robert Peter Oakes

    Robert Peter Oakes  wrote:

     

    To hopefully simplify things a little

     

    We have this,

     

    Upper op amp is simply to provide an inversion of the measured value back tot he ADC, hence the gain of -1

    Lower right op amp measures the volts across the shunt and amplifies it tot he same range as the set point from DAC

    Lower left op-amp integrates the difference of the two (Based on value of summing junction) so if the sum is not zero then the integrator will attempt to correct it by driving the mosfet more on or off..

    image

     

     

    So simplifying the diagram we end up with this

    image

    if the measured value is equal and opposite to the set point then the sum junction will of course be zero, this relies on the two resistors being the same value, if not perfect then it can be corrected in software.

    All the silicon is to get the ranges the same and of the correct polarities for this to work, also the integrator is relied upon to make fast changes if the difference is great and small slower changes as they get close together, all pretty standard stuff

     

    What I think Jan is seeing is a none zero value at the sum when in fact it should be zero, this could be the resistors are not the same value but the SP and Actual are the same but opposite.

     

    Also consider that the meter you measure with is 10MOhm input impedance (May be less but probably this, check the meter manual)  this will have a measurable affect on the sum junction, perhaps 1% (10M in parallel with 100K), it may be better to use a high impedance meter if you have one or use the output of the integrator as you guide. (Or do the math to see what you would actually expect with 100K in series with 100K and 10M in parallel

    Robert Peter Oakes, thanks for the scenario. What I am investigation is if we can avoid negative voltage at the ADC A pin. On my device it's -0.2 V and that doesn't impact the measurements of ADC channel B, C and D.

    I'd have to see how much below zero we can have before the ADC starts to error (all channels are 30% off with -0.8 V on ADC A), and then check how we can control that this situation doesn't occur.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to DAB

    DAB  wrote:

     

    Nice update.

     

    Can you elaborate on which performance parameters are affected by the negative voltage inputs?

     

    Thanks

    DAB

    thank you DAB.

    when there’s a substantial negative value on ADC channel A, all sampled readings - also channel B, C and D - are wrong.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Robert Peter Oakes

    Robert Peter Oakes  wrote:

     

    I just noticed that you have a 680K going from the UC3 + to ground, this should not be populated and will throw things off in the real circuit when the common mode volts start being applied etc.

    this isn’t populated. it’s there for experimental reasons but not part of our BOM.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago

    Been thinking about it some more, to add to my previous comments, if the inputs are static then the value at the summing junction will be static but if it is marginally off from 0V possibly due to the difference in value of the 2 100K resistors (Or did you put in 0.0000000000001% resistors image ), then the output of the integrator will ultimately drift one way or the other, it is designed to do this, its an integrator. so if the input measured value is not adjusting to reflect this change int he integrator output and that would be in an opposite direction to the error, it will continue to drift until it hits a supply rail or close to it.

     

    In summary, you cant measure the output of the integrator in a static test as no matter how hard you try, there will always be some error that will cause it to drift. a small error and slowly perhaps but still drift never the less

     

    I hope this will close this concern

    Peter

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago

    I just noticed that you have a 680K going from the UC3 + to ground, this should not be populated and will throw things off in the real circuit when the common mode volts start being applied etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago

    To hopefully simplify things a little

     

    We have this,

     

    Upper op amp is simply to provide an inversion of the measured value back tot he ADC, hence the gain of -1

    Lower right op amp measures the volts across the shunt and amplifies it tot he same range as the set point from DAC

    Lower left op-amp integrates the difference of the two (Based on value of summing junction) so if the sum is not zero then the integrator will attempt to correct it by driving the mosfet more on or off..

    image

     

     

    So simplifying the diagram we end up with this

    image

    if the measured value is equal and opposite to the set point then the sum junction will of course be zero, this relies on the two resistors being the same value, if not perfect then it can be corrected in software.

    All the silicon is to get the ranges the same and of the correct polarities for this to work, also the integrator is relied upon to make fast changes if the difference is great and small slower changes as they get close together, all pretty standard stuff

     

    What I think Jan is seeing is a none zero value at the sum when in fact it should be zero, this could be the resistors are not the same value but the SP and Actual are the same but opposite.

     

    Also consider that the meter you measure with is 10MOhm input impedance (May be less but probably this, check the meter manual)  this will have a measurable affect on the sum junction, perhaps 1% (10M in parallel with 100K), it may be better to use a high impedance meter if you have one or use the output of the integrator as you guide. (Or do the math to see what you would actually expect with 100K in series with 100K and 10M in parallel image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 8 years ago

    Nice update.

     

    Can you elaborate on which performance parameters are affected by the negative voltage inputs?

     

    Thanks

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<