Experimenting with Vibration Sensors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Vibration Sensors
  • More
  • Cancel
Experimenting with Vibration Sensors
Blog Vibration Sensor - Wrap Up
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
  • Author Author: ralphjy
  • Date Created: 23 Jan 2021 3:46 PM Date Created
  • Views 843 views
  • Likes 5 likes
  • Comments 0 comments
  • experimenting_with_vibration_sensors
  • kemet vibration sensor
  • edge impulse
  • wio terminal
  • footstep detection
Related
Recommended

Vibration Sensor - Wrap Up

ralphjy
ralphjy
23 Jan 2021

Experimenting with Vibration Sensors Challenge Summary

It has been another fun challenge.  I was not able to achieve what I had proposed (TinyML model to identify people by their footstep vibrations), but as always I learned a lot working on the project.  And I've developed some hardware and software tools that will be valuable for future projects.

 

The Kemet/Tokin VS-BV203 Piezo Vibration Sensor is ultra compact (8.4 x 11.4 x 2.9 mm) and the 3 meter miniature flexible cable makes it easy to attach to instrumentation at a reasonable measurement distance.  It has a sensitivity of 10 m/s^2 and a buffered voltage output that centers the output at 1/2 the power supply voltage which makes it easy to interface to an ADC.

 

The sensor was probably not a good choice for my application (or at least my implementation).  I think a more traditional seismic sensor with mechanical amplification might have worked better.  From papers that I've been able to find on footstep detection/classification, it seems that the problem is best solved with an array of sensors rather than a single sensor.  And in some cases audio sensors are utilized rather than seismic sensors to detect the footsteps.  In all cases, a lot of data is required (a couple orders of magnitude greater than what I had proposed).  I think a viable solution would require automatic data capture and automatic data labeling to deal with the large volume of data.  A possible implementation could use a camera and image recognition for triggering and labeling the data capture.

 

I think a better TinyML application for the Kemet sensor that I'd like to try is monitoring my HVAC system.  I've always wanted to install a smart, network connected, thermostat.  I could use information from the thermostat to trigger and label data captured from the sensor mounted on the HVAC unit.  Then, I could try to use TinyML for Predictive Maintenance.  Something to think about.....

 

Thanks to Element14 for the challenge opportunity.

   

 

Links to my other blogs for this challenge

Person Identification using Footstep Vibration Patterns

Vibration Sensor Setup

Vibration Sensor - First Look

Vibration Sensor - Data Capture Setup

Vibration Sensor - Data Capture Program

Vibration Sensor - Upload to Edge Impulse

Vibration Sensor - Evaluating the data

Vibration Sensor - Impulse Design?