N-gaged Design Challenge
  • Challenges & Projects
  • Design Challenges
  • N-gaged Design Challenge
  • More
  • Cancel
N-gaged Design Challenge
N-Gaged Blog PV Monitor #4 - The great pretender (2)
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Leaderboard
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: amgalbu
  • Date Created: 6 May 2022 5:57 AM Date Created
  • Views 2315 views
  • Likes 7 likes
  • Comments 2 comments
  • n-gaged design challenge
  • pvmonitor
  • iot system
  • OMEGA’s Layer N EcoSystem
  • n-gaged
  • remote monitoring
Related
Recommended

PV Monitor #4 - The great pretender (2)

amgalbu
amgalbu
6 May 2022
Blogs in this series
PVMonitor #1 - Unboxing and project description
PVMonitor #2 - Getting started
PVMonitor #3 - The great pretender (1)
PVMonitor #4 - The great pretender (2)
PVMonitor #5 - Installation and preliminary data
PVMonitor #6 - Anomaly detection
PVMonitor #7 - System performances
PVMonitor #8 - Anomaly detection (2)
PVMonitor #9 - Conclusions
 
 
In this post I will complete the implementation of the protocol converter by adding the support for the Delta Solivia protocol
 
1. Inverter interface
Delta Solivia inverters can communicate with external equipment via an RS485 interface, located at the bottom of the inverter itself
image
The connector is a standard RJ45 (the same connector used for LAN cables) and the pinout is shown in diagram below
image
We need to connect only pin 6 and 7. Inverter user manual suggests to connect a 120 Ohm terminating resistor. However, since connection cable is quite short and transmission speed is low, this will not matter much, but you may run into trouble with long cables.
image

2. Delta Solivia protocol description

Delta Solivia inverters use a simple serial protocol over RS485. The default baud rate by default is 19200 bits per second, although this can be changed in the inverter settings. You may need to lower it if you have a really long cable, otherwise the default should be fine. The RS485 bus-ID can also be set for each inverter. The default value is 001, but each inverter should be given a unique ID if they're connected to the same bus. The bus needs to have a terminating resistor at each end, the inverters are fitted with a DIP-switch next to the RS485-connector to enable (1) or disable (0) bus termination.

Messages on the RS485-bus look like this:

Size Name Value Description
1 byte STX 0x02 Start of message
1 byte ENQ Enquiry type (0x05 for requests, 0x06 for responses)
1 byte Inverter ID
1 byte LEN Number of bytes to follow, excluding CRC and ETX
2 bytes CMD command and subcommand e.g. 0x10 0x02 to request the current DC voltage, 0x10 0x02 to request the current DC current, etc.
LEN-2 bytes data bytes
2 bytes CRC CRC-16, over preceding bytes excluding STX, LSB first (little-endian)
1 byte ETX 0x03 End of message
Unfortunately, the protocol is supposed to be proprietary and, for this reason, limited documentation is available. On some forums, I found some information about the supported commands but looks like each Delta inverter model implements its own dialect of the protocol, where commands and responses vary.
So a bit of reverse engineering is required here.
First of all, I installed the Delta Solivia Solar inverter service app on my PC. This is an application Delta (the manufacturer of the Solivia inverters) makes available to its distributors and installers and can be download from Delta's website.
Here are two screenshots of Delta Solivia Solar inverter service application with the measures I want to read
 
imageimage
 
I connected two USB-to-RS485 converters to my PC. The first converter will be used by the inverter service app to communicate with the inverter, the latter will be used to sniff the serial traffic. By comparing the values being displayed by the application and the serial packets, it was quite easy to decode the function of (almost) every command. Here is a list of command codes I decoded
Request Response Value Meaning
[02][05][01][02][00][01][AD][FC][03] [02][06][01][0C][00][01][30][30][30][30][30][30][37][38][39][34][2D][D0][03] 0000007894 Serial number
[02][05][01][02][10][02][E0][3D][03] [02][06][01][04][10][02][01][88][32][E7][03] 0x0188 DC voltage (actual)
[02][05][01][02][11][02][E1][AD][03] [02][06][01][04][11][02][01][78][33][5F][03] 0x0178 DC voltage (average)
[02][05][01][02][10][01][A0][3C][03]
[02][06][01][04][10][01][00][09][03][17][03] 0x0009 DC current (actual). Unit is 0.1 A
[02][05][01][02][11][01][A1][AC][03]
[02][06][01][04][11][01][00][05][02][EE][03] 0x0005 DC current (average). Unit is 0.1 A
[02][05][01][02][11][03][20][6D][03]
[02][06][01][04][11][03][00][D7][23][73][03] 0x00d7 DC power
[02][05][01][02][21][04][75][AF][03]
[02][06][01][04][21][04][07][D0][DE][40][03] 0x07d0 Isolation (actual, MOhm)
[02][05][01][02][11][0F][20][68][03]
[02][06][01][04][11][0F][07][DA][20][85][03] 0x07da Isolation (average, MOhm)
[02][05][01][02][10][08][60][3A][03]
[02][06][01][04][10][08][00][EC][12][9E][03] 0x00ec AC Voltage (actual)
[02][05][01][02][11][08][61][AA][03]
[02][06][01][04][11][08][00][EA][93][60][03] 0x00ea AC Voltage (average)
[02][05][01][02][10][07][20][3E][03]
[02][06][01][04][10][07][00][11][E3][1C][03] 0x0011 AC current (actual). Unit is 0.1 A
[02][05][01][02][11][07][21][AE][03]
[02][06][01][04][11][07][00][0B][63][2B][03] 0x000b AC current (average). Unit is 0.1 A
[02][05][01][02][10][09][A1][FA][03]
[02][06][01][04][10][09][01][72][C3][66][03] 0x0172 AC power (actual)
[02][05][01][02][11][09][A0][6A][03]
[02][06][01][04][11][09][00][EE][C3][63][03] 0x00ee AC power (average)
[02][05][01][02][21][06][F4][6E][03]
[02][06][01][04][21][06][00][1B][3C][27][03] 0x001b DC NTC Temperature
[02][05][01][02][20][05][B5][FF][03]
[02][06][01][04][20][05][00][18][8D][DA][03] 0x0018 AC NTC Temperature
 
Let's split one of the requests to see each part in detail
 
[02] STX
[05] ENQ
[01] Inverter ID
[02] Number of data bytes
[21][06] Command and subcommand (DC NTC Temperature in this case)
[F4][6E] CRC-16
[03] ETX
 
Let's now split the response
 
[02] STX
[06] RESPONSE
[01] Inverter ID
[04] Number of data bytes
[20][06] Command and subcommand (the same of the request)
[00][1B] 16-bit value of the requested parameter
[3C][27] CRC-16
[03] ETX
​ 
UPDATE: I added some other data, namely the daily yield
 
image
 
which can be read by means of the following request
 
Request Response Value Meaning
[02][05][01][02][13][03][21][0D][03] [02][06][01][04][13][03][00][AE][E3][29][02] 0x00AE (174) Daily yield (Wh)
 
3. Implementation

To implement the Delta Solivia protocol, I started from this project. I had to make some changes to use python3 (the library was written to support python2) and to use the correct commands.

Here is a brief description of the functions involved

3.1 solivia_readData

This function reads a specific value from the Delta Solivia inverter (DC power, AC power, etc).  The only caveat here is that I had to add a check to remove some trailing 0xff characters that are probably mistakenly read by the USB-to-RS485 converter when inverter drives RS485 from RX to TX.

def solivia_readData(s):
    log.debug("Reading %s"%(s))

    cmd = solivia_inverter.getCmdStringFor(s)
    log.debug("Command: %s"%binascii.hexlify(cmd))
    solivia_connection.write(cmd)
    rawResponse = solivia_connection.read(100)

    cntr = 0
    while (cntr < len(rawResponse) and rawResponse[cntr] == 0xff):
       cntr += 1

    response = rawResponse[cntr:]

    floatValue = float("0")
    if response:
        log.debug("Received response %s\n"%binascii.hexlify(response))

        value = solivia_inverter.getValueFromResponse(response)
        #log.debug("Value %s"%value)
        if solivia_isFloat(value):
            floatValue = float(value)

    return floatValue 

The code leverages functions in the deltaInv.py file to extract a value as a floating point number from the inverter response

3.2 solivia_updateChannel

This function updates all the Modbus registers required to mimic one of Omega OM240 channels. The following Modbus registers are initialized

  • 2 16-bits registers with the value
  • 8 16-bits registers with the timestamp string
  • 1 16-bits registers with the flags

Here is the code

def solivia_updateChannel(ch, value, ts):
    """ Registers are as follow
    0-1 Input A (IEE754)
    2-3 Input B
    4-5 Temperature
    6-14 Timestamp "dd/mm/yy hh:mm:ss"
    15  Flags
    """
    vHex = solivia_floatToHex(value)[2:]
    log.debug("value=%f, vHex=%s"%(value,vHex))
    stime = ts.strftime("%d/%m/%y %H:%M:%S").encode('utf-8').hex().ljust(36, '0')

    values = [int(vHex[0:4],16), int(vHex[4:8],16),
                 0, 0,
                 0, 0,
              int(stime[0:4],16), int(stime[4:8],16), int(stime[8:12],16), int(stime[12:16],16), int(stime[16:20],16), int(stime[20:24],16), int(stime[24:28],16), int(stime[28:32],16), int(stime[32:36],16),
                 3]
    return values 

 

3.3 solivia_reader

This functions reads all the measures and update the corresponding channels

def solivia_reader(a):
    """ A worker process that runs every so often and
    updates live values of the context. It should be noted
    that there is a race condition for the update.
    :param arguments: The input arguments to the call
    """
    log.info("Updating inverter data\n")

    dcVolts = solivia_readData('DC Volts1')
    dcCur = solivia_readData('DC Cur1')
    dcPow = solivia_readData('DC Pwr1')
    acVolts = solivia_readData('AC Volts')
    acCur = solivia_readData('AC Current')
    acPow = solivia_readData('AC Power')
    acTemp = solivia_readData('AC Temp')
    dcTemp = solivia_readData('DC Temp')

    context = a[0]
    register = 3
    slaveId = 0x00

    address = 0
    values = solivia_updateChannel(0, dcPow, datetime.now())
    context[slaveId].setValues(register, address, values)

    address = 16
    values = solivia_updateChannel(0, acPow, datetime.now())
    context[slaveId].setValues(register, address, values)

    address = 32
    values = solivia_updateChannel(0, acTemp, datetime.now())
    context[slaveId].setValues(register, address, values)

    address = 48
    values = solivia_updateChannel(0, dcTemp, datetime.now())
    context[slaveId].setValues(register, address, values)

    currDate = datetime.now().strftime("%d/%m/%y").encode('utf-8').hex().ljust(10, '0')
    currTime = datetime.now().strftime("%H:%M:%S").encode('utf-8').hex().ljust(8, '0')

    log.debug(currDate+"-"+currTime+" %.6f %.6f %.6f %.6f %.6f %.6f %.6f %.6f OK\n" %(dcVolts, dcCur, dcPow, acVolts, acCur, acPow, dcTemp, acTemp )) 

3.4 Task
Finally, I called the solivia_reader periodically using the Twister LoopingCall function
    log.info("Scheduling task")
    time = 5.0
    loop = LoopingCall(f=solivia_reader, a=(context,))
    loop.start(time, now=True)  # initially delay by time 
That's all for the moment. I will be back soon with photos of the actual installation and some preliminary data!
3.5 Start protocol converter at boot
To start the protocol converter at boot, I added a rule to the crontab. To edit the crontab, enter the command
sudo crontab -e 
and add the following line, which instructs the cron daemon to launch script launcher.sh at boot. Output of the script is redirected to file /home/pi/logs/server.log for debugging purposes
@reboot sh /home/pi/launcher.sh >/home/pi/logs/server.log 2>&1
Script file simple launch the Python interpreter
#!/bin/sh
# launcher.sh
# navigate to home directory, then to this directory, then execute python script, then back home

cd /home/pi/nmodbus
sudo python3 server.py
cd /
Here is the complete content of the crontab
 
# Edit this file to introduce tasks to be run by cron.
#
# Each task to run has to be defined through a single line
# indicating with different fields when the task will be run
# and what command to run for the task
#
# To define the time you can provide concrete values for
# minute (m), hour (h), day of month (dom), month (mon),
# and day of week (dow) or use '*' in these fields (for 'any').
#
# Notice that tasks will be started based on the cron's system
# daemon's notion of time and timezones.
#
# Output of the crontab jobs (including errors) is sent through
# email to the user the crontab file belongs to (unless redirected).
#
# For example, you can run a backup of all your user accounts
# at 5 a.m every week with:
# 0 5 * * 1 tar -zcf /var/backups/home.tgz /home/
#
# For more information see the manual pages of crontab(5) and cron(8)
#
# m h dom mon dow command
@reboot sh /home/pi/launcher.sh >/home/pi/logs/server.log 2>&1
 
The protocol converter will be started every time the Raspberry Pi boots up and the logs will be saved to file /home/pi(logs/server.log
 
  
<< Prev: The great pretender (1)
Next: Installation and preliminary data >>
  • Sign in to reply
Parents
  • Jan Cumps
    Jan Cumps over 4 years ago

    We need to connect only pin 7 and 8. 

    I was expecting 6 and 7, looking at the first drawing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 4 years ago

    We need to connect only pin 7 and 8. 

    I was expecting 6 and 7, looking at the first drawing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • amgalbu
    amgalbu over 4 years ago in reply to Jan Cumps

    Yes, my mistake: I updated the post. Thank you very much!