PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog Hologram Pi-ramid - Plexiglass Pyramid
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
  • Author Author: luislabmo
  • Date Created: 24 Apr 2019 12:22 AM Date Created
  • Views 6094 views
  • Likes 11 likes
  • Comments 15 comments
  • mechanical drawings
  • picasso
  • rpi 3b+
  • addressable led
  • raspberri pi
  • plexiglass
  • rgb
  • touchscreen
  • luislab
  • acrylic_welding
  • acrylic
Related
Recommended

Hologram Pi-ramid - Plexiglass Pyramid

luislabmo
luislabmo
24 Apr 2019

I'm very excited about the progress of the Hologram Pi-ramid. At this point I'm just one step away of testing the Pepper's Ghost principle.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

In the previous blog post, I've covered the 3d printed parts and some assembly. Such parts will help in the construction of the Plexiglass pyramid too as they will provide support when gluing the pyramid which is made of 3 pieces of 2mm thick (0.08 inches) clear Acrylic -also known as Plexiglass among many other names. To cut the Plexiglass I used a Plastic/Laminate Scorer and only needed three or four passes for each cut with clean results. To avoid scratching the Acrylic I added some blue masking tape as can be appreciated in some of the pictures.

 

{gallery:width=960,height=768,autoplay=false} Cutting Plexiglass Pyramid

image

Scoring Plexiglass: Scoring Plexiglass/Acrylic with a Plastic/Laminate Scorer

image

Plexiglass pyramid cutting: Plexiglass pyramid - before cutting preparation

image

Plexiglass pyramid front piece: Front piece (Plexiglass/Acrylic pyramid)

image

Plexiglass pyramid assembly: Technical drawings Acrylic/Plexiglass pyramid

 

To bond all the Plexiglass pieces together I used Methylene chloride, also known as dichloromethane or DCM; a fast drying solvent that welds some plastics by softening the polymer and fusing it together, which I applied with a small blunt tip syringe allowing it to flow along the surfaces to be joined via capillary action. To add support I used some of the 3d printed parts assembled together, a rubber band and a little help of gravity.

{gallery:width=960,height=768,autoplay=false} Gluing the Plexiglass Pyramid

image

Welding Plexiglass: Welding the Plexiglass/Acrylic with Methylene chloride

image

Zoomed-in weld: Zoomed-in Plexiglass/Acrylic weld

As can be appreciated results are very good, the Plexiglass pyramid seems sturdy enough and can be removed/placed in the project easily -as seen on the video- which is one of the features I had planned which I will be covering in more detail in a later entry.

image

 

 

Blogs in this series

 

  1. Hologram Pi-ramid - Intro and initial design
  2. Hologram Pi-ramid - 3D CAD/CAM design
  3. Hologram Pi-ramid - 3D printed parts and initial assembly
  4. Hologram Pi-ramid - Plexiglass Pyramid
  5. Hologram Pi-ramid - My name is Automan
  6. Hologram Pi-ramid - PCB Design
  7. Hologram Pi-ramid - Painting the 3D printed parts
  8. Hologram Pi-ramid - Electronic Parts
  9. Hologram Pi-ramid - Displaying Holograms
  10. Hologram Pi-ramid - Project complete!

 

  • My Picasso Design Challenge entries

 

 

image
3D printed parts and initial assembly

image
My name is Automan

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 7 years ago +6
    Very accurate and nice building. Two important things I have appreciated and never known. The first is the way you joined the transparent parts, I have always used Cyanoacrilate but with your solution…
  • luislabmo
    luislabmo over 7 years ago in reply to dubbie +6
    Hi Dubbie, I think it all boils down to patience and trying and trying. It took me about a month to calibrate my new printer to get smooth prints and the features I add to the 3d printed parts like the…
  • luislabmo
    luislabmo over 7 years ago in reply to balearicdynamics +6
    Hello Enrico, This is the first time I've heard of the Cyanocrilate. If you ever try the D ichloromethane method, the edges that will be welded should be "rough", ironically laser-cut parts are hard to…
Parents
  • kiri-ll
    kiri-ll over 7 years ago

    That's a great progress!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • luislabmo
    luislabmo over 7 years ago in reply to kiri-ll

    Thank you Kiri!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • luislabmo
    luislabmo over 7 years ago in reply to kiri-ll

    Thank you Kiri!