Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog MSP432 and TI-RTOS: another I2C example - talk to a DAC
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
  • Author Author: Jan Cumps
  • Date Created: 28 Feb 2017 3:01 PM Date Created
  • Views 4709 views
  • Likes 6 likes
  • Comments 21 comments
  • safe and sound
  • i2c
  • sketch
  • dac8571
  • safe & sound
  • msp432
  • safe&sound
Related
Recommended

MSP432 and TI-RTOS: another I2C example - talk to a DAC

Jan Cumps
Jan Cumps
28 Feb 2017

How to make an MSP432 LaunchPad talk i2c to a DAC.

image

This TI-RTOS program tells the DAC to output a sine wave. It could be something else but I reused an existing Arduino sketch.

 

In my previous i2c example, the focus was on reading data from a sensor. This one only writes data out. t's not intended to be a useful application, just a test bed to see if the DAC that I have here is listening properly.

 

The schema and code are derived from work of Robert Peter Oakes:

The Modular Bench Power Supply ++, Arduino UNO and precision ADC, DAC + MDO3000 I2C debugging

Raspberry PI 2, Fun with I2C DACs and ADC's

 

If you understand Arduino sketches, look there to understand how the program works. The code below is a fairly true port to TI-RTOS.

 

Schema

image

You can see a BoosterPack in the making here.

The difference with Peter's schema is that I'm using a single DAC (DAC8571). He uses a quad DAC in a single chip. Doesn't matter for this exercise.

Key take-aways from the schema is that we can use the MSP432 to set the output voltage of the DAC.

A voltage reference REF5020 helps the DAC to improve its performance. We don't talk to that chip, it just does its work by being there.

You can think away the i2c isolator ic (ISO1541). It's there to save the laptop's USB port when something happens downstream.

 

image

 

 

Firmware

 

I've copied my own project from the first i2c blog and replaced the part that talks to a temperature sensor with Peter's DAC Arduino code.

 

#define DAC_I2C_ADDR           (0x4C)
#define DAC_I2C               MSP_EXP432P401R_I2CB0

uint16_t Sin_tab[256] = {  32768,33572,34376,35178,35980,36779,37576,38370,39161,39947,40730,41507,42280,
                               43046,43807,44561,45307,46047,46778,47500,48214,48919,49614,50298,50972,51636,
                               52287,52927,53555,54171,54773,55362,55938,56499,57047,57579,58097,58600,59087,
                               59558,60013,60451,60873,61278,61666,62036,62389,62724,63041,63339,63620,63881,
                               64124,64348,64553,64739,64905,65053,65180,65289,65377,65446,65496,65525,65535,
                               65525,65496,65446,65377,65289,65180,65053,64905,64739,64553,64348,64124,63881,
                               63620,63339,63041,62724,62389,62036,61666,61278,60873,60451,60013,59558,59087,
                               58600,58097,57579,57047,56499,55938,55362,54773,54171,53555,52927,52287,51636,
                               50972,50298,49614,48919,48214,47500,46778,46047,45307,44561,43807,43046,42280,
                               41507,40730,39947,39161,38370,37576,36779,35980,35178,34376,33572,32768,31964,
                               31160,30358,29556,28757,27960,27166,26375,25589,24806,24029,23256,22490,21729,
                               20975,20229,19489,18758,18036,17322,16617,15922,15238,14564,13900,13249,12609,
                               11981,11365,10763,10174,9598,9037,8489,7957,7439,6936,6449,5978,5523,5085,4663,
                               4258,3870,3500,3147,2812,2495,2197,1916,1655,1412,1188,983,797,631,483,356,247,
                               159,90,40,11,1,11,40,90,159,247,356,483,631,797,983,1188,1412,1655,1916,2197,
                               2495,2812,3147,3500,3870,4258,4663,5085,5523,5978,6449,6936,7439,7957,8489,9037,
                               9598,10174,10763,11365,11981,12609,13249,13900,14564,15238,15922,16617,17322,
                               18036,18758,19489,20229,20975,21729,22490,23256,24029,24806,25589,26375,27166,
                               27960,28757,29556,30358,31160,31964};

 

Paste these lines of code in that previous i2c example, before the definition of the RTOS task.

The first two lines define the i2c address of the DAC ic and the i2c port f the MSP432 that we'll use.

The Sin_tab is an array with sine wave sample values. Try to paste these values in Excel and make a line graph. You'll see what's happening in there.

 

Then replace the existing RTOS task with this one:

 

Void taskFxn(UArg arg0, UArg arg1)
{
    unsigned int    i;

    uint8_t         txBuffer[3];
    uint8_t         rxBuffer[2];
    I2C_Handle      i2c;
    I2C_Params      i2cParams;
    I2C_Transaction i2cTransaction;


    /* Create I2C for usage */
    I2C_Params_init(&i2cParams);
    i2cParams.bitRate = I2C_400kHz;
    i2c = I2C_open(DAC_I2C, &i2cParams);
    if (i2c == NULL) {
        System_abort("Error Initializing I2C\n");
    }
    else {
        System_printf("I2C Initialized!\n");
    }

    i2cTransaction.slaveAddress = DAC_I2C_ADDR;
    i2cTransaction.writeBuf = txBuffer;
    i2cTransaction.writeCount = 3;
    i2cTransaction.readBuf = rxBuffer;
    i2cTransaction.readCount = 0;

    txBuffer[0] = 0x10;

    while (1) {
        for (i = 0; i< 256; i++) {
            txBuffer[1] = Sin_tab[i] >> 8;
            txBuffer[2] = Sin_tab[i];
            if (I2C_transfer(i2c, &i2cTransaction)) {
            }
            else {
                System_printf("I2C Bus fault\n");
                System_flush();
            }
        }
        Task_sleep(10);
    }

    /* Deinitialized I2C */
    I2C_close(i2c);
    System_printf("I2C closed!\n");
    System_flush();
}

 

The code iterates the array, sends each value to the DAC until it reaches the end.

Then we yield to the RTOS for a while to give other tasks (there aren't any image ) the chance to execute, and start all over.

 

Now pull out the datasheet of the DAC. The combination of code and specifications show the full picture of this example.

This translates to the address 0x4C:

image

 

#define DAC_I2C_ADDR           (0x4C)

 

 

And these three bytes say: set the output value (byte 0 is the command, 1 the most significant byte of the 16 bit value, 2 the least significant one.

 

image

 

    txBuffer[0] = 0x10;

    while (1) {
        for (i = 0; i< 256; i++) {
            txBuffer[1] = Sin_tab[i] >> 8;
            txBuffer[2] = Sin_tab[i];

 

 

 

 

image

 

 

 

TI-RTOS Series
MSP432 and TI-RTOS: Getting Started Pt. 1 - Set Up and 1st RTOS Task
MSP432 and TI-RTOS: Getting Started Pt. 2 - Add an ADC Sample Task
MSP432 and TI-RTOS: Getting Started Pt. 3 - USB with Minimal CPU Use
MSP432 and TI-RTOS: PWM
MSP432 and TI-RTOS: I2C Configuration for Sensors BoosterPack
MSP432 and TI-RTOS: another I2C example - talk to a DAC
MSP432 and TI-RTOS: Sharp LCD BoosterPack
MSP432 and TI-RTOS: PID Library Part 1 - Intro
MSP432 and TI-RTOS: PID Library Part 2 - Real World Example
  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 9 years ago +2
    I don't understand why you're all fussing. The DAC doesn't have the drive that the processor does, but it's still registering an ACK successfully. Much more importantly, when are we going to hear it playing…
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to jc2048 +2
    Answer:
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to Jan Cumps +2
    That will do it lol
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to shabaz

    The one I use is bidirectional for data, unidirectional for the clock (From master to slaves).

    i'm not surprised that there's a voltage, but i'm wondering why it's such a nice square form, the lenght of a typical data pulse. It appears on the data line on both sides of the isolator, by the way (I thought I made a scope capture of that but can't find it back).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Robert Peter Oakes

    I can't see a reason why the 1541 shouldn't do:

    image

    I have a REF5020 (a 2V ref) instead of a 5040, and 3V3 at the business side, but all is within the specs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to Jan Cumps

    Hi guys,

     

    I think that could be due to the isolator device, I've not used that particular one, but they have a tricky task to perform because the bus is bidirectional, and so they do use slightly unusual levels depending on which side of the isolator is doing the pulling to 0V. Some have certain requirements like they must be only used one way around (i.e. one side is compatible with a higher bus voltage than the other side).

    But I didn't check the circuit in detail, so I could be totally wrong.

     

    EDIT: The datasheet too specifies that the output level on one particular side will be between 0.65 and 0.8V (section 6.9).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Jan Cumps

    (although in an i2c setting, no-one is supposed to pull a signal up except for the resistors...)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Robert Peter Oakes

    I haven't delved into that yet. I've seen them too - almost as if two I2C chips are fighting to pull the signal in two directions. I'm planning to do two things to find out more:

    • simulate the traffic with the BusPirate
    • attach a logic analyzer.

    Do you get these when you run Arduino sketch?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>