Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog [Upcycle It] Interactive Race Car Driver - Furby Hacking
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
  • Author Author: Workshopshed
  • Date Created: 23 Apr 2017 8:04 PM Date Created
  • Views 2744 views
  • Likes 5 likes
  • Comments 9 comments
  • interactiveracecardriver
  • upcycle_it
  • upcycled_interactiveracecardriver
Related
Recommended

[Upcycle It] Interactive Race Car Driver - Furby Hacking

Workshopshed
Workshopshed
23 Apr 2017

I'm not quite sure when I bought the Furby but I do remember the Furby Autopsy website inspiring the purchase. So that suggests it was perhaps after 1998.

image

When I recently checked there are some others that have also done some investigations including puppeteers and universities. A big thanks to Kelly Heaton for giving me permission to re-use her image showing the key parts of the Furby. As you can see there are loads of switches and sensors all over the Furby, there are also lots of moving parts but those are all run from a motor and cam mechanism.

 

Furby Anatomy

image

Furby Anatomy: From Kelly Heaton - anatomy of the furby

 

All I can say are that the original designers from Tiger Electronics were absolute wizards. They also did not skimp on construction with all the key components being attached via plugs and sockets. The "brains" of the operation are 2 boards with black blobs, it looks like one is a controller and the other is for processing the sounds. There is also an Eprom, Microphone and pre-amp and IR communications.

image

Schematics created by Chris Brown.

 

The motor seems to be controlled by a transistor based H-Bridge to the one I found in the RC car, so I think that I'll be swapping that out with a module again. To control the motor I also need to be able to count the pulses from the optical sensor and monitor the home switch. I think there's a couple of errors around this part of the schematics, the H-Bridge seems lopsided and the sensors on the gear position seem to be reverse. However they have saved me a whole load of work and I should be able to hook in my circuits to the connectors where I'll be removing the controller and sound chips.

imageimage

Equally helpful, the team at Northwestern University Mechatronics Design Laboratory have mapped out the Encoder Pulses for the different kinds of motion.

Number of pulses relative to the home position

Pose of the Furby

0 to 30

ears up, eyes open, mouth closed, not tilted

30 to 60

ears down, eyes open, mouth open, not tilted

60 to 100

ears down, eyes open, mouth shut, not tilted

100 to 130

ears down, eyes shut, mouth shut, tilted

130 to 170

ears up, eyes shut, mouth open, not tilted

170 to 200

ears up, eyes open, mouth open, not tilted

Note:

The encoder generates about 200 pulses per revolution of the motor and the number of pulses goes back to 0 again after one complete revolution.

The motion of the Furby is continuous and there the poses described above are just approximations. In many cases, the eyes or ears are partly open or closed.

By looking at the mapping above, however, you can have a rough idea of which number of pulses corresponds to which pose.

The comment "The motion of the Furby is continuous" does seem to tally with my experiments on the drive motor h-bridge which suggest that the motor does not have a stopped option. As per the maindrive my plan is to use a TB6612FNG module for the Furby motor, I'll use transistors to turn on and off the signals to the module.

 

Inside the Furby

I removed the casing and the speaker assembly and that allowed access to the PCB. I disconnected all of the sockets and extracted the board. Using some desolder braid I carefully removed the two "COB" (chip on blob?) boards. I wanted to keep the main PCB operational as that had signal conditioning and a driver for the opto-sensor for the main drive motor.

 

{gallery} Inside the Furby

image

Furby Guts: Inside the back of the Furby

image

Mechanics: Main drive gear and cams to activate the movements

image

Situp Plunger: This plunger causes the Furby to tilt forward

image

Homing Switch: These contacts are closed once per rotation

image

PCB: Note the after production modifications, LED for the optical sensor top left, the 2 daughter boards for control and sound, and the black circle bottom left is the tilt switch

image

PCB underside: The black and white wires connect up the power connection

image

Battery Compartment: Looking at the battery compartment as a place to put the Edison and a battery

image

Brain removal: With the two daughter boards removed there might be space for the Edison in the main housing

 

I wanted to understand the optical sensor as that would be needed to determine the positions for the animations. I realised that the LED on the PCB sticks into a tube and the sensor must be at the other end of that. There's some Schmitt triggers on the output of the photo transistor so we should get a clean signal from that.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

As per the car, I also wanted to check that the motor was running and the mechanism was working, so I hooked up the motor directly to a 5v USB from a powerbank. The circuit diagram has this running from 6v so I wanted to be sure it would run correctly from 5v, which it does.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The next thing to do for the Furby is to hook up a H-Bridge and the two sensors to the Edison to check it can be controlled. Some of the other furby hackers have reported problems with the signal from the optical sensor.

 

Reference

Furby Autopsy

Furby-hacking-101

Puppet studio - Furby

Northwestern University - Mechatronics - Furby Dissection

Anatomy of the furby

 

Previous Posts

[Upcycle It] Interactive Race Car Driver - Plan of action

[Upcycle It] Interactive Race Car Driver - Software

[Upcycle It] Interactive Race Car Driver - Lights

[Upcycle It] Interactive Race Car Driver - Detailed Plan

[Upcycle It] Interactive Race Car Driver - Edison

[Upcycle It] Interactive Race Car Driver - Drive Motor Testing

[Upcycle It] Interactive Race Car Driver - Car modification

  • Sign in to reply

Top Comments

  • jasonwier92
    jasonwier92 over 9 years ago +2
    I thought it was a simple kids toy. That is a lot of actions.
  • mcb1
    mcb1 over 9 years ago +2
    At least the H-Bridge in this one looks like a better design .. Some of those old electronic toys were a masterpiece of engineering and interfacing.
  • Workshopshed
    Workshopshed over 9 years ago +2
    The twiteratti have confirmed that COB stands for "Chip on Board" https://learn.sparkfun.com/tutorials/how-chip-on-boards-are-made#cob-manufacturing
Parents
  • DAB
    DAB over 9 years ago

    Great post Andy.

     

    I knew that the Furby was full of nice toys.

     

    I have been on the look out for some, but none have shown up in any of my garage sale ventures.

     

    It was toys like these that finally convinced the old Soviet Union that they could not keep up with the West.

    Many of our toys had better electronics in them than some of the old Soviet era military electronics.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 9 years ago

    Great post Andy.

     

    I knew that the Furby was full of nice toys.

     

    I have been on the look out for some, but none have shown up in any of my garage sale ventures.

     

    It was toys like these that finally convinced the old Soviet Union that they could not keep up with the West.

    Many of our toys had better electronics in them than some of the old Soviet era military electronics.

     

    DAB