Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog [Upcycle It] Interactive Race Car Driver - Powering Motors
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
  • Author Author: Workshopshed
  • Date Created: 22 Apr 2017 10:27 AM Date Created
  • Views 1461 views
  • Likes 7 likes
  • Comments 6 comments
  • upcycle_it
  • dc motors
  • upcycled_interactiveracecardriver
  • interactiveracingcardriver
Related
Recommended

[Upcycle It] Interactive Race Car Driver - Powering Motors

Workshopshed
Workshopshed
22 Apr 2017

After discounting the transistor based H-Bridges in the original car, I started experimenting with the TB6612FNG module. Despite its small size, it should be able to easily to take the few hundred mA needed for the motors.

image

My first experiments with this were not successful, every time I hooked up the motor supply connector the current shot up and the supply voltage collapsed causing the Edison to reset. After a few hours of double checking all the wiring and general frustration, I swapped to using LEDs to determine if my code or wiring was at fault. This worked fine with the direction LEDs turning on and off, and the PWM one fading on and off. I did get caught out by the fact that not all pins support PWM but you can swap those with the "swizzler", a set of header connectors that I've not quite worked out yet.

image

var mraa = require('mraa');
console.log('MRAA Version: ' + mraa.getVersion());

var pwm = new mraa.Pwm(6);  //PWM available on default swizzler positions. (3,5,6,9)
var forwards = new mraa.Gpio(7);
var backwards = new mraa.Gpio(8);
forwards.dir(mraa.DIR_OUT);
backwards.dir(mraa.DIR_OUT);
var dir = true;
var value = 0.0;
var step = 0.01;

pwm.period_us(700);
pwm.enable(true);

toggleDirection();

setInterval(function () {
    value = value + step;
    if (value <= 0 || value >= 1) {
       if (step <= 0) {
            toggleDirection();
        }
        step = -step;
    }
    pwm.write(value);
    } , 50);

function toggleDirection() {
    forwards.write(dir?1:0);
    backwards.write(dir?0:1);
    dir = !dir;
    }

process.on('SIGINT', function () {
    console.log("Shutting down SIGINT (Ctrl-C)");
    pwm.write(0);
    forwards.write(0);
    backwards.write(0);
    process.exit();
});

 

After success with the LEDs, I tried a second H-Bridge module (from a different supplier). That did not have the same issue so I concluded the problem was with the first board which is now discarded.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Power supply

Given the motors are the main power drain being about 300mA each, I was looking for a supply that could supply about 1A, was light, easily recharged, had capacity for a few hours play and was in around the 5v - 9v range. Despite having a range of different battery boxes and rechargable batteries I did not have anything that met those requirements. I also had a small 6v lead-acid battery but that was very heavy. Finally, I looked at buying some RC car batteries but these were very expensive and I'd need a charger too.

 

Then I realised that I did have a phone "power bank" that I'd won in a prize draw the previous year.

image

 

Capacity: 4000 mAh

Output: 1A

Input/Output Voltage: 5V

Battery Type: Rechargeable Li-Ion

Charging time (to charge power bank): Up to 4 hours

Standby Time: Up to 4 months

That should be perfect, so I doctored a USB cable so I could attach it to my breadboard. Unfortunately my cables were not coloured coded as per "standard" but I worked it out with a multimeter. The battery box happily powered my test LED and also the motors.

imageimage

 

Reference

TB6612FNG Hookup Guide

Power Consumption for IntelRegistered Edison Board for Arduino*

Power Banks | My Doodles

Previous Posts

[Upcycle It] Interactive Race Car Driver - Plan of action

[Upcycle It] Interactive Race Car Driver - Software

[Upcycle It] Interactive Race Car Driver - Lights

[Upcycle It] Interactive Race Car Driver - Detailed Plan

[Upcycle It] Interactive Race Car Driver - Edison

[Upcycle It] Interactive Race Car Driver - Drive Motor Testing

[Upcycle It] Interactive Race Car Driver - Car modification

[Upcycle It] Interactive Race Car Driver - Furby Hacking

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 9 years ago +1
    Andy I have appreciated the pragmatic approach. When all the possible solutions are explored, the only one remaining, event impossible, should be the truth
  • DAB
    DAB over 9 years ago +1
    Great post Andy. Good debug in going back to the input and walking yourself through the circuit path to find the problem. Nice example on how you need to test your components before you can integrate the…
  • carmelito
    carmelito over 9 years ago +1
    Nice update, the TB6612FNG module is my favorite motor driver..
Parents
  • balearicdynamics
    balearicdynamics over 9 years ago

    Andy I have appreciated the pragmatic approach. When all the possible solutions are explored, the only one remaining, event impossible, should be the truth

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 9 years ago

    Andy I have appreciated the pragmatic approach. When all the possible solutions are explored, the only one remaining, event impossible, should be the truth