Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Legacy Personal Blogs

Please Note:

This blog contains the legacy personal blog posts of our members, other than our Top Members whose content has been migrated into individual blogs in this area. Our new platform does not have personal blogs so this is how we have preserved the personal blog posts of our members from the Jive platform. No new posts will be permitted in this blog. Instead, if you wish to create blog content, please post it in the blog in the most appropriate topic area.

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • CAD Toy Design and Scale Model

    e14 Contributor
    e14 Contributor
    Hallow this Mahesh Deshmukh from India. This is small effort for creating intrest towards Science And Technology amoung the young generation. I tried to create toy design and scale model as first step towards achiving my goel. Lot of people have...
    • 11 May 2013
  • Endless Research...Nearly

    e14 Contributor
    e14 Contributor
    I had a co-worker send me the link for the RPi.  For 35 bucks, that would be a nice little project. I've always wanted a Seismic type monitor. The idea.  A Seismic monitor, powered by battery/solar, buried, with hourly updates and...
    • 10 May 2013
  • New USB library for NXP microcontrollers by DZX Designs

    tdrazich
    tdrazich
     DZX Designs is introducing an all new set of usb libraries for connecting your NXP microcontroller to a software application via usb. The DZX USBPort messaging system gives you everything you need, embedded firmware and PC Windows .NET software...
    • 10 May 2013
  • GCCC's 22nd Annual "Last" Chicago CoCoFEST!

    SGarciaV
    SGarciaV
    Glenside Color Computer Club The 22nd Annual “Last” Chicago CoCoFEST!Recap by Salvador Garcia I was over at the 22nd Annual “Last” Chicago CoCoFEST! on Saturday April 27. This Fest is held annually by the Glenside Color Computer Club (GCCC). Eac...
    • 9 May 2013
  • Des "smart" billets de banque avec puce RFID

    Crozemarie
    Crozemarie
    Le simple fait que de l'argent change de mains pourrait prochainement devenir beaucoup moins privé . Des chercheurs Américains ont mis au point une nouvelle façon d'intégrer des puces de traçabilité dans du "smart" papier offrant ainsi la possibilité...
    • 3 May 2013
  • Android Jelly Bean for the BeagleBone Black?

    patkelly
    patkelly
    I'm not sure if this is a little old now but I stumbled across the Android Development kits for the Sitara microprocessors on ti.com and it got me thinking which boards used a Sitara microprocessor. Then it hit me the BeagleBone Black has one of them...
    • 3 May 2013
  • 50 points worth of work

    billabott
    billabott
    Dude! There is nothing wrong with the example program or the Tone library.The problem is the Arduino IDE.  It can be a little uncooperative when adding a new library. Make sure you have the Tone folder where it is supposed to be. ...
    • 3 May 2013
  • Road Test for EATON's SmartWire System

    jeastwood
    jeastwood
    Eaton’s SmartWire-DT Element 14 Road Test Background I work at an aircraft repair facility in the R&D Department and am involved with the designing and building of test equipment for testing various aircraft systems; electronic, electri...
    • 29 Apr 2013
  • PCB Manufacturing process

    e14 Contributor
    e14 Contributor
    PCB Etching Process All PCB’s are made by bonding a layer of copper over the entire substrate, sometimes on both sides. Etching process has to be done to remove unnecessary copper after applying a temporary mask, leaving only the desired copper trace...
    • 29 Apr 2013
  • Try to win LPC800 mini-board

    RWM
    RWM
    Try to win LPC800 mini-boardhttp://www.nxp.com/campaigns/lpc800-go/raffle
    • 24 Apr 2013
  • Tiny ARM boards

    e14 Contributor
    e14 Contributor
    Overview on tiny ARM boards that run Linuxhttp://bitkistl.blogspot.co.at/2013/04/tiny-boards.html
    • 23 Apr 2013
  • Smartwire-DT Roadtest (Part I)

    cghaba
    cghaba
    From the beginning I was very excited to test the Smartwire-DT kit from Eaton. I have heard about the Smartwire technology some years ago, when first developed by Moeller (now part of Eaton), but never have to opportunity to test it. Working on ...
    • 22 Apr 2013
  • BP 0x0008

    billabott
    billabott
    Thank you, Mr. Mike Conners, for posting where to find the recent info about STM32 for Dummies which can be found at http://www.cs.indiana.edu/~geobrown/book.pdf.  It shall be like a Golden Compass unto me. I will start immediately to consu...
    • 22 Apr 2013
  • Tests électriques

    association.polyjoule
    association.polyjoule
    C'est le jeudi 18 Avril (2013) qu'ont eut lieux les premiers tests de fonctionnements électriques de Cityjoule à l'aide du banc d'essai à rouleaux développée par le lycée La Joliverie. Ces premiers tests sont concluants et encour...
    • 22 Apr 2013
  • The Basic Idea

    e14 Contributor
    e14 Contributor
    The main idea is to use a PICAXE 20M2 to make a simple handheld gaming system to show off at places. There is a few things I havent really thought about yet, these are:Audio. Why and How?Controller. Which design i should choose.Connectivity. Can you ...
    • 21 Apr 2013
  • Le protocole MiWi de Microchip

    Crozemarie
    Crozemarie
    Présentation du protocole Miwi de Microchip par www.domogy.fr  Miwi est un protocole de communication qui permet de réaliser des réseaux sans fil.Ce protocole propriétaire est proposé par le fabricantMicrochip Technology très connu en autre...
    • 16 Apr 2013
  • Autostarting a Python program when the Raspberry Pi is powered up

    mistertee
    mistertee
    When developing an application using python, it is essential to have the Raspberry Pi connected up with keyboard, mouse and monitor. However in most control applications, once the application has been debugged and is working OK, one does not need the...
    • 15 Apr 2013
  • reprap cnc machine 4 axis new boards

    e14 Contributor
    e14 Contributor
    Today I'm working with a new board ATMEGA644P Sanguino, and some drivers for stepper motors based drv8825, the engines have gained by recycling such things as printers and CD drives, today I want to build a reprap based recycled technology but bigger...
    • 11 Apr 2013
  • Le Projet HomeBox présenté par Domogy

    Crozemarie
    Crozemarie
    Le Projet HomeBoxJe voulais vous parler du projet HomeBox. Ce projet a été développé par cinq étudiants de l'école d'ingénieur ECE Paris (École Centrale Electronique). Ils ont travaillé et développé un serveur domotique multi-protocole (aujourd'*** d...
    • 10 Apr 2013
  • Rectangular connectors for missiles, torpedoes, and avionics industrial apps

    e14 Contributor
    e14 Contributor
    Rectangular connectors for missiles, torpedoes, and avionics industrial appsintroducing a high-density rectangular connector for advanced missile systems, torpedoes, flight guidance systems, and related military electronics equipment. The CCM-20, 21,...
    • 9 Apr 2013
  • Special Blog

    billabott
    billabott
    It is my estimate that way less than 25% of the adult population of the world have disciplined their minds to solve a problem like the one I solved.   Volume of the Cylinder   =   (pi) (r^2) (h)   =  ...
    • 9 Apr 2013
  • Parts

    e14 Contributor
    e14 Contributor
    These are the parts I currently have, or are in my cart(s) 1. HD44780 LCD Display    1 x 74HC595 Shift Register (element14)    1 x BC547 NPN (or MOFSET or similar NPN) (sparkfun)    1 x 10k Trimmer Po...
    • 7 Apr 2013
  • Eaton SmartWire-DT Road Test Kit

    markav
    markav
    Eaton SmartWire-DT Road Test Kit Hi this is my review of the Eaton Smartwire DT road test kit. The kit consisted of: 1 x Programmable Relay – EASY802-DC-SWD 2 x Contactor Adapter DIL-SWD-32-002  2 x Contactors DILM7-10 2 x twin pu...
    • 5 Apr 2013
  • Blog

    nlarson
    nlarson
    sfdfhsdfdshgdsghg  ParPart Product LinkProduct Link
    • 4 Apr 2013
  • High Altitude/Near Space Ballooning

    e14 Contributor
    e14 Contributor
    I have experimented with electronics for a while. Very few of my projects have been useful (if finished). So I wanted to settle in on a project for a few months that I can learn form. Allot of people have created near space balloons, and I want to jo...
    • 4 Apr 2013
<>