Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Legacy Personal Blogs

Please Note:

This blog contains the legacy personal blog posts of our members, other than our Top Members whose content has been migrated into individual blogs in this area. Our new platform does not have personal blogs so this is how we have preserved the personal blog posts of our members from the Jive platform. No new posts will be permitted in this blog. Instead, if you wish to create blog content, please post it in the blog in the most appropriate topic area.

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Wire

    tomdolan97
    tomdolan97
    I have the Solid Tinned Annealed Copper Wire, PVC Insulation which has an outer diameter of 1.2mm. Is there any wires available made from the same or a similar material with a smaller outer diameter available from Farnell?
    • 17 Jan 2019
  • Picoscope memory depth application calculation

    weiwei2
    weiwei2
    In a customer project that i have implemented few years ago, we have selected PicoScope 5204. Back then the requirement was to able to sample the signal for 30s.Specifications wise, 5204 is able to sample at 8 bit at 1GS/s and its memory 128MS. Table...
    • 14 Jan 2019
  • Merry Boxes and LED's Software.

    danielw
    danielw
    I couldn't fit the code into the original merry boxes and LED's  If you want to see the original blog ckick here -> Automatic christmas bell ringers. The Arduino code. #include <Servo.h> /****************************...
    • 14 Jan 2019
  • Avnet LTE IoT Starter Kit Example software Release 2

    james.flynn
    james.flynn
    Boot Button Operation UART2 Operation Low Power Mode  The initial release of firmware for the System On a Module (SOM) lacked support for the BOOT button, Low Power Mode (LPM), or the second UART on the SOM.  Now, there is a new/secon...
    • 14 Jan 2019
  • Studying : Being Robotics : Week 2

    dubbie
    dubbie
    Week 2 of the FutureLearn Begin Robotics MOOC has now come and it contains some interesting material. The MOOC has many small steps (30 in Week 2) some with just written articles. some with short videos and some with demonstrations and exercises. The...
    • 14 Jan 2019
  • You Are Here

    wolfgangfriedrich
    wolfgangfriedrich
    I decided to explore the artistic PCB realm and the map location pin became the theme.A reverse mounted red LED, powered by a CR2032 coin cell, is shining through the PCB to provide a bright homing beacon. Soon also available in blue. The 1...
    • 13 Jan 2019
  • MyERIC #1 : The Initial Construction

    dubbie
    dubbie
    As part of the Begin Robotics MOOC that I am currently following, a two wheeled mobile robot is used for many of the examples (see Studying : Begin Robotics : Week 1 ). For the MOCC a simulation of the two wheeled robot is used but having seen a vide...
    • 11 Jan 2019
  • FPGA Algorithms and Applications in the IoT, AI, and High-Performance Computing - Invitation to Editorial Advisory Board (EAB) and Call for Chapter (CFC)

    ngd012019
    ngd012019
    Dear Professor(s) ,(1)   Invitation to Editorial Advisory Board (EAB)I trust this e-mail finds you well. I am contacting you based on your expertise in Internet of Things and Field Programmable Gate Array (FPGA). Currently, I am in the proc...
    • 10 Jan 2019
  • Debugging DDR Memory on IoT Devices

    caroline_teledynelecroy
    caroline_teledynelecroy
    Internet of Things (IoT) devices are, at heart, just another embedded computing system, albeit one with an extremely well-defined function. As such, there's bound to be some amount of on-board data storage, and the storage medium of choice these ...
    • 9 Jan 2019
  • Eagle 3d povray

    gmail
    gmail
    Regards...Thank you for allowing me to join ...I just got to know Eagle 3d rendering povray, and I was very interested in it, for months I was looking for the right site for Eagle 3d povray. All sites always directed me to the site matwei.de .... and...
    • 8 Jan 2019
  • PS3 Controller compatibility with Final Burn Alpha & MAME

    ajkatz83
    ajkatz83
    players.brightcove.net/.../index.html With regards to this video here, I had found this enclosure and concept pretty compelling so I had to make on myself. The enclosure came from user Snille--Retro Pi Station as it was console design that was c...
    • 7 Jan 2019
  • Studying : Begin Robotics : Week 1

    dubbie
    dubbie
    The first week of the Future Learn Begin Robotics MOOC has now started and I have worked my way through the material. This is a sequence of short videos, written pages and exercises using a simulation. Being and introduction course the content and ma...
    • 7 Jan 2019
  • Intel Neural Compute Stick 2

    tonydbeck
    tonydbeck
    I Came across the new Intel Neural Compute Stick 2 which it looks like a pretty cool piece of hardware!.......It houses an Intel Movidius Myriad   X Vision Processing Unit (VPU) that can give your board deep neural network capabilities! w...
    • 3 Jan 2019
  • Bluetooth Controller for LEDs #3 : Trying to Connect

    dubbie
    dubbie
    After playing with the hardware for a while I thought I would see if I could actually make a connection to one of the Bluetooth Christmas Tree light controllers. I eventually managed to download the correct App for my Android smart phone, it is the o...
    • 2 Jan 2019
  • Studying : Introduction to Robotics MOOC

    dubbie
    dubbie
    Recently received an email from Future Learn about the Begin Robotics MOOC that I have signed up for, starting on 7th Jan'19. Only a few days now before the fun begins. Ill get to play with ERIC the robot - whatever that is - a simulation I think...
    • 2 Jan 2019
  • ESP32 LoRaWAN node with Arduino

    oksbwn
    oksbwn
    To test out the recent addition in my lab that is the LoRa gateway, I needed one LoRa node also. LoRa modules are available to be used with Arduino as well as Raspberry Pi and are pretty cheap too. However, you can get complete LoRa module with ESP32...
    • 1 Jan 2019
  • Bluetooth Controller for LEDs #2 : The Output

    dubbie
    dubbie
    I have managed to connect up the output of the LED controller to my oscilloscope. This is the non-Bluetooth version of the controller because it is still fully shrouded so it is much safer, but it should be the same as the same LEDs are plugged in. I...
    • 31 Dec 2018
  • Maui Monitor Arduino Code

    airbornesurfer
    airbornesurfer
    Here's my contribution to the code for Episode 367: Most Useless IoT Device Ever - Part 2 It's ugly, but it works! //element14 Presents IoT Rock Phase II //Maui airport monitor by Matthew Eargle //https://airbornesurfer.com //Completely useless ...
    • 31 Dec 2018
  • A Transistor Load: How it Works

    jc2048
    jc2048
    A Transistor Load A Transistor Load: Stability A Transistor Load: Stability Part 2  Introduction Important note: I'm learning about design with transistors and this is an investigation of transistor design techniques and presents a first pr...
    • 30 Dec 2018
  • A Transistor Load: Stability Part 2

    jc2048
    jc2048
    Introduction This is a short follow-up to A Transistor Loadwhich I blogged about as part of the Project14 Test and Instrumentation competition. In the last blog A Transistor Load: StabilityI got as far as compensating the amplifier section ...
    • 30 Dec 2018
  • Bluetooth Controller for LEDs #1 : De-constructing the Controller

    dubbie
    dubbie
    Whilst wandering around a local store after Christmas looking for reduced cost Christmas decorations and hence bargains - of which there were only a very small number this year, I noticed a Christmas Wonderland Bluetooth Transfer, for controlling a s...
    • 27 Dec 2018
  • Alps exhibited at electronica 2018

    alpselectric
    alpselectric
    Alps electric exhibited at electronica 2018 held in Munich, Germany.The booth introduced its technologies and products for market like IoT, automotive, virtual reality. HighlightTouch input module: a fusion of Alps (manufacturer of electronic co...
    • 27 Dec 2018
  • Issue using Energia for the CC3200 LaunchXL

    kweber250
    kweber250
    Hello All,I'm trying to compile this code in Energia and I receive the error below, I receive a similar error regardless of the code, if I need to download a library to write in c, which library and where do I download it.Thank you!//////////////////...
    • 26 Dec 2018
  • LoadCape, MotorCape, and BBBW/Flask and Ideas

    silver2row
    silver2row
    Hello, ... I was making some ideas come to life on GitHub.com. The two major items were related to BBBW and BBGW w/ the newer Capes available. I used the MotorCape to make some motors move and the LoadCape to make some loads (motors) m...
    • 23 Dec 2018
  • Getting up and running with Arm Design Start, Generating the SW

    adamtaylorcengfiet
    adamtaylorcengfiet
    In my last blog we examined how we could get the Arm Design Start Cortex M3 up and running on out Arty A7-35T board using the example SW application provided. In this blog we are going to look at how we can create our own application software. T...
    • 19 Dec 2018
<>