EAGLE User Support (English) AC mains on a PCB ?
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
  • State Verified Answer
  • Replies 107 replies
  • Answers 10 answers
  • Subscribers 186 subscribers
  • Views 18242 views
  • Users 0 members are here
Related

AC mains on a PCB ?

anishkgt
anishkgt over 9 years ago

A total newbie to eagle design and PCB fab. So plase bear with on my silly questions, trying to learn.

 

I have pcb that is schematically completed with the layout. Before i start the fabrication process i need some expert advise if the components placed and the wires routed are ok for the ac mains and the others. The load here will be a transformer. The ac mains are 240VAC and all works well as designed in the schematic on a bread broad except for the load for which MOC3023 is yet to arrive from where i've ordered.

 

 

 

Thanks in advance.

 

image

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 9 years ago in reply to anishkgt +2
    Hi George, It looks like you're really learning a lot with this design and you've had lots of good advice from people on this thread already and the difference between the initial version you posted and…
  • michaelkellett
    michaelkellett over 9 years ago in reply to rachaelp +1 suggested
    For mains input spike suppression I think you are much better off with this kind of device: http://uk.farnell.com/epcos/b72214s0231k101/varistor-60-0j-230vac/dp/1004389 Farnell 1004389 This one is rated…
  • autodeskguest
    autodeskguest over 9 years ago in reply to anishkgt +1 suggested
    On 11/09/16 12:02, George Thomas wrote: Why two thrustirs to control the load and am trouble witching on yhe Triac. Triacs can suffer commutation problems with certain types of load - highly inductive…
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to anishkgt

    The input of the micro is quite a high impedance so putting a 10R (or 100R resistor in series will have no detectable effect.

     

    You ought to move D1 down a little since it is now the closest thing on the low voltage side to the mains.

     

    For safety the ground plane (polygon) should be very solidly connected to mains earth - then if you do get a short on your board the dangerous current will flow to earth rather than though you.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to anishkgt

    Hi George,

     

    I think you misunderstood the point of adding the resistor between IC1 and IC4. The point was so you could use the resistor as a physical bridge over the other traces which were in the way and causing you to have to route the trace around the houses, what you have done with it is not helping in this regard and you've had to carve up the 5V and reroute part of it with a very thin trace.

     

    Also, why have D1 and D4 become huge? Have you replaced these with the type of TVS we spoke about previously? That wasn't meant for these locations, it was meant for across the AC input.

     

    Finally, It's going to sound nit picky, but I don't like the traces as strange angles.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to anishkgt

    George Thomas wrote:

     

    no electrical link but a mechanical link ????? what does that mean ? wouldn't it act like current limiting resistor.

    Use a 0R resistor, or just a wire jumper.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to michaelkellett

    On 15.09.2016 16:57, Michael Kellett wrote:

    The input of the micro is quite a high impedance so putting a 10R (or 100R resistor in series will have no detectable effect.

     

    You ought to move D1 down a little since it is now the closest thing on the low voltage side to the mains.

     

    For safety the ground plane (polygon) should be very solidly connected to mains earth - then if you do get a short on your board the dangerous current will flow to earth rather than though you.

     

    The design looks earthless (isoladed AC). I don't know if there are any

    compliance rules that says you need to do that, but the fact that the

    LOAD is ext to pcb, and you are probably exposing the LOAD AC contacts

    for spot welding, makes me thing you do need it. Maybe it even requires

    isolated high voltage there, wich would make this design require an

    isolating 1:1 transformer in front.

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to michaelkellett

    On 15.09.2016 16:57, Michael Kellett wrote:

    The input of the micro is quite a high impedance so putting a 10R (or 100R resistor in series will have no detectable effect.

     

    You ought to move D1 down a little since it is now the closest thing on the low voltage side to the mains.

     

    For safety the ground plane (polygon) should be very solidly connected to mains earth - then if you do get a short on your board the dangerous current will flow to earth rather than though you.

     

    The design looks earthless (isoladed AC). I don't know if there are any

    compliance rules that says you need to do that, but the fact that the

    LOAD is ext to pcb, and you are probably exposing the LOAD AC contacts

    for spot welding, makes me thing you do need it. Maybe it even requires

    isolated high voltage there, wich would make this design require an

    isolating 1:1 transformer in front.

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 9 years ago

    Hmmmm hope this went well.

     

    image

    Update:

         Rachel the TVS used here are quite big in size, approximately 5mm hence the size in the layout.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 9 years ago in reply to anishkgt

    added AC tvs and PTC

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to anishkgt

    George Thomas wrote:

     

    added AC tvs and PTC

    It looks like you have put the TVS in series with the AC input. This is not correct, it should go in parallel with it.

     

    George Thomas wrote:

     

    Update:

         Rachel the TVS used here are quite big in size, approximately 5mm hence the size in the layout.

     

    The TVS in those DC side locations don't need to be that big. The power rating of 1500W is excessive for where it's located so you could choose smaller ones if you were running out of space.

     

    Rachael wrote:

     

    Finally, It's going to sound nit picky, but I don't like the traces as strange angles.

    And now look at the strange angled trace from the '+' pin of B1 which is almost (possibly is) touching the '-' pin. If you don't route at ugly odd angles you wont do this. Use the right mouse button when in routing mode to cycle through the bend styles or use the buttons at the top and use the two 45 degree ones (hint: you need to use both 45 degree styles depending on which way you'd like it to route)

     

    Morten Leikvoll wrote:

     

    The design looks earthless (isoladed AC). I don't know if there are any compliance rules that says you need to do that, but the fact that the LOAD is ext to pcb, and you are probably exposing the LOAD AC contacts for spot welding, makes me thing you do need it. Maybe it even requires isolated high voltage there, which would make this design require an isolating 1:1 transformer in front.

     

    This is sensible advice, I believe I mentioned in earlier posts my concerns about the lack of an earth connection. It all comes back to safety.

     

    George Thomas wrote:

     

    My idea for the connector was this.

    So what happened to these connectors? It looks like you still have the old ones in the design?

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 9 years ago

    And now look at the strange angled trace from the '+' pin of B1 which is almost (possibly is) touching the '-' pin. If you don't route at ugly odd angles you wont do this. Use the right mouse button when in routing mode to cycle through the bend styles or use the buttons at the top and use the two 45 degree ones (hint: you need to use both 45 degree styles depending on which way you'd like it to route)

    How could i miss that i did notice it earlier but slipped it, changed it now. Thanks for that.

     

    I've replaced the TVS at the DC side to this and changed the AC side too.

     

    This is sensible advice, I believe I mentioned in earlier posts my concerns about the lack of an earth connection. It all comes back to safety.

    I did notice that suggestion and kept it to be done at the end. So would that go ? just connect it to the earth terminal from the mains ?

    image

    Update: rotated the C1 and C2 for a better route.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 9 years ago

    hmmmm where did everyone go ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>