Moto Mods
  • Products & Partners
  • Manufacturers
  • Moto Mods
  • More
  • Cancel
Moto Mods
Blog Moto Mods Developer Part 2 - Getting Started - SDK Setup & Android Studio Install
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Moto Mods to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 28 Apr 2017 6:34 PM Date Created
  • Views 2433 views
  • Likes 0 likes
  • Comments 0 comments
  • android
  • developer
  • embedded
  • Design
  • mobile
  • cabeatwell
  • moto mods
  • innovation
  • linux
Related
Recommended

Moto Mods Developer Part 2 - Getting Started - SDK Setup & Android Studio Install

Catwell
Catwell
28 Apr 2017

Index of the Moto Mods Developer project:

Moto Mods Developer Part 1 - Getting Started - Virtual Machine Setup and Linux Install

Moto Mods Developer Part 2 - Getting Started - SDK Setup & Android Studio Install

Moto Mods Developer Part 3 - Firmware Setup

Moto Mods Developer Part 4 - Getting Started - Make Build-Folder, add Utility and OS files

Moto Mods Developer Part 5 - Flashing Firmware with MDK Utility

Moto Mods Developer Part 6 - Blinking an LED on the Moto Mods Perfboard

Moto Mods Developer Part 7 - Modifying the C file for the perfboard LED

Moto Mods Developer Part 8 - Configure Nuttx

Moto Mods Developer Part 9 - Updating the Hardware Manifests file

Moto Mods Developer Part 10 - Cont’d Configure and Compile Nuttx

Moto Mods Developer Part 11 - Load newly created Nuttx Firmware onto Reference Board

Moto Mods Developer Part 12 - Soldering the Test Points to use the perfboard

Moto Mods Developer Part 13 - Making custom App to control the Firmware

 

Believe me, developing on the Moto Mod platform is not for the faint of heart. Be sure to see Part 1 of the Moto Mod Developer series, click this link. A wrong move means bigtime headaches. Follow it exactly. Then come on back here.

 

Part 2

 

Install JDK and Android Studio

 

This tutorial will show you how to Install JDK, Android Studio, and the Moto Mods SDK on Ubuntu 16.04

 

Android Studio requires the Java Development Kit (JDK) so we will install that first. In terminal, type “sudo apt-add-repository ppa:webupd8team/java”. Follow the terminal commands shown

 

image



image

 

image

 

image



image



Once the installer is done, type “javac -version” and “java -version” to check if the JDK was installed.

 

image



Now that JDK is installed, we can now install Android Studio in Ubuntu VM, open firefox and download Android Studio 



image

 

Save the file and extract it

 

image

 

Create a folder called Apps in the /home/<username> directory. Move the extracted folder in the /home/<username>/Apps, using right click->Move To...



image

 

In terminal, navigate to the directory and execute “./studio.sh”. Shown above. If you get a permissions error then, Navigate to Android Studio’s directory bin folder, give yourself permission for the .sh file and execute it

 

image

 

This is a new copy, Select the second option



image

 

Android Studio will launch

 

image

 

The Android Studio Welcome will show, click Next

 

image

 

Choose Standard Installation

 

image

 

Click Next

 

image

 

Hit Finish

 

image

 

Android Studio is now installed

 

image



Setup Moto Mods Project in Android Studio

 

Start a new Android Studio Project and configure your application name



image



Set Android API version to 6.0 (API level 23), Moto Mods only supports API level 23+ (Android 6.0+). It does not support earlier versions of Android.

 

image

 

It will install API23: Android 6.0 SDK

 

image

 

Create an empty activity

 

image

 

For beginning Moto Mods Development we will start with a Blinky application

 

image

 

Click Finish

 

image

 

Finally, the Android Studio Blinky application is setup, ready for development.

 

image

 

Install Moto Mods SDK

 

Now that Android Studio is installed and a project is created we need to add the Moto Mods SDK to the newly created project so that we can make API calls to the Reference Moto Mod

 

Download the Mod Mods SDK Library. Provided at: https://developer.motorola.com/build/tools/setup-environment

Save the ZIP file.

 

Moto Mods Developer Steps 2.jpg

 

In your downloads folder, Right click on the “ModLib-01.00.000.zip” and hit “Extract Here”

 

image



Once the ZIP is extracted, Right click and “Move To….”

image

 

Navigate to ‘/home/<username>’ and hit select

 

image

 

Once moved, open the “ModLib-01.00.000” folder and Move or Copy To…

 

image

 

Now we will put the SDK into our Android Studio Project. Move the .jar file into the /libs folder of our created project. ‘/home/<username>/AndroidStudioProjects/MotoModsDevelopment-Blinky/app/libs’

 

image

 

In the /res folder of /ModLib-01.00.000 there is a version.xml file that we need to move as well. Hit Move or Copy To...

 

image

 

Move or Copy “version.xml” to ‘/home/<username>/AndroidStudioProjects/MotoModsDevelopment-Blinky/app/src/main/res/values’

 

image

 

Shown below is how the “modlib-01.00.000.jar” and “version.xml” should look in the project explorer tree.

 

image



 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

The SDK is now added to the project and we can start using it to develop.

 

You can read Part 1 here!