Say Hello to Raspberry Pi 5!

The Raspberry Pi 5 delivers over a 2x increase in CPU performance and a significant uplift in GPU performance. Available in 4GB, or 8GB LPDDR4X-4267 SDRAM, the Pi 5 comes loaded with a 2.4GHz 64-bit quad-core ARM processor, VideoCore VII GPU, 2x4 lane MIPI camera/display transceivers, real-time clock, and a convenient, on-board power button.

Meet the Raspberry Pi 5 , Available in 4GB RAM, 8GB RAM and learn more about the New Raspberry Pi 5 16GB.

Introducing the Raspberry Pi Compute Module 5
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
Raspberry Pi Poster
Raspberry Pi Webinars and eBooks
Featured Products
power supply

27W USB-C PD Power Supply

5.1V, 5A power supply

pi 5 case

Raspberry Pi 5 Case

Improved thermal features, built-in fan, made specifically for the Pi 5.

Active Cooler

Active Cooler

Cooling solution with a large heatsink and variable-speed fan

RECENT BLOG POSTS
  • Blog: Receiving Weather Satellites on a Raspberry Pi or Linux

     I found it necessary to create this article for a few reasons Most of the YouTube/Instructables focus on aerials or only Windows installation The ones that are for the Raspberry Pi are out of date A url has changed which prevents WxToImg updat...
  • Blog: Pico IoT LoRaWAN EasyNode

    Table of Contents Introduction What does it do? How Does it Work? Circuit Diagram Building It Current Features Future Features Known Defects Security System Power Controller Firmware Pico Firmware Optionally Building the Pico Code Configuring It Ex...
  • Blog: Using CLion for Easier Coding with Pi Pico and C/C++

    Table of Contents 2024 Update Introduction Some CLion Highlights Code Navigation SSH and Command Line Windows Code Inspection Git and GitHub Working with Pico: Installing Pre-Requisites (Pico C SDK, Pico Examples, and CLion) Opening Projects wit...
  • Blog: XR-1000 Chassis and Electromechanicals: Putting it Together

    Table of Contents Introduction Assembling the Chassis Attaching the Control Boards Using It Ideas Introduction The XR-1000 is an easy-to-build, hopefully easy-to-use, Python-operated, open-source/open-hardware hackable eXperimental Robot just sl...
Related Projects
  • Video: Infrared night vision with the NoIR V2

    The primary advantage of the Raspberry Pi NoIR camera is seeing in complete darkness. By using an Infrared light source - completely invisible to the human eye - images and videos can be captured with no visible illumination whatsoever. This vid...
  • A more powerful Plex media server using Raspberry Pi 3

    Recently we built a Plex Media Server using the Raspberry Pi 2, at the time the Raspberry Pi 2 was the most powerful board in the Raspberry Pi range. But on February 29th 2016 the Raspberry Pi Foundation announced their latest board, the Raspberry Pi...
  • Gesture Based TV Remote Control

    Here's the latest project I've been working on: controlling the TV using gestures instead of a remote control. Mainly inspired by my kids being able to handle a tablet but not a remote control, it could perhaps also help to Make Life Accessib...
  • 2015 Year in Review: Top 10 Raspberry Pi Projects

    RASPBERRY PI PROJECTSJust between you and me, it can sometimes be tricky finding enough content for "top lists" like these. At times it almost feels like you're settling for certain entries, rather than really wanting to put them front ...
  • Raspberry Pi Zero Internet Connected Information Display

    The Raspberry Pi Zero form factor, makes it perfect for use in smaller project. Combined with internet connectivity, a display and some kind of input, it could be used to visualise virtually anything. Using a Pi Zero, an I2C OLED display from Ad...