Say Hello to Raspberry Pi 5!

The Raspberry Pi 5 delivers over a 2x increase in CPU performance and a significant uplift in GPU performance. Available in 4GB, or 8GB LPDDR4X-4267 SDRAM, the Pi 5 comes loaded with a 2.4GHz 64-bit quad-core ARM processor, VideoCore VII GPU, 2x4 lane MIPI camera/display transceivers, real-time clock, and a convenient, on-board power button.

See the Raspberry Pi 5 4GB Technical Specification and 8GB Technical Specification.

Introducing the Raspberry Pi Compute Module 5
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
Raspberry Pi Poster
Raspberry Pi Webinars and eBooks
Featured Products
power supply

27W USB-C PD Power Supply

5.1V, 5A power supply

pi 5 case

Raspberry Pi 5 Case

Improved thermal features, built-in fan, made specifically for the Pi 5.

Active Cooler

Active Cooler

Cooling solution with a large heatsink and variable-speed fan

RECENT BLOG POSTS
  • Blog: Introducing the Raspberry Pi Compute Module 5

    Raspberry Pi Compute Module 5 is a system on module that delivers the power of Raspberry Pi 5 in a form factor ideal for embedded applications. Priced from $45 and featuring a quad-core Arm Cortex-A76 processor, dual 4Kp60 HDMI output, Gigabit Ether...
  • Blog: Raspberry Pi Pico W Mecanum Wheel Car Kit

    Prime Day rolled around again two weeks ago and it was a good opportunity to find a toy that I could build for my grandson. I bought a Freenove Mecanum Wheel 4WD Car Kit for the Raspberry Pi Pico.  I was able to get it for $39.96 since...
  • Blog: Raspberry Pi AI Camera - with the Sony IMX500

    The AI Camera is built around a Sony IMX500 image sensor with an integrated AI accelerator. It can run a wide variety of popular neural network models, with low power consumption and low latency, leaving the processor in your Raspberry Pi free to pe...
  • Blog: Arducam PiNSIGHT - OAK-SoM AI Camera

    This year has been a difficult one for me in terms of having time to do projects and try out new hardware.  Back in mid-February I pre-ordered an Arducam PiNSIGHT which was selling for a $30 discount from its normal $99.99 price.  I've...
Related Projects
  • Video: Infrared night vision with the NoIR V2

    The primary advantage of the Raspberry Pi NoIR camera is seeing in complete darkness. By using an Infrared light source - completely invisible to the human eye - images and videos can be captured with no visible illumination whatsoever. This vid...
  • A more powerful Plex media server using Raspberry Pi 3

    Recently we built a Plex Media Server using the Raspberry Pi 2, at the time the Raspberry Pi 2 was the most powerful board in the Raspberry Pi range. But on February 29th 2016 the Raspberry Pi Foundation announced their latest board, the Raspberry Pi...
  • Gesture Based TV Remote Control

    Here's the latest project I've been working on: controlling the TV using gestures instead of a remote control. Mainly inspired by my kids being able to handle a tablet but not a remote control, it could perhaps also help to Make Life Accessib...
  • 2015 Year in Review: Top 10 Raspberry Pi Projects

    RASPBERRY PI PROJECTSJust between you and me, it can sometimes be tricky finding enough content for "top lists" like these. At times it almost feels like you're settling for certain entries, rather than really wanting to put them front ...
  • Raspberry Pi Zero Internet Connected Information Display

    The Raspberry Pi Zero form factor, makes it perfect for use in smaller project. Combined with internet connectivity, a display and some kind of input, it could be used to visualise virtually anything. Using a Pi Zero, an I2C OLED display from Ad...