RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs TI Ultrasonic Sensor - First Measurements
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: Jan Cumps
  • Date Created: 19 Dec 2015 8:13 PM Date Created
  • Views 3652 views
  • Likes 2 likes
  • Comments 10 comments
Related
Recommended
  • RoadTest
  • tdc1000-tdc7200evm
  • ultrasonic_sensor
  • steminc
  • texas_instruments
  • tdc1000

TI Ultrasonic Sensor - First Measurements

Jan Cumps
Jan Cumps
19 Dec 2015

The  TDC1000-TDC7200EVMTDC1000-TDC7200EVM evaluation module has 4 main parts

The TDC1000 analog front-end and a pre-programmed MSP430 microcontroller on the board, a 1MHz Piezo Ceramic sensor that plugs into the board and a GUI client for on your PC.

 

In this blog I perform the first measurements.

image

 

Test Setup

 

I've filled the container with water, up to somewhere between 4 and 5 cm. I've used the simplest setup with the sensor mounted under the liquid.

 

image

 

The Piezo sensor is AC, so the color of the wires doesn't really matter. This is how I connected the sensor (all the lower pins are ground).

image

 

The speed of sound is configured at 1480 m/s - the default setting of the test software (I've attached a register file that can be imported into the GUI to this blog).

I'm rather satisfied with the first results:

 

image

 

My First Issue

 

I have a problem when I generate a configuration file in Webench and load that into the gui.

I've logged a post for that on TI's e2e forum.

 

Edit January 7, 2016: The TI application team has looked at my request and confirmed my findings. Visit this link for a temporary solution.

A full solution to make the Webench config app and the evaluation board's GUI is being worked on.

 

Related Posts
RoadTest: Unboxing the TI Ultrasonic Sensing evaluation module
TI Ultrasonic Sensor - A Very First Trial of the GUI
TI Ultrasonic Sensor - Prepping the Transponder
TI Ultrasonic Sensor - First Measurements
TI Ultrasonic Sensor - Set the Parameters for Level Measurement and Content Identification
TI Ultrasonic Sensor - Show 3 Signals on a 2 Channel Oscilloscope (RIGOL DS1052E)
TI Ultrasonic Sensor - Liquid Identification and Concentration
TI Ultrasonic Sensor - Create a KiCad Part for the Sensor IC with KiPart
TI Ultrasonic Sensor - SPI Traffic Snooping

TI Ultrasonic Sensor - RoadTest Review

Attachments:
TDC1000_Setup_Firmware_default.txt.zip
  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 10 years ago +1
    I'm liking these posts. I have a water tank that I want to add guaging to, and so far all the other solutions require adding something inside the tank. This means it has very high moisture content, and…
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to mcb1 +1
    I've received help on TI's e2e forum. TDC1000-TDC7200EVM errors when importing Register file generated by design tool - Ultrasonic Sensing Forum - Ultrasonic … An application expert has detected why the…
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to e14 Contributor

    shubhamg, you would use a similar design as the evaluation module. You'd need a replacement for all the functional blocks in the evaluation module.

     

    Have a look at the reference design section for this IC

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to Jan Cumps

    Do you have an idea of how to use TDC 1000 without evaluation module?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to Jan Cumps

    The application specialist acknowledged the issue with loading files generated by the Webench utility,

    but the core issue - that the utility's settings don't put the board in a working configuration, hasn't been resolved yet.

     

    I've updated the e2e topic with my test results:

     

    http://e2e.ti.com/support/sensor/ultrasonic/f/991/t/478399

     

    I'll keep posting progress here...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to mcb1

    I've received help on TI's e2e forum.

    TDC1000-TDC7200EVM errors when importing Register file generated by design tool - Ultrasonic Sensing Forum - Ultrasonic …

    An application expert has detected why the file that I generated on the Webench doesn't put my evaluation kit in a working modus, and has made corrections to the configuration.

    I'll post back when I tried the solution...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago

    I'm liking these posts.

    I have a water tank that I want to add guaging to, and so far all the other solutions require adding something inside the tank.

    This means it has very high moisture content, and it requires very good sealing that has to last many years.

     

    Using this method it could be outside and being plastic will be suitable for this solution.

     

     

    Thanks, and keep working through the issues.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<