RoadTest: AVNET Azure Sphere MT3620 Starter Kit
Author: dixonselvan
Creation date:
Evaluation Type: Development Boards & Tools
Did you receive all parts the manufacturer stated would be included in the package?: True
What other parts do you consider comparable to this product?: Seeed Azure Sphere MT3620 Development Kit
What were the biggest problems encountered?: 1) SDK Installation - The Azure Sphere SDK took a long time to be installed in my machine. It appeared to be stuck at one point while being installed that I had to cancel the process. Unfortunately, this uninstalled the Visual Studio 2017 that I've installed already. Because of this, I had to repeat the process of installing VS 2017 followed by the SDK (since the SDK required VS 2017 version 5.9 or above to be present). This stretched the getting started time to more than 3-4 hours than what it would have been 1-2 hours at the maximum. 2) Azure Sphere Communication Service - not running - I successfully pinged the contest server (for the Azure Sphere design challenges) in the morning and when I tried to connect the kit in the evening, I received an error "error: Could not connect to the Azure Sphere Device Communication Service. If this issue persists, try uninstalling and reinstalling the Azure Sphere SDK.". Because of this, I had to reinstall the Azure Sphere SDK again and also changed the Azure Sphere Communication Service's log on as my user which resolved the issue. 3) OS Update - I was almost on the verge of completing my project which was built on top of 'Advanced Demo' example code. But an OS update (to 19.09) introduced errors that have to be fixed in order to complete. I know this is expected, but this has caused a delay in completing my project.
Detailed Review:
Table of Contents
Azure Sphere MT3620 Starter Kit. Let's build it word by word and see what they refer to,
Azure - https://azure.microsoft.com/en-in/
This is a cloud computing service by Microsoft. To keep things simple, think it like accessing and using your computer without it physically present where you are.
Microsoft Azure (formerly Windows Azure /ˈæʒər/) is a cloud computing service created by Microsoft for building, testing, deploying, and managing applications and services through Microsoft-managed data centers. It provides software as a service (SaaS), platform as a service (PaaS) and infrastructure as a service (IaaS) and supports many different programming languages, tools and frameworks, including both Microsoft-specific and third-party software and systems.
Azure Sphere- https://azure.microsoft.com/en-in/services/azure-sphere/
We saw Azure before this, so one among the cool things provided by Microsoft Azure is Azure Sphere. Let's see what the Microsoft Azure Sphere home page has to say about it - "Comprehensive IoT security solution—including hardware, OS and cloud components—to help you innovate with confidence". So let's break it down further,
Azure Sphere is a Linux-based operating system created by Microsoft for Internet of Things applications.[1][2][3][4][5][6][7][8] It is the first time Microsoft has publicly released an operating system running the Linux kernel[9] and the second Unix-like operating system that the company has developed for external (public) users – the other being Xenix. The name is derived from Microsoft Azure services.
The first supported processor is the ARM based MediaTek MT3620.[10]
MT3620 - https://www.mediatek.com/products/azureSphere/mt3620
This is the first processor that can support Azure Sphere, from MediaTek. NXP is following this for the next spot - https://media.nxp.com/news-releases/news-release-details/nxp-and-microsoft-bring-microsoft-azure-sphere-security
Azure Sphere MT3620 Starter Kit - Azure Sphere Starter Kit
This is the development kit built around MediaTek's MT3620 chip so this can support Azure Sphere!
To get started with the Azure Sphere MT3620 Starter kit, check out the quick start documentation and example projects from Avnet. In order to grab a quick overview, check out this Element14 & Hackster webinars - IoT Skills: Learn How To Rapidly Secure Your IoT Design with Azure Sphere & https://events.hackster.io/azurespherewebinar. To strengthen your fundamentals, visit this Hackster course -. For activities around Azure Sphere visit this Element14 community page -. Click here if you would like to know about me. Thank you rscasny, danzima, Element14 Community and Avnet for providing me this wonderful opportunity to road test the Azure Sphere MT3620 Starter kit.
References (everything inside quotes and the screengrabs):
Schedule -
Week 1 - Unboxing, Out of the Box Demo/ First Impressions
Week 2 & 3 - Testing sensors and Azure IoT Hub linking and data capture
Week 4 - 7 - Machine Learning the data collected
Week 8 - Summary and Conclusion
My project will be to test
Then capture (preferably a connected temperature or gas sensor) and collect data using the Azure Sphere MT3620 Starter kit and then store the data in Azure for machine learning the data. The results/ predictions will then be displayed in an OLED display connected with the kit.
As usual, the kit box was inside a carton box secured with crushed/ recycled/ compressed paper. The kit was received in perfect condition without any visible damages (and no invisible damage as well). Thanks to UPS and to those concerned in Element14 Community for that. The Azure Sphere MT3620 Starter kit includes,
Below are the pictures of the kit and its contents,
| {gallery:width=680,height=480} Azure Sphere MT3620 Starter Kit - Unboxing |
|---|
Azure Sphere MT3620 Starter Kit - Unboxing: Carrier Board - Top View |
Azure Sphere MT3620 Starter Kit - Unboxing: Carrier Board - Bottom View |
Azure Sphere MT3620 Starter Kit - Unboxing: Carrier Board - Side View |
Azure Sphere MT3620 Starter Kit - Unboxing: Carrier Board - Side View |
Azure Sphere MT3620 Starter Kit - Unboxing: Kit - Full View |
Below is the unboxing video of the Azure Sphere MT3620 Starter Kit,
Microsoft and Avnet have done excellent documentation of how to get started with the Azure Sphere MT3620 Starter Kit. Also, there are lots of blogs in Azure Sphere and some AVNET Azure Sphere MT3620 Starter Kit road test reviews detailing the process. So I don't want to repeat the same again. Rather I choose to explain just the Blink demo.
Blink Demo -
As I always say, there is no joy equivalent to blinking a new kit's LED! Visual Studio after Azure Sphere SDK installed will have an example Blink Project which makes it, even more, easier to attain the joy of blinking the LED. Below is an image of the Azure Sphere MT3620 Starter Kit's RGB LED light up after I programmed it with the Blink example (Forget the kitty in the background!).
The following are the steps to program your kit with the Blink example. The steps may be different for Visual Studio 2017 (but should be a similar process).
Overview
The prime motive/ objective of this project is to use the Azure Machine Learning capability through the Azure Sphere MT3620 Starter Kit. The flow is as follows,
Azure Machine Learning Studio
The Azure Machine Learning Studio is a code-less workspace for developing machine learning solutions. To start, I chose this weather dataset available in the UCI repository - https://archive.ics.uci.edu/ml/datasets/SML2010 Then dataset has temperature, humidity data with date, time and day of the week. Since this is a learning experiment, I chose the day of the week to be the predicted output. So when a particular temperature is reached at a particular time, the day of the week is predicted.
As you can see in the screenshot below, the machine learning experiment is built from the dataset to model. The dataset we chose is then subjected to the 'Linear Regression' model and trained. Then we need to set up a web service that will receive data input and output from our application (in our case Azure Sphere MT3620 Starter Kit). So I set up a predictive web service.
Once the predictive web service is up and running, we can see the sample request/ response page, which has a sample C# code. I have created a console application using that and modified as required.
Once we build and run this console application, we will receive output as shown in the screenshot below which is a decimal value of the day of the week. So, in this case, it can be approximated to 2.
Azure IoT Central
The advanced demo provided here - https://www.element14.com/community/groups/azuresphere/blog/2019/08/01/azure-sphere-starter-kit-advanced-tutorial#commen… can be used for this project. Navigate to the Rules section and create a rule with action as a webhook. Though we use Azure functions, we are creating a webhook here because we can use the URL provided by Azure function in the webhook.
When things were going good, then came the OS update. Because of this, the demo solution is now throwing many errors (see screenshot below). So, unfortunately, I have to stop here for now. I'll update once the issues are fixed with the outcome.
Issue #1 - SDK Installation
The Azure Sphere SDK took a long time to be installed in my machine. It appeared to be stuck at one point while being installed that I had to cancel the process. Unfortunately, this uninstalled the Visual Studio 2017 that I've installed already. Because of this, I had to repeat the process of installing VS 2017 followed by the SDK (since the SDK required VS 2017 version 5.9 or above to be present). This stretched the getting started time to more than 3-4 hours than what it would have been 1-2 hours at the maximum.
Issue #2 - Azure Sphere Communication Service - not running
error: Could not connect to the Azure Sphere Device Communication Service. If this issue persists, try uninstalling and reinstalling the Azure Sphere SDK.
I successfully pinged the contest server (for the Azure Sphere design challenges) in the morning and when I tried to connect the kit in the evening, I received an error "error: Could not connect to the Azure Sphere Device Communication Service. If this issue persists, try uninstalling and reinstalling the Azure Sphere SDK.". Because of this, I had to reinstall the Azure Sphere SDK again and also changed the Azure Sphere Communication Service's log on as my user which resolved the issue.
Issue #3 - OS Update
I was almost on the verge of completing my project which was built on top of 'Advanced Demo' example code. But an OS update (to 19.09) introduced errors that have to be fixed in order to complete. I know this is expected, but this has caused a delay in completing my project.
Avnet's Azure Sphere MT3620 Starter Kit is the perfect blend of hardware and software. Microsoft Azure provides numerous capabilities and security which is the most concerning factor when it comes to IoT. The carrier board built around MediaTek's MT3620 provides a perfect base for rapid prototyping with Click boards, Grove connectors, OLED interface, and Pmod connectors.
Pros
Cons
The road test review may end here, but my journey won't stop until the possibilities of creating with Avnet's Azure Sphere MT3620 runs out of stock.
* Information/ content provided in this road test review is as-is obtained during the time of writing this review and is subjected to change when the respective body owning the product/ service/ application, changes the information/ content. So please refer to the official pages (links available in the 'Useful Links/ Reference' section at the bottom of this review page) for the latest information/ content.
Top Comments
Wow... This is the best road test for Azure Sphere so far. Thanks dixonselvan for the links at the bottom. A pure treasure chest of information.
I agree! This is fantastic.
Thank you clem57 Glad you liked it