Application Note: Single Pair Ethernet for Industrial Applications
ANP085 BY FABIAN VORNHAGEN, MARTIN LEIHENSEDER, ROBERT DEMHARTER, ISMAEL MOLINA ALBA, SIMON MARK, JAIRO BUSTOS, MATTHIAS FRITSCHE
1 Evolution of Ethernet - from 4 pairs to 1 single…
APPLICATION NOTE Behind the Magic of High Frequency SMT Chip Bead Ferrite ANP045 BY JOANNE WU 1 Introduction Technology is advancing at a tremendous rate and the next generation of devices are shifting towards wireless applications. The movement towards…
APPLICATION NOTE Lifetime of Optocouplers ANO006 BY DOMINIK KOECK 1 Introduction One of the main considerations in circuit design is the expected lifetime, based on the product itself and the single components included. When considering the components…
APPLICATION NOTE What do rated current values mean? BY DR. RICHARD BLAKEY // ALEXANDER GERFER 1 Introduction Despite the efforts of some passive magnetic component manufacturers, the concept of rated current continues to be a point of contention in the…
APPLICATION NOTE
Disinfection with UV-C LEDs
ANO008 BY DOMINIK KOECK
1 Introduction
This application note gives you an overview how disinfection with UV-C light works, the benefits of UV-C LEDs and safety issues that need to be considered…
This entry is about the power consumption modes available on the i.MX RT1020 ; and how to make a current measurement when using the MIMXRT1020 EVK (Rev A2). Let’s start with a very short i.MX RT1020 overview, which is a Cortex-M7 based chip that operates…