FPGA
  • Technologies
  • More
FPGA
Blog Learning AMD Zynq: a project to generate a set of PWM signals. 3 - add GATE signal and demodulation clock
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 6 May 2023 5:08 PM Date Created
  • Views 3001 views
  • Likes 12 likes
  • Comments 23 comments
  • pynq-z2
  • amdzynqultrasoundpulse
  • zynq
  • fpga
  • vivado
  • vhdl
  • pynq
  • spartan
Related
Recommended

Learning AMD Zynq: a project to generate a set of PWM signals. 3 - add GATE signal and demodulation clock

Jan Cumps
Jan Cumps
6 May 2023
Learning AMD Zynq: a project to generate a set of PWM signals. 3 - add GATE signal and demodulation clock

Continuation of  Learning AMD Zynq: a project to generate a set of PWM signals. 2 - add overall control block, delay and pulse signal .

 yepe has a goal to create a set of signals for an ultrasone pulse generator.

image

Status after Post 2

In Post 2, we ended up with a PRF, PWM(n) and PULSE working. GATE wasn't implemented.
image

Part of the GATE code was there already. The state machine had states for the delay between the pulse train and gate signal, and for the gate signal itself. 
image

But there was no logic to get the required delay, or to handle that gate signal. Luckily, this is easy.

To get the gate delay, we'll add an extra register to the board design:
image

Don't forget to generate an address for it, using the address editor.

The Jupyter notebook will use that register to set the delay:

gate_delay_address = ol.ip_dict['axi_gpio_gate_delay']['phys_addr']
gate_delay_register = MMIO(gate_delay_address, RANGE) 
# Write 0x00 to the tri-state register at offset 0x4 to configure the IO as outputs.
gate_delay_register.write(0x4, 0x0) # Write 0x0 to location 0x4; Set tri-state to output

# ...

def gatedelay(gatedelay):
    gate_delay_register.write(0x0, gatedelay);
    
# ...

def gatedelay(gatedelay):band(2)
startdelay(20)
trainlength(98)
gatedelay(20)
prime()
fire()

The signal controller state machine will handle both the delay and the uptime of the GATE. The uptime is identical to the pulse train length, so we need no register to set it separately:

    component signal_controller is
    ---
        port (
            ---
            start_delay_i : in   std_logic_vector (start_delay_resolution - 1 downto 0);   -- delay before the pulse train.
            train_length_i: in   std_logic_vector (train_length - 1 downto 0);             -- how many PWMs in a burst train.
            gate_delay_i  : in   std_logic_vector (gate_delay_resolution - 1 downto 0);    -- delay before gate signal.
            ---
        );
    end component;

---


entity signal_controller is
    --- 
    port (
    ---
        start_delay_i : in   std_logic_vector (start_delay_resolution - 1 downto 0);   -- delay before the pulse train.
        train_length_i: in   std_logic_vector (train_length - 1 downto 0);             -- how many PWMs in a burst train.
        gate_delay_i  : in   std_logic_vector (gate_delay_resolution - 1 downto 0);    -- delay before gate signal.
        ---
    );
end signal_controller;

architecture arch of signal_controller is
    ---


begin

                case State is
                
                ---

                    when gate_delay =>
                        leds_o <= (0 => '0', 1 => '0', 2 => '1', others => '0');
                        if counter >= to_integer(unsigned(gate_delay_i)) - 1 then
                            counter <= 0;
                            state <= gate;
                        end if;

                    when gate =>
                        leds_o <= (0 => '1', 1 => '0', 2 => '1', others => '0');
                        gate_o <= '1';
                        if counter = to_integer(unsigned(train_length_i)) - 1 then
                            counter <= 0;
                            state <= done;  -- todo implement
                        end if;
                    ---
                end case;

This is an example capture:

image

Demodulation Clock

An extra requirement is to have a 20 MHz output signal to serve as demodulation clock. The easiest way to generate that, is to add an extra clock output to the existing clocking wizard:
image

That extra output can be made external. Assign it to a PIN in the I/O window or constraints file.

image

Vivado 2022.1 project and Jupyter workbook
pwm_ultrasound_pulser_20230507.zip

link to all posts.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 3 years ago +1
    The additional 20 MHz demodulation clock: The clock is not guaranteed in phase with the PWM. If that's a requirement, the state changes of the signal controller would have to be synced with the…
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to dang74

    I have been holding off digging deep in microblaze. My goal with FPGAs has been to learn vhdl, not microcontroller programming. 

    hdl was a steep learning curve for me, but lately I seem to be able to design the things I want.
    Maybe a good excuse to pick up microblaze integration. I've redone the Mastering Microblaze webinar exercise and got things working fairly easy. A good exercise for @self could be to rebuild this project on the Arty / Spartan 7 ...

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dang74
    dang74 over 3 years ago in reply to Jan Cumps

    Indeed.  Portability is the strength of FPGAs.  There would definitely be some work involved porting the portion implemented in the ARM to Microblaze but that could be fun.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

    (better link:  Learning Xilinx Zynq: a Quadrature Oscillator - 2 implementations )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to yepe

    If you need a quadrature pulse generator for the experiment:  Learning Xilinx Zynq: a Quadrature Oscillator - variable frequency 

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to yepe

    done. You'll find it at the end of the post.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>