FPGA
  • Technologies
  • More
FPGA
Blog XXICC (21st Century Co-design) release 0.0n
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: johnbeetem
  • Date Created: 20 Jan 2015 4:17 AM Date Created
  • Views 2138 views
  • Likes 2 likes
  • Comments 5 comments
  • galaxc
  • gchd
  • fpga
  • flavia
  • logi-pi
  • xxicc
  • logi-bone
Related
Recommended

XXICC (21st Century Co-design) release 0.0n

johnbeetem
johnbeetem
20 Jan 2015

Here is the new release 0.0n of XXICC, which adds Xilinx Spartan-6 Flavia implementations for the ValentF(x) LOGI-Pi board and LOGI-Bone.

 

XXICC (21st Century Co-design) is a not-for-profit research project which attempts to bring digital hardware/software co-design into the 21st Century using an improved programming language and a Reduced Software Complexity philosophy.  Its goal is to make it easier and more enjoyable to write and maintain digital hardware and software. XXICC is pronounced "Chicken Coop", so-called because it has so many layers.

 

For an overview of XXICC, see the xxicc.org home page and wiki.  For details on the GalaxC programming language, XXICC Object Editor, and GalaxC extensions for Hardware Design (GCHD), here are the latest documents and complete code.

 

Release notes for XXICC rev 0.0n

Programming in the GalaxC Language rev 0.0j: reference and user guide for the GalaxC programming language, unchanged for 0.0n.

The XXICC Anthology rev 0.0n: collection of miscellaneous XXICC topics, including user guides for the XXICC Object Editor, GCHD and Flavia.

Data files for FlaviaP32 release 0.0n: Data files for the FlaviaP32 implementation of the Free Logic Array for the Papilio One 250K.

Data files for FlaviaP48 release 0.0n: Data files for the FlaviaP48 implementation for the Papilio One 500K.

Data files for FlaviaLP56 release 0.0n: Data files for the FlaviaLP56 implementation for the ValentF(x) LOGI-Pi.

Data files for FlaviaLB56 release 0.0n:  Data files for the FlaviaLB56 implementation for the ValentF(x) LOGI-Bone.

Taming the Wild Bitstream (unchanged for 0.0n): Supplement to Flavia: the Free Logic Array.

XXICC code release 0.0n: all source code for XXICC.

XXICC source code listing rev 0.0n: source code listing in PDF.

XXICC executable binaries rev 0.0n:executable XXICC binaries if you don't want to build from source code.

GalaxC sample/demo programs rev 0.0k: sample GalaxC programs and GCHD logic libraries, unchanged for 0.0n.

GalaxC sample/demo program listings rev 0.0k: PDF listing of the sample GalaxC programs and GCHD examples, unchanged for 0.0n.

Editable XXICC documentation files rev 0.0n: editable XOE files for XXICC documentation.

Installing and Running XXICC rev 0.0n: Document describing how to install and run XXICC.

Compiling and Running GalaxC Programs rev 0.0k: Document describing how to compile and run your own GalaxC programs, unchanged for 0.0n.

 

I've tested XXICC 0.0n on GNU/Linux (Ubuntu, Raspberry Pi Debian "Wheezy", BeagleBone Debian, and BeagleBoard Ångström) and Windows (2000 and 7).  My main machine is Ubuntu, so the others are more likely to have anomalies.  Constructive comments and suggestions are most welcome.  I'd especially like to find out how to reproduce some of the bugs that have been eluding me.

 

XXICC is a FLOSS (Free as in Liberty Open Source Software) project.  Software is licensed under GPLv3 and other content is licensed under Creative Commons CC-BY-SA 3.0.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +1
    Nice update John. Do you have an end project that you intend to implement with the board or are you just looking at options to make it useful? DAB
  • johnbeetem
    johnbeetem over 11 years ago in reply to DAB +1
    DAB wrote: Nice update John. Do you have an end project that you intend to implement with the board or are you just looking at options to make it useful? Thank you for the compliment! I don't…
  • johnbeetem
    johnbeetem over 11 years ago +1
    The Papilio One works great with ODROID-C1 now. To fix the "Raspberry Pi Effect" I hooked up a USB 1.1 hub to ODROID-C1's OTG port. OTG uses a separate controller from the four USB A ports, so by keeping…
Parents
  • johnbeetem
    johnbeetem over 11 years ago

    XXICC rev 0.0n mostly runs on the ODROID-C1 ODroid - Oh Boy! using Hardkernel's Ubuntu v1.3 software.  Here are some issues and hints.  [updated item 5]

     

    1.  X11 windows don't render properly with BPP (bits per pixel) set to 32 in boot.ini.  They work for me with 24 BPP.

     

    2.  I did need to get libxft-dev to compile xxicc.  This is described in Installing and Running XXICC rev 0.0n, section 1.1.

     

    3.  Windows resize slowly because XXICC redraws many times as you drag the mouse instead of waiting for a pause.  I'll try to fix this.  Also, it's tricky to grab the lower-right corner of the window, at least with the metacity window manager.

     

    4.  To compile Flavia I needed to add a link for libftdi.so.  This is described in Installing and Running XXICC rev 0.0n, section 5.2.

     

    5. update: Flavia also works when programming over JTAG using an FTDI device.  You must set FTDI permissions as described in Installing and Running section 5.3.  I have tried both Papilio One 250K and LOGI-Pi (programmed over JTAG, not over the GPIO connector).  LOGI-Pi compiles and downloads very quickly -- about a second for Bcount4LP.  Papilio One programs very slowly.  I think this is because it's downloading over full-speed USB, which may not be optimized properly on ODROID-C1.  It's likely losing USB packets due to the "Raspberry Pi Effect".  I program LOGI-Pi using an Adafruit FT232H breakout board, which has high-speed USB.

     

    6.  Other than the above issues, XXICC seems to work fine on ODROID-C1 image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • johnbeetem
    johnbeetem over 11 years ago

    XXICC rev 0.0n mostly runs on the ODROID-C1 ODroid - Oh Boy! using Hardkernel's Ubuntu v1.3 software.  Here are some issues and hints.  [updated item 5]

     

    1.  X11 windows don't render properly with BPP (bits per pixel) set to 32 in boot.ini.  They work for me with 24 BPP.

     

    2.  I did need to get libxft-dev to compile xxicc.  This is described in Installing and Running XXICC rev 0.0n, section 1.1.

     

    3.  Windows resize slowly because XXICC redraws many times as you drag the mouse instead of waiting for a pause.  I'll try to fix this.  Also, it's tricky to grab the lower-right corner of the window, at least with the metacity window manager.

     

    4.  To compile Flavia I needed to add a link for libftdi.so.  This is described in Installing and Running XXICC rev 0.0n, section 5.2.

     

    5. update: Flavia also works when programming over JTAG using an FTDI device.  You must set FTDI permissions as described in Installing and Running section 5.3.  I have tried both Papilio One 250K and LOGI-Pi (programmed over JTAG, not over the GPIO connector).  LOGI-Pi compiles and downloads very quickly -- about a second for Bcount4LP.  Papilio One programs very slowly.  I think this is because it's downloading over full-speed USB, which may not be optimized properly on ODROID-C1.  It's likely losing USB packets due to the "Raspberry Pi Effect".  I program LOGI-Pi using an Adafruit FT232H breakout board, which has high-speed USB.

     

    6.  Other than the above issues, XXICC seems to work fine on ODROID-C1 image