Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Stepper Motor Control with Hercules High-End Timer - Part 5: Hercules RM57 Hardware Provisioning
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 4 Jun 2017 9:10 PM Date Created
  • Views 1503 views
  • Likes 3 likes
  • Comments 4 comments
  • stepper_motor
  • boosterpack
  • drv8711
  • texas_instruments
  • rm57
  • hercules
  • launchpad
Related
Recommended

Stepper Motor Control with Hercules High-End Timer - Part 5: Hercules RM57 Hardware Provisioning

Jan Cumps
Jan Cumps
4 Jun 2017

There you go. A dragon of a title image - just because I can.

 

I'm trying to control an unknown stepper motor with the high-end timer (NHET) module of a Texas Instruments Hercules microcontroller

image

I got a freebee from TI almost a year ago. An unknown stepper motor, a driver board and a Hercules RM57 LaunchPad. The code to run the motor was expected to arrive too (it was an assignment for an internal) but that never materialised. In this blog series I'm trying to program the NHET module so that it sends the right signals to make the stepper step.

 

 

In the fifth post I check what peripherals should be used to drive the DRV8711 from the Hercules RM57 safety microcontroller..

 

 

Matching the Hercules Controller with the DRV8711 Stepper Driver

I'm using a LaunchPad and a BoosterPack.

That's a double-edged sword. I don't have to make PCBs - but on the other hand I'm dependent on the TI boards for matching pins (always a bet when combining LaunchPads and BoosterPacks).

The DRV8711 BoosterPack is the driver for requirements. We need to be able to drive or read all of its pins.

I know the exercise has to be possible because someone at TI showed me a video of this combination ramping up a stepper motor.

So if at the end of the blog series this doesn't work, it's me.

 

Side note to self: this (found when writing the blog image ) Pulse Train Output application note from TI may contain most of the PWM code.

image

If that's true, it may be an unexpected windfall.

I was afraid to start programming the NHET subcontroller with the HET assembly language. It's been my weak point since as long as I work with the Hercules family.

I haven't checked the document in detail but it looks promising ...

 

... continuing with the:

 

DRV8711 BoosterPack pins

image

 

The critical ones are the SPI pins (SCLK, SDI, SDO, SCS) and the PWM pin (STEP/AIN1).

The green pins and DIR/AIN2 can be handled with any pin that's GIO capable.

3V3 and GND are standard, not to worry.

I don't need the potentiometer input and the BIN pins.

 

Hercules RM57 LaunchPad pins

Good news. A match for many. This is not that common with Hercules Launchpads. They defer often from the BoosterPack layout (deliberately not using the word standard here).

 

image

The match table below shows where I am confident and where more investigation is necessary.

 

BoosterPackFunctionRequirements for HerculesHeader 4
3.3V
nSLEEPtell driver to sleep (no current to the stepper coils)GIO out

AD1[17] or AD2[0]

SCLKSPI clockSPI clockMIBSPI3CLK
RESETreset driverGIO outGIOA[6]
STEP/AIN1PWM inputHET / PWM outNHET1[4]
DIR/AIN2motor directionGIO outNHET1[9]
GND
nSTALLis the motor stalled?GIO inNHET1[22]
nFAULTis the driver in error state?GIO inNHET1[[25] or MIBSPI3NCS[1]
SDISPI Slave in Master outSPI MOSIMIBSPI3SIMO
SDOSPI Slave out Master inSPI MISOMIBSPI6SOMI
SCSSPI chip select (active high !)SPI CSGIOB[2]

 

My main worry is the nSLEEP pin. I'll have to read the doco to see if I can render an analog input into a digital output.

I don't understand why this particular pin is used on the BoosterPack for a signal that has to be driven by the microcontroller.

On the BoosterPack standard, this is reserved for analog in signals. The pin above that is a generic IO pin. And its free. Why?

 

Related Blog
Part 1: Hardware Overview
Part 2: Stepper Controller and MSP430 Firmware
Part 3: SPI Commands and Pulse Control
Part 4: Analyse MSP430 PWM Step Signal
Part 5: Hercules RM57 Hardware Provisioning
Part 6: Hercules RM57 SPI
Part 7: HET Assembly Language Test
Part 8: HET Based Pulse Train Output
  • Sign in to reply
Parents
  • Jan Cumps
    Jan Cumps over 9 years ago

    I have SPI working on the Hercules.

     

    This is a capture of the same init sequence I captured earlier on on the MSP430:

    image

     

    Protocol Analysis:

    image

     

    Easiest job done. Now the high-end timer ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 9 years ago

    I have SPI working on the Hercules.

     

    This is a capture of the same init sequence I captured earlier on on the MSP430:

    image

     

    Protocol Analysis:

    image

     

    Easiest job done. Now the high-end timer ...